Data Fields
GPTimerWFF3_ChannelConf Struct Reference

GPTimerWFF3 channel dependent pin configuration struct. More...

#include <GPTimerWFF3.h>

Data Fields

uint8_t pin
 
uint8_t pinMux
 
uint8_t nPin
 
uint8_t nPinMux
 

Detailed Description

GPTimerWFF3 channel dependent pin configuration struct.

GPTimer struct used by the GPTimerWFF3_HWAttrs.

Field Documentation

§ pin

uint8_t GPTimerWFF3_ChannelConf::pin

Channel pin

§ pinMux

uint8_t GPTimerWFF3_ChannelConf::pinMux

Channel pin mux

§ nPin

uint8_t GPTimerWFF3_ChannelConf::nPin

Complementary channel pin

§ nPinMux

uint8_t GPTimerWFF3_ChannelConf::nPinMux

Complementary channel pin mux


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale