Data Fields
FlashStigEraseCfg Struct Reference

Flash STIG erase configuration structure. More...

#include <XMEMWFF3.h>

Collaboration diagram for FlashStigEraseCfg:
Collaboration graph
[legend]

Data Fields

uint32_t preStigCfg
 
uint32_t StigCfg
 
uint32_t postStigCfg
 
FlashRegister preStigOperation [1]
 
FlashRegister stigOperation [1]
 
FlashRegister postStigOperation [1]
 

Detailed Description

Flash STIG erase configuration structure.

Structure containing configuration parameters and register operations for STIG-based flash erase operations.

Field Documentation

§ preStigCfg

uint32_t FlashStigEraseCfg::preStigCfg

Is pre STIG configuration needed

§ StigCfg

uint32_t FlashStigEraseCfg::StigCfg

Is erase operation needed

§ postStigCfg

uint32_t FlashStigEraseCfg::postStigCfg

Is post STIG configuration needed

§ preStigOperation

FlashRegister FlashStigEraseCfg::preStigOperation[1]

Register operations to perform before STIG erase

§ stigOperation

FlashRegister FlashStigEraseCfg::stigOperation[1]

Register operations for STIG erase command

§ postStigOperation

FlashRegister FlashStigEraseCfg::postStigOperation[1]

Register operations to perform after STIG erase


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale