![]() |
![]() |
Flash polling configuration structure. More...
#include <XMEMWFF3.h>
Data Fields | |
| uint32_t | NumOfIteration |
| uint32_t | command |
| uint32_t | timeOut |
| uint32_t | polarity |
| uint32_t | mask |
Flash polling configuration structure.
Structure containing parameters for polling flash status during operations.
| uint32_t FlashPollingCfg::NumOfIteration |
Maximum number of polling iterations
| uint32_t FlashPollingCfg::command |
Command to execute for polling
| uint32_t FlashPollingCfg::timeOut |
Timeout value for polling operation
| uint32_t FlashPollingCfg::polarity |
Expected polarity of status bit
| uint32_t FlashPollingCfg::mask |
Bit mask for status checking