![]() |
![]() |
| ADC.h | Analog to Digital Conversion (ADC) Input Driver |
| ADCWFF3.h | ADC driver implementation for the ADC peripheral on Wi-Fi F3 devices |
| AnsiColor.h | |
| Board.h | Portable board-specific symbols |
| Button.h | Button driver |
| ClockP.h | Clock interface for the RTOS Porting Interface |
| CommonResourceXXF3.h | Shared resources to arbitrate access to the HSM, CAN, and APU |
| DebugP.h | Debug support |
| Display.h | Generic interface for text output |
| DisplayHost.h | Display driver for printf-like output |
| DisplayUart2.h | Display.h implementation for UART output |
| DMAWFF3.h | DMAWFF3 driver implementation |
| Driver_Init.h | |
| EventP.h | Event Group support |
| FlashWFF3.h | |
| GPIO.h | General Purpose I/O driver interface |
| GPIOWFF3.h | GPIO driver implementation for WiFi F3 devices |
| GPTimerWFF3.h | GPTimer driver implementation for Wi-Fi F3 devices |
| HSMResourceXXF3.h | Shared resources to arbitrate access to the HSM |
| hw_cpu_dwt.h | |
| hw_cpu_itm.h | |
| hw_cpu_scs.h | |
| hw_cpu_tpiu.h | |
| HwiP.h | Hardware Interrupt module for the RTOS Porting Interface |
| I2C.h | Inter-Integrated Circuit (I2C) Controller Driver |
| I2CSupport.h | Holder of common helper functions for the I2C driver |
| I2CWFF3.h | I2C driver implementation for a WiFi F3 device I2C controller |
| I2S.h | Inter-Integrated Circuit Sound (I2S) Bus Driver |
| I2SWFF3.h | I2S driver implementation for WFF3 devices |
| ITM.h | ITM driver header |
| ITMWFF3.h | CC35XX specific ITM implementation |
| LED.h | LED driver |
| List.h | Linked List interface for use in drivers |
| LogSinkBuf.h | |
| LogSinkITM.h | PRELIMINARY LogSinkITM interface |
| LogSinkUART.h | PRELIMINARY LogSinkUART interface |
| Math.h | Math utility functions |
| MessageQueueP.h | MessageQueue module for the RTOS Porting Interface |
| MutexP.h | Mutex module for the RTOS Porting Interface |
| NoRTOS.h | NoRTOS framework module |
| NVS.h | Non-Volatile Storage driver interface |
| Power.h | Power Manager |
| PowerWFF3.h | Power manager interface for WFF3 devices |
| PWM.h | Pulse Width Modulation (PWM) driver |
| PWMTimerWFF3.h | PWM driver implementation for Wi-Fi F3 devices |
| RingBuf.h | |
| SD.h | Secure Digital (SD) Driver |
| SDIO.h | Secure Digital Input Output (SDIO) Driver |
| SDIOWFF3.h | |
| SDWFF3.h | |
| SemaphoreP.h | Semaphore module for the RTOS Porting Interface |
| SPI.h | Serial Peripheral Interface (SPI) Driver Interface |
| spiffs.h | |
| SPIFFSNVS.h | Module to enable the SPI Flash File System (SPIFFS) on the TI NVS driver |
| SPIWFF3DMA.h | SPI driver implementation for a Wi-Fi F3 device SPI controller using the DMA controller |
| StructRingBuf.h | |
| SwiP.h | Software Interrupt module for the RTOS Porting Interface |
| SystemP.h | System module for the RTOS Porting Interface |
| TaskP.h | Task module for the RTOS Porting Interface |
| TimestampP.h | Timestamp module for the RTOS Porting Interface |
| types.h | |
| UART2.h | PRELIMINARY UART driver interface |
| UART2Support.h | Holder of common helper functions for the UART driver |
| UART2WFF3.h | UART driver implementation for a Low Power F3 device UART controller |
| unistd.h | |
| Watchdog.h | Watchdog driver interface |
| WatchdogWFF3.h | Watchdog driver implementation for WiFi F3 devices |
| XMEMWFF3.h |