Data Structures
Here are the data structures with brief descriptions:
 C_NoRTOS_ConfigNoRTOS framework global configuration
 CADC_Config_ADC driver's custom configuration structure
 CADC_FxnTableThe definition of an ADC function table that contains the required set of functions to control a specific ADC driver implementation
 CADC_ParamsADC Parameters used with ADC_open()
 CADCWFF3_HWAttrsADCWFF3 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions
 CADCWFF3_ObjectADCWFF3 Object
 CButton_ConfigButton configuration
 CButton_HWAttrsHardware specific settings for a button
 CButton_ObjectInternal to Button module. Members should not be accessed by the application
 CButton_ParamsButton Parameters
 CClockP_FreqHzFrequency-in-hertz struct
 CClockP_ParamsBasic ClockP Parameters
 CClockP_StructClockP structure
 CDisplay_ConfigDisplay Global configuration
 CDisplay_FxnTableThe definition of a Display function table that contains the required set of functions to control a specific Display driver implementation
 CDisplay_ParamsDisplay Parameters
 CDisplayHost_HWAttrsDisplayHost Attributes
 CDisplayHost_ObjectDisplayHost Object
 CDisplayUart2_HWAttrsDisplayUart2 Attributes
 CDisplayUart2_ObjectDisplayUart2 Object
 CEventP_StructEventP structure
 CFlashPollingCfgFlash polling configuration structure
 CFlashRegisterFlash register structure for address-data pairs
 CFlashStigEraseCfgFlash STIG erase configuration structure
 CFlashStigReadCfgFlash STIG read configuration structure
 CFlashStigWriteCfgFlash STIG write configuration structure
 CFlashTypeFlash type configuration structure
 CGPIO_ConfigGPIO driver configuration structure
 CGPTimerWFF3_ChannelConfGPTimerWFF3 channel dependent pin configuration struct
 CGPTimerWFF3_ChannelPropGPTimerWFF3 channel dependent properties struct
 CGPTimerWFF3_ConfigGPTimer Global configuration
 CGPTimerWFF3_HWAttrsGPTimerWFF3 Hardware attributes
 CGPTimerWFF3_ObjectGPTimerWFF3 Object
 CGPTimerWFF3_ParamsGPTimerWFF3 Parameters
 CHwiP_ParamsBasic HwiP Parameters
 CHwiP_StructHwiP structure
 CI2C_Config_I2C driver's custom configuration structure
 CI2C_ParamsI2C parameters used with I2C_open()
 CI2C_TransactionDefines a transaction to be used with I2C_transfer() or I2C_transferTimeout()
 CI2CWFF3_HWAttrsI2CWFF3 Hardware attributes
 CI2CWFF3_ObjectI2CWFF3 Object
 CI2S_ConfigI2S Global configuration
 CI2S_ParamsBasic I2S Parameters
 CI2S_TransactionI2S transaction descriptor
 CI2SWFF3_ADFSAdaptive Digital Frequency Synthesizer (ADFS)
 CI2SWFF3_HWAttrsI2S Hardware attributes
 CITM_HWAttrsITM Hardware Attributes
 CITMWFF3_HWAttrs
 CLED_ConfigLED configuration
 CLED_HWAttrsHardware specific settings for a LED module
 CLED_ObjectLED Object structure
 CLED_ParamsLED Parameters
 CList_Elem_
 CList_List
 CLogSinkBuf_Instance
 CLogSinkBuf_Rec
 CLogSinkITM_Instance
 CLogSinkUART_ConfigLogSinkUART Global configuration
 CLogSinkUART_HWAttrsLogSinkUART Hardware attributes
 CLogSinkUART_InstanceLogSinkUART Sink parameters
 CLogSinkUART_ObjectLogSinkUART Object
 CMessageQueueP_StructMessageQueueP structure
 CMutexP_ParamsBasic MutexP Parameters
 CMutexP_StructMutexP structure
 CNVS_AttrsNVS attributes
 CNVS_Config_NVS Global configuration
 CNVS_FxnTableThe definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation
 CNVS_ParamsNVS Parameters
 CPower_NotifyObjPower notify object structure
 CPowerWFF3_ConfigGlobal configuration structure
 CPWM_Config_PWM Global configuration
 CPWM_FxnTableThe definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation
 CPWM_ParamsPWM Parameters
 CPWMTimerWFF3_HwAttrsPWMTimerWFF3 Hardware attributes
 CPWMTimerWFF3_ObjectPWMTimerWFF3 Object
 CRingBuf_Object
 CSD_Config_SD Global configuration
 CSD_FxnTableThe definition of a SD function table that contains the required set of functions to control a specific SD driver implementation
 CSD_ParamsSD Parameters
 CSDIO_Config_SDIO Global configuration
 CSDIO_ParamsSDIO Parameters
 CSDIOWFF3_HwAttrs
 CSDIOWFF3_ObjectSDIOWFF3 driver object
 CSDIOWFF3_Param
 CSDWFF3_HwAttrs
 CSDWFF3_ObjectSDWFF3 driver object
 CSDWFF3_Param
 CSemaphoreP_ParamsBasic SemaphoreP Parameters
 CSemaphoreP_StructSemaphoreP structure
 CSPI_Config_SPI Global configuration
 CSPI_FxnTableThe definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation
 CSPI_ParamsSPI Parameters
 CSPI_TransactionA SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK
 Cspiffs_config
 Cspiffs_DIR
 Cspiffs_dirent
 Cspiffs_stat
 Cspiffs_t
 CSPIFFSNVS_Data_SPIFFSNVS data object
 CSPIFFSNVS_Lock_SPIFFSNVS Lock
 CSPIWFF3DMA_HWAttrsSPIWFF3DMA Hardware attributes
 CSPIWFF3DMA_ObjectSPIWFF3DMA Object
 CStructRingBuf_Object
 CSwiP_ParamsBasic SwiP Parameters
 CSwiP_StructSemaphoreP structure
 CTaskP_Params
 CTaskP_StructTaskP structure
 CTimestampP_Format
 CUART2_Config_UART2 Global configuration
 CUART2_ParamsUART2 Parameters
 CUART2WFF3_HWAttrsUART2WFF3 Hardware attributes
 CUART2WFF3_ObjectUART2WFF3 Object
 CWatchdog_Config_Watchdog Global configuration
 CWatchdog_FxnTableThe definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation
 CWatchdog_ParamsWatchdog Parameters
 CWatchdogWFF3_HWAttrsWatchdog hardware attributes for WFF3
 CWatchdogWFF3_ObjectWatchdog Object for WFF3
 CXMEM_AttrsXMEM attributes
 CXMEM_Config_XMEM Global configuration
 CXMEM_ParamsParameters for opening an XMEM region
 CXMEMWFF3_HWAttrsHardware attributes structure for the XMEMWFF3 driver
 CXMEMWFF3_ObjectRuntime state object for the XMEMWFF3 driver instance
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale