159 #ifndef ti_drivers_watchdog_WatchdogWFF3__include 160 #define ti_drivers_watchdog_WatchdogWFF3__include uint32_t reloadValue
Definition: WatchdogWFF3.h:180
Watchdog driver interface.
Watchdog hardware attributes for WFF3.
Definition: WatchdogWFF3.h:178
bool isOpen
Definition: WatchdogWFF3.h:190
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:357
Watchdog Object for WFF3.
Definition: WatchdogWFF3.h:188
const Watchdog_FxnTable WatchdogWFF3_fxnTable
Watchdog function table for WFF3.