49 #ifndef ti_drivers_uart2_UART2WFF3__include 50 #define ti_drivers_uart2_UART2WFF3__include 58 #include <ti/devices/DeviceFamily.h> 59 #include DeviceFamily_constructPath(inc/hw_types.h) 60 #include DeviceFamily_constructPath(driverlib/dma.h) Definition: UART2WFF3.h:81
uint32_t * dmaRxSrcAddr
Definition: UART2WFF3.h:159
Definition: UART2WFF3.h:82
PRELIMINARY UART driver interface
UART2WFF3 Hardware attributes.
Definition: UART2WFF3.h:133
uint32_t rxDmaChannel
Definition: UART2WFF3.h:137
Definition: UART2WFF3.h:80
UART2_BASE_HWATTRS uint32_t txDmaChannel
Definition: UART2WFF3.h:136
UART2WFF3_CodingScheme
UART TXD/RXD encoding/decoding scheme.
Definition: UART2WFF3.h:78
Semaphore module for the RTOS Porting Interface.
Power_NotifyObj postNotify
Definition: UART2WFF3.h:157
int32_t rtsPinMux
Definition: UART2WFF3.h:141
struct UART2WFF3_Object * UART2WFF3_Handle
uint8_t powerID
Definition: UART2WFF3.h:144
Power notify object structure.
Definition: Power.h:441
UART2_BASE_OBJECT Power_NotifyObj preNotify
Definition: UART2WFF3.h:156
bool concatenateFIFO
Definition: UART2WFF3.h:145
int32_t ctsPinMux
Definition: UART2WFF3.h:140
uint32_t * dmaTxDestAddr
Definition: UART2WFF3.h:158
UART2WFF3_CodingScheme codingScheme
Definition: UART2WFF3.h:142
uint8_t irLPClkDivider
Definition: UART2WFF3.h:143
Hardware Interrupt module for the RTOS Porting Interface.
UART2WFF3 Object.
Definition: UART2WFF3.h:153
int32_t txPinMux
Definition: UART2WFF3.h:138
int32_t rxPinMux
Definition: UART2WFF3.h:139