204 #ifndef ti_drivers_sdio_SDIOWFF3__include 205 #define ti_drivers_sdio_SDIOWFF3__include 212 #include <ti/devices/DeviceFamily.h> 213 #include DeviceFamily_constructPath(inc/hw_types.h) 214 #include DeviceFamily_constructPath(inc/hw_sdio_card_fn1.h) 215 #include DeviceFamily_constructPath(inc/hw_sdio_core.h) 216 #include DeviceFamily_constructPath(inc/hw_memmap.h) 217 #include DeviceFamily_constructPath(inc/hw_iomux.h) 218 #include DeviceFamily_constructPath(inc/hw_ints.h) Definition: SDIOWFF3.h:239
HwiP structure.
Definition: HwiP.h:166
Definition: SDIOWFF3.h:243
Definition: SDIOWFF3.h:238
Definition: SDIOWFF3.h:242
uint32_t data3PinMux
Definition: SDIOWFF3.h:323
Clock interface for the RTOS Porting Interface.
uint32_t data1Pin
Definition: SDIOWFF3.h:308
Definition: SDIOWFF3.h:244
uint32_t data3Pin
Definition: SDIOWFF3.h:320
Definition: SDIOWFF3.h:263
Definition: SDIOWFF3.h:342
uint32_t FN1baseAddr
Definition: SDIOWFF3.h:269
Definition: SDIOWFF3.h:237
uint32_t cmdPinMux
Definition: SDIOWFF3.h:299
HwiP_Struct hwiStruct
Definition: SDIOWFF3.h:335
uint32_t FN0baseAddr
Definition: SDIOWFF3.h:266
uint32_t data0Pin
Definition: SDIOWFF3.h:302
Definition: SDIOWFF3.h:235
uint32_t data1PinMux
Definition: SDIOWFF3.h:311
HwiP_Params hwiPrms
Definition: SDIOWFF3.h:332
Secure Digital Input Output (SDIO) Driver.
bool isOpen
Definition: SDIOWFF3.h:256
uint32_t irqPin
Definition: SDIOWFF3.h:326
SDIOWFF3EventCB SDIOWFF3_CallbackFxn
Definition: SDIOWFF3.h:345
SDIOWFF_eventIDX
Definition: SDIOWFF3.h:233
bool SDIOWFF3_isSdioInitialized(void)
Function to check if SDIO host already initialize SDIO peripheral SDIO initialize definition is: TRUE...
uint32_t cmdPin
Definition: SDIOWFF3.h:296
void(* SDIOWFF3EventCB)(SDIO_Handle handle, uint8_t eventIDX)
Definition: SDIOWFF3.h:231
bool isInit
Definition: SDIOWFF3.h:253
uint32_t data2Pin
Definition: SDIOWFF3.h:314
uint32_t clkPinMux
Definition: SDIOWFF3.h:293
uint32_t intPriority
Definition: SDIOWFF3.h:275
uint32_t irqPinMux
Definition: SDIOWFF3.h:329
uint32_t txDmaChannel
Definition: SDIOWFF3.h:284
SDIOWFF3 driver object.
Definition: SDIOWFF3.h:250
uint32_t rxDmaChannel
Definition: SDIOWFF3.h:281
bool cardInitiated
Definition: SDIOWFF3.h:259
uint32_t thresholdLen
Definition: SDIOWFF3.h:287
uint32_t data0PinMux
Definition: SDIOWFF3.h:305
Definition: SDIOWFF3.h:236
Definition: SDIOWFF3.h:240
uint32_t powerID
Definition: SDIOWFF3.h:278
SDIO Global configuration.
Definition: SDIO.h:124
uint32_t clkPin
Definition: SDIOWFF3.h:290
Basic HwiP Parameters.
Definition: HwiP.h:205
Hardware Interrupt module for the RTOS Porting Interface.
uint32_t intNum
Definition: SDIOWFF3.h:272
SDIOWFF3EventCB SDIOWFF3_CBFunction
Definition: SDIOWFF3.h:338
uint32_t data2PinMux
Definition: SDIOWFF3.h:317
Definition: SDIOWFF3.h:241