![]() |
![]() |
I2S driver implementation for WFF3 devices.
============================================================================
Only the following memory lengths are supported:
Some attributes in the I2S_Params structure have a limited set of supported values. These limitations are described below:
This section describes the structure and requirements for the sample buffers used in the I2S_Transaction objects.
Sample words are read from or written to the sample buffers in little-endian byte order, meaning that the least significant byte (LSByte) is stored at the lower byte address, and the most significant byte (MSByte) is stored at the higher byte address.
The sample buffers are divided into frames which are further subdivided into channels, and if a channel is used by both SD0 and SD1 (where the direction of the two pins are the same), then that channel is further subdivided into a sample word for first SD0 and then SD1.
The size of the buffers used in I2S_Transaction objects must be an even multiple of the number of bytes per frame. I.e. the number of bytes in the buffers must be of the form: 2*n*k, where k is the size of a frame in bytes and n is an integer satisfying n>=2. 2*n is the number of frames in the buffer.
Below code describes the general structure of a sample buffer if SD0 and SD1 are configured to the same direction.
Notes:
SD0_USE_CHANNEL_n should be true if SD0 uses channel n, otherwise false.SD1_USE_CHANNEL_n should be true if SD1 uses channel n, otherwise false.BYTES_PER_WORD is based on the configured memory length:
FRAMES_PER_BUFFER must be divisible by 2sampleBufferFrames needs to be cast to an uint8_t pointer to be used with the I2S driver.If SD0 and SD1 are not configured to the same direction (or only one is used) then the structure can be simplified as below:
Notes:
USE_CHANNEL_n should be true if channel n is used, otherwise false.If for example SD0 and SD1 are configured to the same direction and if channel 0 and 1 are used for SD0 and channel 0 is used for SD1, then the sample buffer would be structured as in the code below.
The I2S module uses an Adaptive Digital Frequency Synthesizer (ADFS) to divide a selected clock source and produce the audio clock (ACLK) frequency.
Using the ADFS it is possible to achieve an ACLK frequency that is a multiple of the most common sample rates, which can then be used to achieve the most common sample frequencies. It is also possible to configre the ADFS to use the selected clock source as the audio clock. This is not intended for any standard sample rate, but it can still be selected if desired.
Using I2SWFF3_HWAttrs.clkSrc it is possible to select the input clock to the ADFS. The selected input is the clock cource used by the ADFS used to generate the audio clock frequency.
The following clock sources are available:
To achieve the best performance, it is suggested to use I2SWFF3_CLK_SRC_SOC_PLL_CLK as the clock source. This is because this clock is un-swallowed. Swallowing is a clock division technique that works by eliminating/delaying pulses, which has the downside of introducing jitter. Note that I2SWFF3_CLK_SRC_SOC_CLK uses swallowing.
Another advantage of selecting the SOC PLL clock is its ability to produce the largest division factor in the ADFS due to its higher frequency. This also reduces jitter.
The audio clock (ACLK) is the output of the ADFS. This is used by the I2S hardware module when the I2S driver is opened in Controller mode (I2S_Params.moduleRole == I2S_CONTROLLER). The I2S hardware module will divide the ACLK to generate the I2S clocks (BCLK (SCK), WCLK (Ws) and CCLK). The ACLK therefore directly determines the possible sample rates, i.e. the frequency of WCLK.
To achieve a desired sample frequency (f_s), the following requirements must be met, where f_aclk is the frequency of the ACLK:
For example, if f_s = 44.1 kHz, then the first requirement is met if for example f_aclk = 11.2896 MHz = 256 * 44.1 kHz. The second requirement is met if for example the number of bits per frame is 32, because it evenly divides into 256.
If the requirements are not met, the closest possible sampling frequency to the desired sampling frequency will be used.
The frequencies most suited to be used with I2S are listed below:
The ADFS is used to generate an arbitrary clock frequency from a given input clock by division and adaptive swallowing. The resultant clock frequency mean is equal to the desired value although a significant jitter may occur. The best results are achieved when there is a large factor between the input clock frequency (Fref) and the desired output frequency (Freq).
In I2S, the ADFS is used to divide the clock source into an ACLK that is a multiple of the most common sample rates. To achieve this, the ADFS is configured with the following parameters:
The next equations can be used to compute the parameters:
Populate the I2SWFF3_ADFS structure with the computed parameters in order to use the ADFS. The computation should be done using one of the supported clock sorces as Fref and the desired audio clock as Freq.
Due to rounding errors, the ADFS may not be able to achieve the desired audio clock frequency. To compute the actual output frequency in hertz use the following formula (Fref must be in hertz):
Assign the calculated adfsOutputFreq to I2SWFF3_HWAttrs.audioClkFreq to specify the actual ACLK frequency used by the module.
#include <stdint.h>#include <stdbool.h>#include <ti/drivers/I2S.h>#include <ti/drivers/dpl/SemaphoreP.h>#include <ti/drivers/dpl/HwiP.h>#include <ti/drivers/Power.h>#include <ti/devices/DeviceFamily.h>#include <DeviceFamily_constructPath(driverlib/i2s.h)>
Go to the source code of this file.
Data Structures | |
| struct | I2SWFF3_ADFS |
| Adaptive Digital Frequency Synthesizer (ADFS) More... | |
| struct | I2SWFF3_HWAttrs |
| I2S Hardware attributes. More... | |
Enumerations | |
| enum | I2SWFF3_ClkSrc { I2SWFF3_CLK_SRC_SOC_CLK = I2S_CLK_SRC_SOC_CLK, I2SWFF3_CLK_SRC_SOC_PLL_CLK = I2S_CLK_SRC_SOC_PLL_CLK, I2SWFF3_CLK_SRC_HFXT_CLK = I2S_CLK_SRC_HFXT_CLK } |
| Clock Source. More... | |
| enum I2SWFF3_ClkSrc |
Clock Source.
Option to select the clock source used by the I2S hardware module when the I2S driver is opened in Controller mode.
| Enumerator | |
|---|---|
| I2SWFF3_CLK_SRC_SOC_CLK | System-on-Chip clock, 80 Mhz. |
| I2SWFF3_CLK_SRC_SOC_PLL_CLK | Divided Phase-Locked Loop clock, 160 Mhz. |
| I2SWFF3_CLK_SRC_HFXT_CLK | High-Frequency Crystal clock, 40 Mhz. |