119 #ifndef ti_drivers_i2c_I2CWFF3__include 120 #define ti_drivers_i2c_I2CWFF3__include I2C_BitRate bitRate
Definition: I2CWFF3.h:213
uint32_t addressMode
Definition: I2CWFF3.h:219
I2C_BASE_HWATTRS unsigned long powerMngrId
Definition: I2CWFF3.h:185
I2C_BitRate
Bit rate for an I2C driver instance specified in the I2C_Params.
Definition: I2C.h:575
uint8_t sdaPin
Definition: I2CWFF3.h:193
Power_NotifyObj i2cPostObj
Definition: I2CWFF3.h:223
uint32_t swiPriority
Definition: I2CWFF3.h:191
uint8_t sdaPinMux
Definition: I2CWFF3.h:194
I2CWFF3 Object.
Definition: I2CWFF3.h:205
uint8_t sclPinMux
Definition: I2CWFF3.h:197
void * i2cPostFxn
Definition: I2CWFF3.h:222
Software Interrupt module for the RTOS Porting Interface.
Power notify object structure.
Definition: Power.h:441
I2CWFF3 Hardware attributes.
Definition: I2CWFF3.h:180
uint8_t sclPin
Definition: I2CWFF3.h:196
I2C_BASE_OBJECT SwiP_Struct swi
Definition: I2CWFF3.h:211
SemaphoreP structure.
Definition: SwiP.h:68
Inter-Integrated Circuit (I2C) Controller Driver.