Functions
CommonResourceXXF3.h File Reference

Detailed Description

Shared resources to arbitrate access to the HSM, CAN, and APU.

============================================================================

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/dpl/SemaphoreP.h>
Include dependency graph for CommonResourceXXF3.h:

Go to the source code of this file.

Functions

void CommonResourceXXF3_constructRTOSObjects (void)
 
bool CommonResourceXXF3_acquireLock (uint32_t timeout)
 
void CommonResourceXXF3_releaseLock (void)
 
bool CommonResourceXXF3_acquireLockWithDelay (void)
 

Function Documentation

§ CommonResourceXXF3_constructRTOSObjects()

void CommonResourceXXF3_constructRTOSObjects ( void  )

§ CommonResourceXXF3_acquireLock()

bool CommonResourceXXF3_acquireLock ( uint32_t  timeout)

§ CommonResourceXXF3_releaseLock()

void CommonResourceXXF3_releaseLock ( void  )

§ CommonResourceXXF3_acquireLockWithDelay()

bool CommonResourceXXF3_acquireLockWithDelay ( void  )
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale