Board.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 /*!****************************************************************************
34  * @file Board.h
35  * @brief Portable board-specific symbols
36  *
37  * The Board header file should be included in an application as follows:
38  * @code
39  * #include <ti/drivers/Board.h>
40  * @endcode
41  *
42  * This header serves as device-independent interface for applications using
43  * peripherals connected to the device via standard digital interfaces; e.g,
44  * GPIO, SPI, I2C, UART, etc. Its purpose is to enable application code that
45  * references a peripheral to be portable to any device and board that
46  * supports the peripheral.
47  *
48  * ## Usage ##
49  *
50  * @anchor ti_drivers_Board_Synopsis
51  * ### Synopsis #
52  * @anchor ti_drivers_Board_Synopsis_Code
53  * @code
54  * #include <ti/drivers/Board.h>
55  *
56  * void main(void)
57  * {
58  * Board_init();
59  * :
60  * }
61  * @endcode
62  *
63  * ## Initializing the hardware ##
64  *
65  * \p Board_init() must be called before any other driver API. This function
66  * is owned by the user (typically generated by SysConfig), and is
67  * responsible for device specific initialization; e.g., initializing clocks
68  * and power management functionality.
69  ******************************************************************************
70  */
71 
72 #ifndef ti_drivers_Board__include
73 #define ti_drivers_Board__include
74 
75 #ifdef __cplusplus
76 extern "C" {
77 #endif
78 
93 extern void Board_init(void);
94 
95 #ifdef __cplusplus
96 }
97 #endif
98 
99 #endif /* ti_drivers_Board_include */
void Board_init(void)
Performs "early" board-level initialization required by TI-DRIVERS.
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale