![]() |
![]() |
|
CC35xxDriverLibrary
|
#include <stdint.h>#include <stdbool.h>#include "../inc/hw_types.h"#include "../inc/hw_memmap.h"#include "../inc/hw_hostmcu_aon.h"#include "../inc/hw_ints.h"

Go to the source code of this file.
Macros | |
| #define | HOSTMCU_AON_CFGWICSNS_ELP_TMR_EN (HOSTMCU_AON_CFGWICSNS_VAL_TMRREQ_EN << 0) |
| #define | HOSTMCU_AON_CFGWUTP_ELP_TMR_FAST (HOSTMCU_AON_CFGWUTP_VAL_TMRREQ << 0) |
Functions | |
| __STATIC_INLINE void | WatchdogClearWakeUpEvent (void) |
| Clears the timer wake-up event. More... | |
| __STATIC_INLINE void | WatchdogDisableWakeUpEvent (void) |
| Disables the timer wake-up event. More... | |
| __STATIC_INLINE void | WatchdogDisableResetEvent (void) |
| Disables the timer reset event. More... | |
| __STATIC_INLINE void | WatchdogEnableWakeUpEvent (void) |
| Enables the timer wake-up event. More... | |
| __STATIC_INLINE void | WatchdogEnableResetEvent (void) |
| Enables the timer reset event. More... | |
| __STATIC_INLINE bool | WatchdogStatus (void) |
| Reads the status of the timer. More... | |
| __STATIC_INLINE void | WatchdogWaitUntilEnabled (void) |
| Waits until the timer is enabled. More... | |
| __STATIC_INLINE void | WatchdogWaitUntilDisabled (void) |
| Waits until the timer is disabled. More... | |
| __STATIC_INLINE void | WatchdogReset (void) |
| Re-sets the timer back to zero. More... | |
| __STATIC_INLINE void | WatchdogSetWakeUpThreshold (uint32_t ticks) |
| Sets the wake-up threshold. More... | |
| __STATIC_INLINE void | WatchdogSetResetThreshold (uint32_t ticks) |
| Sets the reset threshold. More... | |
| __STATIC_INLINE void | WatchdogSetSwMode (void) |
| Configures the timer to work in software mode. More... | |
| void | WatchdogStartSequence (void) |
| Sequence to start the timer. More... | |
| void | WatchdogStopSequence (void) |
| Sequence to stop the timer. More... | |