![]() |
![]() |
|
CC35xxDriverLibrary
|

Go to the source code of this file.
Data Structures | |
| struct | ARM_MPU_Region_t |
Macros | |
| #define | ARM_MPU_ARMV8_H |
| #define | ARM_MPU_ATTR_DEVICE ( 0U ) |
| Attribute for device memory (outer only) More... | |
| #define | ARM_MPU_ATTR_NON_CACHEABLE ( 4U ) |
| Attribute for non-cacheable, normal memory. More... | |
| #define | ARM_MPU_ATTR_MEMORY_(NT, WB, RA, WA) ((((NT) & 1U) << 3U) | (((WB) & 1U) << 2U) | (((RA) & 1U) << 1U) | ((WA) & 1U)) |
| Attribute for normal memory (outer and inner) More... | |
| #define | ARM_MPU_ATTR_DEVICE_nGnRnE (0U) |
| Device memory type non Gathering, non Re-ordering, non Early Write Acknowledgement. More... | |
| #define | ARM_MPU_ATTR_DEVICE_nGnRE (1U) |
| Device memory type non Gathering, non Re-ordering, Early Write Acknowledgement. More... | |
| #define | ARM_MPU_ATTR_DEVICE_nGRE (2U) |
| Device memory type non Gathering, Re-ordering, Early Write Acknowledgement. More... | |
| #define | ARM_MPU_ATTR_DEVICE_GRE (3U) |
| Device memory type Gathering, Re-ordering, Early Write Acknowledgement. More... | |
| #define | ARM_MPU_ATTR(O, I) ((((O) & 0xFU) << 4U) | ((((O) & 0xFU) != 0U) ? ((I) & 0xFU) : (((I) & 0x3U) << 2U))) |
| Memory Attribute. More... | |
| #define | ARM_MPU_SH_NON (0U) |
| Normal memory non-shareable. More... | |
| #define | ARM_MPU_SH_OUTER (2U) |
| Normal memory outer shareable. More... | |
| #define | ARM_MPU_SH_INNER (3U) |
| Normal memory inner shareable. More... | |
| #define | ARM_MPU_AP_(RO, NP) ((((RO) & 1U) << 1U) | ((NP) & 1U)) |
| Memory access permissions. More... | |
| #define | ARM_MPU_RBAR(BASE, SH, RO, NP, XN) |
| Region Base Address Register value. More... | |
| #define | ARM_MPU_RLAR(LIMIT, IDX) |
| Region Limit Address Register value. More... | |
Functions | |
| __STATIC_INLINE void | ARM_MPU_Enable (uint32_t MPU_Control) |
| __STATIC_INLINE void | ARM_MPU_Disable (void) |
| __STATIC_INLINE void | ARM_MPU_SetMemAttrEx (MPU_Type *mpu, uint8_t idx, uint8_t attr) |
| __STATIC_INLINE void | ARM_MPU_SetMemAttr (uint8_t idx, uint8_t attr) |
| __STATIC_INLINE void | ARM_MPU_ClrRegionEx (MPU_Type *mpu, uint32_t rnr) |
| __STATIC_INLINE void | ARM_MPU_ClrRegion (uint32_t rnr) |
| __STATIC_INLINE void | ARM_MPU_SetRegionEx (MPU_Type *mpu, uint32_t rnr, uint32_t rbar, uint32_t rlar) |
| __STATIC_INLINE void | ARM_MPU_SetRegion (uint32_t rnr, uint32_t rbar, uint32_t rlar) |
| __STATIC_INLINE void | ARM_MPU_OrderedMemcpy (volatile uint32_t *dst, const uint32_t *__RESTRICT src, uint32_t len) |
| __STATIC_INLINE void | ARM_MPU_LoadEx (MPU_Type *mpu, uint32_t rnr, ARM_MPU_Region_t const *table, uint32_t cnt) |
| __STATIC_INLINE void | ARM_MPU_Load (uint32_t rnr, ARM_MPU_Region_t const *table, uint32_t cnt) |
| #define ARM_MPU_ARMV8_H |
| #define ARM_MPU_ATTR_DEVICE ( 0U ) |
Attribute for device memory (outer only)
| #define ARM_MPU_ATTR_NON_CACHEABLE ( 4U ) |
Attribute for non-cacheable, normal memory.
| #define ARM_MPU_ATTR_MEMORY_ | ( | NT, | |
| WB, | |||
| RA, | |||
| WA | |||
| ) | ((((NT) & 1U) << 3U) | (((WB) & 1U) << 2U) | (((RA) & 1U) << 1U) | ((WA) & 1U)) |
Attribute for normal memory (outer and inner)
| NT | Non-Transient: Set to 1 for non-transient data. |
| WB | Write-Back: Set to 1 to use write-back update policy. |
| RA | Read Allocation: Set to 1 to use cache allocation on read miss. |
| WA | Write Allocation: Set to 1 to use cache allocation on write miss. |
| #define ARM_MPU_ATTR_DEVICE_nGnRnE (0U) |
Device memory type non Gathering, non Re-ordering, non Early Write Acknowledgement.
| #define ARM_MPU_ATTR_DEVICE_nGnRE (1U) |
Device memory type non Gathering, non Re-ordering, Early Write Acknowledgement.
| #define ARM_MPU_ATTR_DEVICE_nGRE (2U) |
Device memory type non Gathering, Re-ordering, Early Write Acknowledgement.
| #define ARM_MPU_ATTR_DEVICE_GRE (3U) |
Device memory type Gathering, Re-ordering, Early Write Acknowledgement.
| #define ARM_MPU_ATTR | ( | O, | |
| I | |||
| ) | ((((O) & 0xFU) << 4U) | ((((O) & 0xFU) != 0U) ? ((I) & 0xFU) : (((I) & 0x3U) << 2U))) |
Memory Attribute.
| O | Outer memory attributes |
| I | O == ARM_MPU_ATTR_DEVICE: Device memory attributes, else: Inner memory attributes |
| #define ARM_MPU_SH_NON (0U) |
Normal memory non-shareable.
| #define ARM_MPU_SH_OUTER (2U) |
Normal memory outer shareable.
| #define ARM_MPU_SH_INNER (3U) |
Normal memory inner shareable.
| #define ARM_MPU_AP_ | ( | RO, | |
| NP | |||
| ) | ((((RO) & 1U) << 1U) | ((NP) & 1U)) |
Memory access permissions.
| RO | Read-Only: Set to 1 for read-only memory. |
| NP | Non-Privileged: Set to 1 for non-privileged memory. |
| #define ARM_MPU_RBAR | ( | BASE, | |
| SH, | |||
| RO, | |||
| NP, | |||
| XN | |||
| ) |
Region Base Address Register value.
| BASE | The base address bits [31:5] of a memory region. The value is zero extended. Effective address gets 32 byte aligned. |
| SH | Defines the Shareability domain for this memory region. |
| RO | Read-Only: Set to 1 for a read-only memory region. |
| NP | Non-Privileged: Set to 1 for a non-privileged memory region. |
| XN | eXecute Never: Set to 1 for a non-executable memory region. |
| #define ARM_MPU_RLAR | ( | LIMIT, | |
| IDX | |||
| ) |
Region Limit Address Register value.
| LIMIT | The limit address bits [31:5] for this memory region. The value is one extended. |
| IDX | The attribute index to be associated with this memory region. |
| __STATIC_INLINE void ARM_MPU_Enable | ( | uint32_t | MPU_Control | ) |
Enable the MPU.
| MPU_Control | Default access permissions for unconfigured regions. |
References __DMB(), __DSB(), __ISB(), SCB, and SCB_SHCSR_MEMFAULTENA_Msk.
| __STATIC_INLINE void ARM_MPU_Disable | ( | void | ) |
Disable the MPU.
References __DMB(), __DSB(), __ISB(), __STATIC_INLINE, SCB, and SCB_SHCSR_MEMFAULTENA_Msk.
| __STATIC_INLINE void ARM_MPU_SetMemAttrEx | ( | MPU_Type * | mpu, |
| uint8_t | idx, | ||
| uint8_t | attr | ||
| ) |
Set the memory attribute encoding to the given MPU.
| mpu | Pointer to the MPU to be configured. |
| idx | The attribute index to be set [0-7] |
| attr | The attribute value to be set. |
Referenced by ARM_MPU_SetMemAttr().
| __STATIC_INLINE void ARM_MPU_SetMemAttr | ( | uint8_t | idx, |
| uint8_t | attr | ||
| ) |
Set the memory attribute encoding.
| idx | The attribute index to be set [0-7] |
| attr | The attribute value to be set. |
References __STATIC_INLINE, and ARM_MPU_SetMemAttrEx().
| __STATIC_INLINE void ARM_MPU_ClrRegionEx | ( | MPU_Type * | mpu, |
| uint32_t | rnr | ||
| ) |
Clear and disable the given MPU region of the given MPU.
| mpu | Pointer to MPU to be used. |
| rnr | Region number to be cleared. |
Referenced by ARM_MPU_ClrRegion().
| __STATIC_INLINE void ARM_MPU_ClrRegion | ( | uint32_t | rnr | ) |
Clear and disable the given MPU region.
| rnr | Region number to be cleared. |
References __STATIC_INLINE, and ARM_MPU_ClrRegionEx().
| __STATIC_INLINE void ARM_MPU_SetRegionEx | ( | MPU_Type * | mpu, |
| uint32_t | rnr, | ||
| uint32_t | rbar, | ||
| uint32_t | rlar | ||
| ) |
Configure the given MPU region of the given MPU.
| mpu | Pointer to MPU to be used. |
| rnr | Region number to be configured. |
| rbar | Value for RBAR register. |
| rlar | Value for RLAR register. |
Referenced by ARM_MPU_SetRegion().
| __STATIC_INLINE void ARM_MPU_SetRegion | ( | uint32_t | rnr, |
| uint32_t | rbar, | ||
| uint32_t | rlar | ||
| ) |
Configure the given MPU region.
| rnr | Region number to be configured. |
| rbar | Value for RBAR register. |
| rlar | Value for RLAR register. |
References __STATIC_INLINE, and ARM_MPU_SetRegionEx().
| __STATIC_INLINE void ARM_MPU_OrderedMemcpy | ( | volatile uint32_t * | dst, |
| const uint32_t *__RESTRICT | src, | ||
| uint32_t | len | ||
| ) |
Memcopy with strictly ordered memory access, e.g. for register targets.
| dst | Destination data is copied to. |
| src | Source data is copied from. |
| len | Amount of data words to be copied. |
Referenced by ARM_MPU_LoadEx().
| __STATIC_INLINE void ARM_MPU_LoadEx | ( | MPU_Type * | mpu, |
| uint32_t | rnr, | ||
| ARM_MPU_Region_t const * | table, | ||
| uint32_t | cnt | ||
| ) |
Load the given number of MPU regions from a table to the given MPU.
| mpu | Pointer to the MPU registers to be used. |
| rnr | First region number to be configured. |
| table | Pointer to the MPU configuration table. |
| cnt | Amount of regions to be configured. |
References ARM_MPU_OrderedMemcpy(), and ARM_MPU_Region_t::RBAR.
Referenced by ARM_MPU_Load().
| __STATIC_INLINE void ARM_MPU_Load | ( | uint32_t | rnr, |
| ARM_MPU_Region_t const * | table, | ||
| uint32_t | cnt | ||
| ) |
Load the given number of MPU regions from a table.
| rnr | First region number to be configured. |
| table | Pointer to the MPU configuration table. |
| cnt | Amount of regions to be configured. |
References __STATIC_INLINE, and ARM_MPU_LoadEx().