25 #if defined ( __ICCARM__ ) 26 #pragma system_include 27 #elif defined (__clang__) 28 #pragma clang system_header 29 #elif defined ( __GNUC__ ) 30 #pragma GCC diagnostic ignored "-Wpedantic" 33 #ifndef __CORE_ARMV8MML_H_GENERIC 34 #define __CORE_ARMV8MML_H_GENERIC 68 #define __ARMv8MML_CMSIS_VERSION_MAIN (__CM_CMSIS_VERSION_MAIN) 69 #define __ARMv8MML_CMSIS_VERSION_SUB (__CM_CMSIS_VERSION_SUB) 70 #define __ARMv8MML_CMSIS_VERSION ((__ARMv8MML_CMSIS_VERSION_MAIN << 16U) | \ 71 __ARMv8MML_CMSIS_VERSION_SUB ) 73 #define __CORTEX_M (80U) 78 #if defined ( __CC_ARM ) 79 #if defined __TARGET_FPU_VFP 80 #if defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U) 83 #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)" 90 #if defined(__ARM_FEATURE_DSP) 91 #if defined(__DSP_PRESENT) && (__DSP_PRESENT == 1U) 94 #error "Compiler generates DSP (SIMD) instructions for a devices without DSP extensions (check __DSP_PRESENT)" 101 #elif defined (__ARMCC_VERSION) && (__ARMCC_VERSION >= 6010050) 103 #if defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U) 104 #define __FPU_USED 1U 106 #warning "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)" 107 #define __FPU_USED 0U 110 #define __FPU_USED 0U 113 #if defined(__ARM_FEATURE_DSP) 114 #if defined(__DSP_PRESENT) && (__DSP_PRESENT == 1U) 115 #define __DSP_USED 1U 117 #error "Compiler generates DSP (SIMD) instructions for a devices without DSP extensions (check __DSP_PRESENT)" 118 #define __DSP_USED 0U 121 #define __DSP_USED 0U 124 #elif defined ( __GNUC__ ) 125 #if defined (__VFP_FP__) && !defined(__SOFTFP__) 126 #if defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U) 127 #define __FPU_USED 1U 129 #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)" 130 #define __FPU_USED 0U 133 #define __FPU_USED 0U 136 #if defined(__ARM_FEATURE_DSP) 137 #if defined(__DSP_PRESENT) && (__DSP_PRESENT == 1U) 138 #define __DSP_USED 1U 140 #error "Compiler generates DSP (SIMD) instructions for a devices without DSP extensions (check __DSP_PRESENT)" 141 #define __DSP_USED 0U 144 #define __DSP_USED 0U 147 #elif defined ( __ICCARM__ ) 148 #if defined __ARMVFP__ 149 #if defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U) 150 #define __FPU_USED 1U 152 #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)" 153 #define __FPU_USED 0U 156 #define __FPU_USED 0U 159 #if defined(__ARM_FEATURE_DSP) 160 #if defined(__DSP_PRESENT) && (__DSP_PRESENT == 1U) 161 #define __DSP_USED 1U 163 #error "Compiler generates DSP (SIMD) instructions for a devices without DSP extensions (check __DSP_PRESENT)" 164 #define __DSP_USED 0U 167 #define __DSP_USED 0U 170 #elif defined ( __TI_ARM__ ) 171 #if defined __TI_VFP_SUPPORT__ 172 #if defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U) 173 #define __FPU_USED 1U 175 #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)" 176 #define __FPU_USED 0U 179 #define __FPU_USED 0U 182 #elif defined ( __TASKING__ ) 183 #if defined __FPU_VFP__ 184 #if defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U) 185 #define __FPU_USED 1U 187 #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)" 188 #define __FPU_USED 0U 191 #define __FPU_USED 0U 194 #elif defined ( __CSMC__ ) 195 #if ( __CSMC__ & 0x400U) 196 #if defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U) 197 #define __FPU_USED 1U 199 #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)" 200 #define __FPU_USED 0U 203 #define __FPU_USED 0U 217 #ifndef __CMSIS_GENERIC 219 #ifndef __CORE_ARMV8MML_H_DEPENDANT 220 #define __CORE_ARMV8MML_H_DEPENDANT 227 #if defined __CHECK_DEVICE_DEFINES 228 #ifndef __ARMv8MML_REV 229 #define __ARMv8MML_REV 0x0000U 230 #warning "__ARMv8MML_REV not defined in device header file; using default!" 233 #ifndef __FPU_PRESENT 234 #define __FPU_PRESENT 0U 235 #warning "__FPU_PRESENT not defined in device header file; using default!" 238 #ifndef __MPU_PRESENT 239 #define __MPU_PRESENT 0U 240 #warning "__MPU_PRESENT not defined in device header file; using default!" 243 #ifndef __SAUREGION_PRESENT 244 #define __SAUREGION_PRESENT 0U 245 #warning "__SAUREGION_PRESENT not defined in device header file; using default!" 248 #ifndef __DSP_PRESENT 249 #define __DSP_PRESENT 0U 250 #warning "__DSP_PRESENT not defined in device header file; using default!" 253 #ifndef __VTOR_PRESENT 254 #define __VTOR_PRESENT 1U 255 #warning "__VTOR_PRESENT not defined in device header file; using default!" 258 #ifndef __NVIC_PRIO_BITS 259 #define __NVIC_PRIO_BITS 3U 260 #warning "__NVIC_PRIO_BITS not defined in device header file; using default!" 263 #ifndef __Vendor_SysTickConfig 264 #define __Vendor_SysTickConfig 0U 265 #warning "__Vendor_SysTickConfig not defined in device header file; using default!" 280 #define __I volatile const 283 #define __IO volatile 286 #define __IM volatile const 287 #define __OM volatile 288 #define __IOM volatile 325 uint32_t _reserved0:16;
327 uint32_t _reserved1:7;
338 #define APSR_N_Pos 31U 339 #define APSR_N_Msk (1UL << APSR_N_Pos) 341 #define APSR_Z_Pos 30U 342 #define APSR_Z_Msk (1UL << APSR_Z_Pos) 344 #define APSR_C_Pos 29U 345 #define APSR_C_Msk (1UL << APSR_C_Pos) 347 #define APSR_V_Pos 28U 348 #define APSR_V_Msk (1UL << APSR_V_Pos) 350 #define APSR_Q_Pos 27U 351 #define APSR_Q_Msk (1UL << APSR_Q_Pos) 353 #define APSR_GE_Pos 16U 354 #define APSR_GE_Msk (0xFUL << APSR_GE_Pos) 365 uint32_t _reserved0:23;
371 #define IPSR_ISR_Pos 0U 372 #define IPSR_ISR_Msk (0x1FFUL ) 383 uint32_t _reserved0:7;
385 uint32_t _reserved1:4;
398 #define xPSR_N_Pos 31U 399 #define xPSR_N_Msk (1UL << xPSR_N_Pos) 401 #define xPSR_Z_Pos 30U 402 #define xPSR_Z_Msk (1UL << xPSR_Z_Pos) 404 #define xPSR_C_Pos 29U 405 #define xPSR_C_Msk (1UL << xPSR_C_Pos) 407 #define xPSR_V_Pos 28U 408 #define xPSR_V_Msk (1UL << xPSR_V_Pos) 410 #define xPSR_Q_Pos 27U 411 #define xPSR_Q_Msk (1UL << xPSR_Q_Pos) 413 #define xPSR_IT_Pos 25U 414 #define xPSR_IT_Msk (3UL << xPSR_IT_Pos) 416 #define xPSR_T_Pos 24U 417 #define xPSR_T_Msk (1UL << xPSR_T_Pos) 419 #define xPSR_GE_Pos 16U 420 #define xPSR_GE_Msk (0xFUL << xPSR_GE_Pos) 422 #define xPSR_ISR_Pos 0U 423 #define xPSR_ISR_Msk (0x1FFUL ) 437 uint32_t _reserved1:28;
443 #define CONTROL_SFPA_Pos 3U 444 #define CONTROL_SFPA_Msk (1UL << CONTROL_SFPA_Pos) 446 #define CONTROL_FPCA_Pos 2U 447 #define CONTROL_FPCA_Msk (1UL << CONTROL_FPCA_Pos) 449 #define CONTROL_SPSEL_Pos 1U 450 #define CONTROL_SPSEL_Msk (1UL << CONTROL_SPSEL_Pos) 452 #define CONTROL_nPRIV_Pos 0U 453 #define CONTROL_nPRIV_Msk (1UL ) 470 __IOM uint32_t ISER[16U];
471 uint32_t RESERVED0[16U];
472 __IOM uint32_t ICER[16U];
473 uint32_t RSERVED1[16U];
474 __IOM uint32_t ISPR[16U];
475 uint32_t RESERVED2[16U];
476 __IOM uint32_t ICPR[16U];
477 uint32_t RESERVED3[16U];
478 __IOM uint32_t IABR[16U];
479 uint32_t RESERVED4[16U];
480 __IOM uint32_t ITNS[16U];
481 uint32_t RESERVED5[16U];
482 __IOM uint8_t IPR[496U];
483 uint32_t RESERVED6[580U];
488 #define NVIC_STIR_INTID_Pos 0U 489 #define NVIC_STIR_INTID_Msk (0x1FFUL ) 509 __IOM uint32_t AIRCR;
512 __IOM uint8_t SHPR[12U];
513 __IOM uint32_t SHCSR;
517 __IOM uint32_t MMFAR;
520 __IM uint32_t ID_PFR[2U];
521 __IM uint32_t ID_DFR;
522 __IM uint32_t ID_ADR;
523 __IM uint32_t ID_MMFR[4U];
524 __IM uint32_t ID_ISAR[6U];
527 __IM uint32_t CCSIDR;
528 __IOM uint32_t CSSELR;
529 __IOM uint32_t CPACR;
530 __IOM uint32_t NSACR;
531 uint32_t RESERVED3[92U];
533 uint32_t RESERVED4[15U];
537 uint32_t RESERVED5[1U];
538 __OM uint32_t ICIALLU;
539 uint32_t RESERVED6[1U];
540 __OM uint32_t ICIMVAU;
541 __OM uint32_t DCIMVAC;
543 __OM uint32_t DCCMVAU;
544 __OM uint32_t DCCMVAC;
546 __OM uint32_t DCCIMVAC;
547 __OM uint32_t DCCISW;
551 #define SCB_CPUID_IMPLEMENTER_Pos 24U 552 #define SCB_CPUID_IMPLEMENTER_Msk (0xFFUL << SCB_CPUID_IMPLEMENTER_Pos) 554 #define SCB_CPUID_VARIANT_Pos 20U 555 #define SCB_CPUID_VARIANT_Msk (0xFUL << SCB_CPUID_VARIANT_Pos) 557 #define SCB_CPUID_ARCHITECTURE_Pos 16U 558 #define SCB_CPUID_ARCHITECTURE_Msk (0xFUL << SCB_CPUID_ARCHITECTURE_Pos) 560 #define SCB_CPUID_PARTNO_Pos 4U 561 #define SCB_CPUID_PARTNO_Msk (0xFFFUL << SCB_CPUID_PARTNO_Pos) 563 #define SCB_CPUID_REVISION_Pos 0U 564 #define SCB_CPUID_REVISION_Msk (0xFUL ) 567 #define SCB_ICSR_PENDNMISET_Pos 31U 568 #define SCB_ICSR_PENDNMISET_Msk (1UL << SCB_ICSR_PENDNMISET_Pos) 570 #define SCB_ICSR_NMIPENDSET_Pos SCB_ICSR_PENDNMISET_Pos 571 #define SCB_ICSR_NMIPENDSET_Msk SCB_ICSR_PENDNMISET_Msk 573 #define SCB_ICSR_PENDNMICLR_Pos 30U 574 #define SCB_ICSR_PENDNMICLR_Msk (1UL << SCB_ICSR_PENDNMICLR_Pos) 576 #define SCB_ICSR_PENDSVSET_Pos 28U 577 #define SCB_ICSR_PENDSVSET_Msk (1UL << SCB_ICSR_PENDSVSET_Pos) 579 #define SCB_ICSR_PENDSVCLR_Pos 27U 580 #define SCB_ICSR_PENDSVCLR_Msk (1UL << SCB_ICSR_PENDSVCLR_Pos) 582 #define SCB_ICSR_PENDSTSET_Pos 26U 583 #define SCB_ICSR_PENDSTSET_Msk (1UL << SCB_ICSR_PENDSTSET_Pos) 585 #define SCB_ICSR_PENDSTCLR_Pos 25U 586 #define SCB_ICSR_PENDSTCLR_Msk (1UL << SCB_ICSR_PENDSTCLR_Pos) 588 #define SCB_ICSR_STTNS_Pos 24U 589 #define SCB_ICSR_STTNS_Msk (1UL << SCB_ICSR_STTNS_Pos) 591 #define SCB_ICSR_ISRPREEMPT_Pos 23U 592 #define SCB_ICSR_ISRPREEMPT_Msk (1UL << SCB_ICSR_ISRPREEMPT_Pos) 594 #define SCB_ICSR_ISRPENDING_Pos 22U 595 #define SCB_ICSR_ISRPENDING_Msk (1UL << SCB_ICSR_ISRPENDING_Pos) 597 #define SCB_ICSR_VECTPENDING_Pos 12U 598 #define SCB_ICSR_VECTPENDING_Msk (0x1FFUL << SCB_ICSR_VECTPENDING_Pos) 600 #define SCB_ICSR_RETTOBASE_Pos 11U 601 #define SCB_ICSR_RETTOBASE_Msk (1UL << SCB_ICSR_RETTOBASE_Pos) 603 #define SCB_ICSR_VECTACTIVE_Pos 0U 604 #define SCB_ICSR_VECTACTIVE_Msk (0x1FFUL ) 607 #define SCB_VTOR_TBLOFF_Pos 7U 608 #define SCB_VTOR_TBLOFF_Msk (0x1FFFFFFUL << SCB_VTOR_TBLOFF_Pos) 611 #define SCB_AIRCR_VECTKEY_Pos 16U 612 #define SCB_AIRCR_VECTKEY_Msk (0xFFFFUL << SCB_AIRCR_VECTKEY_Pos) 614 #define SCB_AIRCR_VECTKEYSTAT_Pos 16U 615 #define SCB_AIRCR_VECTKEYSTAT_Msk (0xFFFFUL << SCB_AIRCR_VECTKEYSTAT_Pos) 617 #define SCB_AIRCR_ENDIANESS_Pos 15U 618 #define SCB_AIRCR_ENDIANESS_Msk (1UL << SCB_AIRCR_ENDIANESS_Pos) 620 #define SCB_AIRCR_PRIS_Pos 14U 621 #define SCB_AIRCR_PRIS_Msk (1UL << SCB_AIRCR_PRIS_Pos) 623 #define SCB_AIRCR_BFHFNMINS_Pos 13U 624 #define SCB_AIRCR_BFHFNMINS_Msk (1UL << SCB_AIRCR_BFHFNMINS_Pos) 626 #define SCB_AIRCR_PRIGROUP_Pos 8U 627 #define SCB_AIRCR_PRIGROUP_Msk (7UL << SCB_AIRCR_PRIGROUP_Pos) 629 #define SCB_AIRCR_SYSRESETREQS_Pos 3U 630 #define SCB_AIRCR_SYSRESETREQS_Msk (1UL << SCB_AIRCR_SYSRESETREQS_Pos) 632 #define SCB_AIRCR_SYSRESETREQ_Pos 2U 633 #define SCB_AIRCR_SYSRESETREQ_Msk (1UL << SCB_AIRCR_SYSRESETREQ_Pos) 635 #define SCB_AIRCR_VECTCLRACTIVE_Pos 1U 636 #define SCB_AIRCR_VECTCLRACTIVE_Msk (1UL << SCB_AIRCR_VECTCLRACTIVE_Pos) 639 #define SCB_SCR_SEVONPEND_Pos 4U 640 #define SCB_SCR_SEVONPEND_Msk (1UL << SCB_SCR_SEVONPEND_Pos) 642 #define SCB_SCR_SLEEPDEEPS_Pos 3U 643 #define SCB_SCR_SLEEPDEEPS_Msk (1UL << SCB_SCR_SLEEPDEEPS_Pos) 645 #define SCB_SCR_SLEEPDEEP_Pos 2U 646 #define SCB_SCR_SLEEPDEEP_Msk (1UL << SCB_SCR_SLEEPDEEP_Pos) 648 #define SCB_SCR_SLEEPONEXIT_Pos 1U 649 #define SCB_SCR_SLEEPONEXIT_Msk (1UL << SCB_SCR_SLEEPONEXIT_Pos) 652 #define SCB_CCR_BP_Pos 18U 653 #define SCB_CCR_BP_Msk (1UL << SCB_CCR_BP_Pos) 655 #define SCB_CCR_IC_Pos 17U 656 #define SCB_CCR_IC_Msk (1UL << SCB_CCR_IC_Pos) 658 #define SCB_CCR_DC_Pos 16U 659 #define SCB_CCR_DC_Msk (1UL << SCB_CCR_DC_Pos) 661 #define SCB_CCR_STKOFHFNMIGN_Pos 10U 662 #define SCB_CCR_STKOFHFNMIGN_Msk (1UL << SCB_CCR_STKOFHFNMIGN_Pos) 664 #define SCB_CCR_BFHFNMIGN_Pos 8U 665 #define SCB_CCR_BFHFNMIGN_Msk (1UL << SCB_CCR_BFHFNMIGN_Pos) 667 #define SCB_CCR_DIV_0_TRP_Pos 4U 668 #define SCB_CCR_DIV_0_TRP_Msk (1UL << SCB_CCR_DIV_0_TRP_Pos) 670 #define SCB_CCR_UNALIGN_TRP_Pos 3U 671 #define SCB_CCR_UNALIGN_TRP_Msk (1UL << SCB_CCR_UNALIGN_TRP_Pos) 673 #define SCB_CCR_USERSETMPEND_Pos 1U 674 #define SCB_CCR_USERSETMPEND_Msk (1UL << SCB_CCR_USERSETMPEND_Pos) 677 #define SCB_SHCSR_HARDFAULTPENDED_Pos 21U 678 #define SCB_SHCSR_HARDFAULTPENDED_Msk (1UL << SCB_SHCSR_HARDFAULTPENDED_Pos) 680 #define SCB_SHCSR_SECUREFAULTPENDED_Pos 20U 681 #define SCB_SHCSR_SECUREFAULTPENDED_Msk (1UL << SCB_SHCSR_SECUREFAULTPENDED_Pos) 683 #define SCB_SHCSR_SECUREFAULTENA_Pos 19U 684 #define SCB_SHCSR_SECUREFAULTENA_Msk (1UL << SCB_SHCSR_SECUREFAULTENA_Pos) 686 #define SCB_SHCSR_USGFAULTENA_Pos 18U 687 #define SCB_SHCSR_USGFAULTENA_Msk (1UL << SCB_SHCSR_USGFAULTENA_Pos) 689 #define SCB_SHCSR_BUSFAULTENA_Pos 17U 690 #define SCB_SHCSR_BUSFAULTENA_Msk (1UL << SCB_SHCSR_BUSFAULTENA_Pos) 692 #define SCB_SHCSR_MEMFAULTENA_Pos 16U 693 #define SCB_SHCSR_MEMFAULTENA_Msk (1UL << SCB_SHCSR_MEMFAULTENA_Pos) 695 #define SCB_SHCSR_SVCALLPENDED_Pos 15U 696 #define SCB_SHCSR_SVCALLPENDED_Msk (1UL << SCB_SHCSR_SVCALLPENDED_Pos) 698 #define SCB_SHCSR_BUSFAULTPENDED_Pos 14U 699 #define SCB_SHCSR_BUSFAULTPENDED_Msk (1UL << SCB_SHCSR_BUSFAULTPENDED_Pos) 701 #define SCB_SHCSR_MEMFAULTPENDED_Pos 13U 702 #define SCB_SHCSR_MEMFAULTPENDED_Msk (1UL << SCB_SHCSR_MEMFAULTPENDED_Pos) 704 #define SCB_SHCSR_USGFAULTPENDED_Pos 12U 705 #define SCB_SHCSR_USGFAULTPENDED_Msk (1UL << SCB_SHCSR_USGFAULTPENDED_Pos) 707 #define SCB_SHCSR_SYSTICKACT_Pos 11U 708 #define SCB_SHCSR_SYSTICKACT_Msk (1UL << SCB_SHCSR_SYSTICKACT_Pos) 710 #define SCB_SHCSR_PENDSVACT_Pos 10U 711 #define SCB_SHCSR_PENDSVACT_Msk (1UL << SCB_SHCSR_PENDSVACT_Pos) 713 #define SCB_SHCSR_MONITORACT_Pos 8U 714 #define SCB_SHCSR_MONITORACT_Msk (1UL << SCB_SHCSR_MONITORACT_Pos) 716 #define SCB_SHCSR_SVCALLACT_Pos 7U 717 #define SCB_SHCSR_SVCALLACT_Msk (1UL << SCB_SHCSR_SVCALLACT_Pos) 719 #define SCB_SHCSR_NMIACT_Pos 5U 720 #define SCB_SHCSR_NMIACT_Msk (1UL << SCB_SHCSR_NMIACT_Pos) 722 #define SCB_SHCSR_SECUREFAULTACT_Pos 4U 723 #define SCB_SHCSR_SECUREFAULTACT_Msk (1UL << SCB_SHCSR_SECUREFAULTACT_Pos) 725 #define SCB_SHCSR_USGFAULTACT_Pos 3U 726 #define SCB_SHCSR_USGFAULTACT_Msk (1UL << SCB_SHCSR_USGFAULTACT_Pos) 728 #define SCB_SHCSR_HARDFAULTACT_Pos 2U 729 #define SCB_SHCSR_HARDFAULTACT_Msk (1UL << SCB_SHCSR_HARDFAULTACT_Pos) 731 #define SCB_SHCSR_BUSFAULTACT_Pos 1U 732 #define SCB_SHCSR_BUSFAULTACT_Msk (1UL << SCB_SHCSR_BUSFAULTACT_Pos) 734 #define SCB_SHCSR_MEMFAULTACT_Pos 0U 735 #define SCB_SHCSR_MEMFAULTACT_Msk (1UL ) 738 #define SCB_CFSR_USGFAULTSR_Pos 16U 739 #define SCB_CFSR_USGFAULTSR_Msk (0xFFFFUL << SCB_CFSR_USGFAULTSR_Pos) 741 #define SCB_CFSR_BUSFAULTSR_Pos 8U 742 #define SCB_CFSR_BUSFAULTSR_Msk (0xFFUL << SCB_CFSR_BUSFAULTSR_Pos) 744 #define SCB_CFSR_MEMFAULTSR_Pos 0U 745 #define SCB_CFSR_MEMFAULTSR_Msk (0xFFUL ) 748 #define SCB_CFSR_MMARVALID_Pos (SCB_SHCSR_MEMFAULTACT_Pos + 7U) 749 #define SCB_CFSR_MMARVALID_Msk (1UL << SCB_CFSR_MMARVALID_Pos) 751 #define SCB_CFSR_MLSPERR_Pos (SCB_SHCSR_MEMFAULTACT_Pos + 5U) 752 #define SCB_CFSR_MLSPERR_Msk (1UL << SCB_CFSR_MLSPERR_Pos) 754 #define SCB_CFSR_MSTKERR_Pos (SCB_SHCSR_MEMFAULTACT_Pos + 4U) 755 #define SCB_CFSR_MSTKERR_Msk (1UL << SCB_CFSR_MSTKERR_Pos) 757 #define SCB_CFSR_MUNSTKERR_Pos (SCB_SHCSR_MEMFAULTACT_Pos + 3U) 758 #define SCB_CFSR_MUNSTKERR_Msk (1UL << SCB_CFSR_MUNSTKERR_Pos) 760 #define SCB_CFSR_DACCVIOL_Pos (SCB_SHCSR_MEMFAULTACT_Pos + 1U) 761 #define SCB_CFSR_DACCVIOL_Msk (1UL << SCB_CFSR_DACCVIOL_Pos) 763 #define SCB_CFSR_IACCVIOL_Pos (SCB_SHCSR_MEMFAULTACT_Pos + 0U) 764 #define SCB_CFSR_IACCVIOL_Msk (1UL ) 767 #define SCB_CFSR_BFARVALID_Pos (SCB_CFSR_BUSFAULTSR_Pos + 7U) 768 #define SCB_CFSR_BFARVALID_Msk (1UL << SCB_CFSR_BFARVALID_Pos) 770 #define SCB_CFSR_LSPERR_Pos (SCB_CFSR_BUSFAULTSR_Pos + 5U) 771 #define SCB_CFSR_LSPERR_Msk (1UL << SCB_CFSR_LSPERR_Pos) 773 #define SCB_CFSR_STKERR_Pos (SCB_CFSR_BUSFAULTSR_Pos + 4U) 774 #define SCB_CFSR_STKERR_Msk (1UL << SCB_CFSR_STKERR_Pos) 776 #define SCB_CFSR_UNSTKERR_Pos (SCB_CFSR_BUSFAULTSR_Pos + 3U) 777 #define SCB_CFSR_UNSTKERR_Msk (1UL << SCB_CFSR_UNSTKERR_Pos) 779 #define SCB_CFSR_IMPRECISERR_Pos (SCB_CFSR_BUSFAULTSR_Pos + 2U) 780 #define SCB_CFSR_IMPRECISERR_Msk (1UL << SCB_CFSR_IMPRECISERR_Pos) 782 #define SCB_CFSR_PRECISERR_Pos (SCB_CFSR_BUSFAULTSR_Pos + 1U) 783 #define SCB_CFSR_PRECISERR_Msk (1UL << SCB_CFSR_PRECISERR_Pos) 785 #define SCB_CFSR_IBUSERR_Pos (SCB_CFSR_BUSFAULTSR_Pos + 0U) 786 #define SCB_CFSR_IBUSERR_Msk (1UL << SCB_CFSR_IBUSERR_Pos) 789 #define SCB_CFSR_DIVBYZERO_Pos (SCB_CFSR_USGFAULTSR_Pos + 9U) 790 #define SCB_CFSR_DIVBYZERO_Msk (1UL << SCB_CFSR_DIVBYZERO_Pos) 792 #define SCB_CFSR_UNALIGNED_Pos (SCB_CFSR_USGFAULTSR_Pos + 8U) 793 #define SCB_CFSR_UNALIGNED_Msk (1UL << SCB_CFSR_UNALIGNED_Pos) 795 #define SCB_CFSR_STKOF_Pos (SCB_CFSR_USGFAULTSR_Pos + 4U) 796 #define SCB_CFSR_STKOF_Msk (1UL << SCB_CFSR_STKOF_Pos) 798 #define SCB_CFSR_NOCP_Pos (SCB_CFSR_USGFAULTSR_Pos + 3U) 799 #define SCB_CFSR_NOCP_Msk (1UL << SCB_CFSR_NOCP_Pos) 801 #define SCB_CFSR_INVPC_Pos (SCB_CFSR_USGFAULTSR_Pos + 2U) 802 #define SCB_CFSR_INVPC_Msk (1UL << SCB_CFSR_INVPC_Pos) 804 #define SCB_CFSR_INVSTATE_Pos (SCB_CFSR_USGFAULTSR_Pos + 1U) 805 #define SCB_CFSR_INVSTATE_Msk (1UL << SCB_CFSR_INVSTATE_Pos) 807 #define SCB_CFSR_UNDEFINSTR_Pos (SCB_CFSR_USGFAULTSR_Pos + 0U) 808 #define SCB_CFSR_UNDEFINSTR_Msk (1UL << SCB_CFSR_UNDEFINSTR_Pos) 811 #define SCB_HFSR_DEBUGEVT_Pos 31U 812 #define SCB_HFSR_DEBUGEVT_Msk (1UL << SCB_HFSR_DEBUGEVT_Pos) 814 #define SCB_HFSR_FORCED_Pos 30U 815 #define SCB_HFSR_FORCED_Msk (1UL << SCB_HFSR_FORCED_Pos) 817 #define SCB_HFSR_VECTTBL_Pos 1U 818 #define SCB_HFSR_VECTTBL_Msk (1UL << SCB_HFSR_VECTTBL_Pos) 821 #define SCB_DFSR_EXTERNAL_Pos 4U 822 #define SCB_DFSR_EXTERNAL_Msk (1UL << SCB_DFSR_EXTERNAL_Pos) 824 #define SCB_DFSR_VCATCH_Pos 3U 825 #define SCB_DFSR_VCATCH_Msk (1UL << SCB_DFSR_VCATCH_Pos) 827 #define SCB_DFSR_DWTTRAP_Pos 2U 828 #define SCB_DFSR_DWTTRAP_Msk (1UL << SCB_DFSR_DWTTRAP_Pos) 830 #define SCB_DFSR_BKPT_Pos 1U 831 #define SCB_DFSR_BKPT_Msk (1UL << SCB_DFSR_BKPT_Pos) 833 #define SCB_DFSR_HALTED_Pos 0U 834 #define SCB_DFSR_HALTED_Msk (1UL ) 837 #define SCB_NSACR_CP11_Pos 11U 838 #define SCB_NSACR_CP11_Msk (1UL << SCB_NSACR_CP11_Pos) 840 #define SCB_NSACR_CP10_Pos 10U 841 #define SCB_NSACR_CP10_Msk (1UL << SCB_NSACR_CP10_Pos) 843 #define SCB_NSACR_CPn_Pos 0U 844 #define SCB_NSACR_CPn_Msk (1UL ) 847 #define SCB_CLIDR_LOUU_Pos 27U 848 #define SCB_CLIDR_LOUU_Msk (7UL << SCB_CLIDR_LOUU_Pos) 850 #define SCB_CLIDR_LOC_Pos 24U 851 #define SCB_CLIDR_LOC_Msk (7UL << SCB_CLIDR_LOC_Pos) 854 #define SCB_CTR_FORMAT_Pos 29U 855 #define SCB_CTR_FORMAT_Msk (7UL << SCB_CTR_FORMAT_Pos) 857 #define SCB_CTR_CWG_Pos 24U 858 #define SCB_CTR_CWG_Msk (0xFUL << SCB_CTR_CWG_Pos) 860 #define SCB_CTR_ERG_Pos 20U 861 #define SCB_CTR_ERG_Msk (0xFUL << SCB_CTR_ERG_Pos) 863 #define SCB_CTR_DMINLINE_Pos 16U 864 #define SCB_CTR_DMINLINE_Msk (0xFUL << SCB_CTR_DMINLINE_Pos) 866 #define SCB_CTR_IMINLINE_Pos 0U 867 #define SCB_CTR_IMINLINE_Msk (0xFUL ) 870 #define SCB_CCSIDR_WT_Pos 31U 871 #define SCB_CCSIDR_WT_Msk (1UL << SCB_CCSIDR_WT_Pos) 873 #define SCB_CCSIDR_WB_Pos 30U 874 #define SCB_CCSIDR_WB_Msk (1UL << SCB_CCSIDR_WB_Pos) 876 #define SCB_CCSIDR_RA_Pos 29U 877 #define SCB_CCSIDR_RA_Msk (1UL << SCB_CCSIDR_RA_Pos) 879 #define SCB_CCSIDR_WA_Pos 28U 880 #define SCB_CCSIDR_WA_Msk (1UL << SCB_CCSIDR_WA_Pos) 882 #define SCB_CCSIDR_NUMSETS_Pos 13U 883 #define SCB_CCSIDR_NUMSETS_Msk (0x7FFFUL << SCB_CCSIDR_NUMSETS_Pos) 885 #define SCB_CCSIDR_ASSOCIATIVITY_Pos 3U 886 #define SCB_CCSIDR_ASSOCIATIVITY_Msk (0x3FFUL << SCB_CCSIDR_ASSOCIATIVITY_Pos) 888 #define SCB_CCSIDR_LINESIZE_Pos 0U 889 #define SCB_CCSIDR_LINESIZE_Msk (7UL ) 892 #define SCB_CSSELR_LEVEL_Pos 1U 893 #define SCB_CSSELR_LEVEL_Msk (7UL << SCB_CSSELR_LEVEL_Pos) 895 #define SCB_CSSELR_IND_Pos 0U 896 #define SCB_CSSELR_IND_Msk (1UL ) 899 #define SCB_STIR_INTID_Pos 0U 900 #define SCB_STIR_INTID_Msk (0x1FFUL ) 903 #define SCB_DCISW_WAY_Pos 30U 904 #define SCB_DCISW_WAY_Msk (3UL << SCB_DCISW_WAY_Pos) 906 #define SCB_DCISW_SET_Pos 5U 907 #define SCB_DCISW_SET_Msk (0x1FFUL << SCB_DCISW_SET_Pos) 910 #define SCB_DCCSW_WAY_Pos 30U 911 #define SCB_DCCSW_WAY_Msk (3UL << SCB_DCCSW_WAY_Pos) 913 #define SCB_DCCSW_SET_Pos 5U 914 #define SCB_DCCSW_SET_Msk (0x1FFUL << SCB_DCCSW_SET_Pos) 917 #define SCB_DCCISW_WAY_Pos 30U 918 #define SCB_DCCISW_WAY_Msk (3UL << SCB_DCCISW_WAY_Pos) 920 #define SCB_DCCISW_SET_Pos 5U 921 #define SCB_DCCISW_SET_Msk (0x1FFUL << SCB_DCCISW_SET_Pos) 938 uint32_t RESERVED0[1U];
940 __IOM uint32_t ACTLR;
941 __IOM uint32_t CPPWR;
945 #define SCnSCB_ICTR_INTLINESNUM_Pos 0U 946 #define SCnSCB_ICTR_INTLINESNUM_Msk (0xFUL ) 970 #define SysTick_CTRL_COUNTFLAG_Pos 16U 971 #define SysTick_CTRL_COUNTFLAG_Msk (1UL << SysTick_CTRL_COUNTFLAG_Pos) 973 #define SysTick_CTRL_CLKSOURCE_Pos 2U 974 #define SysTick_CTRL_CLKSOURCE_Msk (1UL << SysTick_CTRL_CLKSOURCE_Pos) 976 #define SysTick_CTRL_TICKINT_Pos 1U 977 #define SysTick_CTRL_TICKINT_Msk (1UL << SysTick_CTRL_TICKINT_Pos) 979 #define SysTick_CTRL_ENABLE_Pos 0U 980 #define SysTick_CTRL_ENABLE_Msk (1UL ) 983 #define SysTick_LOAD_RELOAD_Pos 0U 984 #define SysTick_LOAD_RELOAD_Msk (0xFFFFFFUL ) 987 #define SysTick_VAL_CURRENT_Pos 0U 988 #define SysTick_VAL_CURRENT_Msk (0xFFFFFFUL ) 991 #define SysTick_CALIB_NOREF_Pos 31U 992 #define SysTick_CALIB_NOREF_Msk (1UL << SysTick_CALIB_NOREF_Pos) 994 #define SysTick_CALIB_SKEW_Pos 30U 995 #define SysTick_CALIB_SKEW_Msk (1UL << SysTick_CALIB_SKEW_Pos) 997 #define SysTick_CALIB_TENMS_Pos 0U 998 #define SysTick_CALIB_TENMS_Msk (0xFFFFFFUL ) 1021 uint32_t RESERVED0[864U];
1023 uint32_t RESERVED1[15U];
1025 uint32_t RESERVED2[15U];
1027 uint32_t RESERVED3[32U];
1028 uint32_t RESERVED4[43U];
1031 uint32_t RESERVED5[1U];
1032 __IM uint32_t DEVARCH;
1033 uint32_t RESERVED6[4U];
1049 #define ITM_STIM_DISABLED_Pos 1U 1050 #define ITM_STIM_DISABLED_Msk (0x1UL << ITM_STIM_DISABLED_Pos) 1052 #define ITM_STIM_FIFOREADY_Pos 0U 1053 #define ITM_STIM_FIFOREADY_Msk (0x1UL ) 1056 #define ITM_TPR_PRIVMASK_Pos 0U 1057 #define ITM_TPR_PRIVMASK_Msk (0xFUL ) 1060 #define ITM_TCR_BUSY_Pos 23U 1061 #define ITM_TCR_BUSY_Msk (1UL << ITM_TCR_BUSY_Pos) 1063 #define ITM_TCR_TRACEBUSID_Pos 16U 1064 #define ITM_TCR_TRACEBUSID_Msk (0x7FUL << ITM_TCR_TRACEBUSID_Pos) 1066 #define ITM_TCR_GTSFREQ_Pos 10U 1067 #define ITM_TCR_GTSFREQ_Msk (3UL << ITM_TCR_GTSFREQ_Pos) 1069 #define ITM_TCR_TSPRESCALE_Pos 8U 1070 #define ITM_TCR_TSPRESCALE_Msk (3UL << ITM_TCR_TSPRESCALE_Pos) 1072 #define ITM_TCR_STALLENA_Pos 5U 1073 #define ITM_TCR_STALLENA_Msk (1UL << ITM_TCR_STALLENA_Pos) 1075 #define ITM_TCR_SWOENA_Pos 4U 1076 #define ITM_TCR_SWOENA_Msk (1UL << ITM_TCR_SWOENA_Pos) 1078 #define ITM_TCR_DWTENA_Pos 3U 1079 #define ITM_TCR_DWTENA_Msk (1UL << ITM_TCR_DWTENA_Pos) 1081 #define ITM_TCR_SYNCENA_Pos 2U 1082 #define ITM_TCR_SYNCENA_Msk (1UL << ITM_TCR_SYNCENA_Pos) 1084 #define ITM_TCR_TSENA_Pos 1U 1085 #define ITM_TCR_TSENA_Msk (1UL << ITM_TCR_TSENA_Pos) 1087 #define ITM_TCR_ITMENA_Pos 0U 1088 #define ITM_TCR_ITMENA_Msk (1UL ) 1091 #define ITM_LSR_ByteAcc_Pos 2U 1092 #define ITM_LSR_ByteAcc_Msk (1UL << ITM_LSR_ByteAcc_Pos) 1094 #define ITM_LSR_Access_Pos 1U 1095 #define ITM_LSR_Access_Msk (1UL << ITM_LSR_Access_Pos) 1097 #define ITM_LSR_Present_Pos 0U 1098 #define ITM_LSR_Present_Msk (1UL ) 1115 __IOM uint32_t CTRL;
1116 __IOM uint32_t CYCCNT;
1117 __IOM uint32_t CPICNT;
1118 __IOM uint32_t EXCCNT;
1119 __IOM uint32_t SLEEPCNT;
1120 __IOM uint32_t LSUCNT;
1121 __IOM uint32_t FOLDCNT;
1123 __IOM uint32_t COMP0;
1124 uint32_t RESERVED1[1U];
1125 __IOM uint32_t FUNCTION0;
1126 uint32_t RESERVED2[1U];
1127 __IOM uint32_t COMP1;
1128 uint32_t RESERVED3[1U];
1129 __IOM uint32_t FUNCTION1;
1130 uint32_t RESERVED4[1U];
1131 __IOM uint32_t COMP2;
1132 uint32_t RESERVED5[1U];
1133 __IOM uint32_t FUNCTION2;
1134 uint32_t RESERVED6[1U];
1135 __IOM uint32_t COMP3;
1136 uint32_t RESERVED7[1U];
1137 __IOM uint32_t FUNCTION3;
1138 uint32_t RESERVED8[1U];
1139 __IOM uint32_t COMP4;
1140 uint32_t RESERVED9[1U];
1141 __IOM uint32_t FUNCTION4;
1142 uint32_t RESERVED10[1U];
1143 __IOM uint32_t COMP5;
1144 uint32_t RESERVED11[1U];
1145 __IOM uint32_t FUNCTION5;
1146 uint32_t RESERVED12[1U];
1147 __IOM uint32_t COMP6;
1148 uint32_t RESERVED13[1U];
1149 __IOM uint32_t FUNCTION6;
1150 uint32_t RESERVED14[1U];
1151 __IOM uint32_t COMP7;
1152 uint32_t RESERVED15[1U];
1153 __IOM uint32_t FUNCTION7;
1154 uint32_t RESERVED16[1U];
1155 __IOM uint32_t COMP8;
1156 uint32_t RESERVED17[1U];
1157 __IOM uint32_t FUNCTION8;
1158 uint32_t RESERVED18[1U];
1159 __IOM uint32_t COMP9;
1160 uint32_t RESERVED19[1U];
1161 __IOM uint32_t FUNCTION9;
1162 uint32_t RESERVED20[1U];
1163 __IOM uint32_t COMP10;
1164 uint32_t RESERVED21[1U];
1165 __IOM uint32_t FUNCTION10;
1166 uint32_t RESERVED22[1U];
1167 __IOM uint32_t COMP11;
1168 uint32_t RESERVED23[1U];
1169 __IOM uint32_t FUNCTION11;
1170 uint32_t RESERVED24[1U];
1171 __IOM uint32_t COMP12;
1172 uint32_t RESERVED25[1U];
1173 __IOM uint32_t FUNCTION12;
1174 uint32_t RESERVED26[1U];
1175 __IOM uint32_t COMP13;
1176 uint32_t RESERVED27[1U];
1177 __IOM uint32_t FUNCTION13;
1178 uint32_t RESERVED28[1U];
1179 __IOM uint32_t COMP14;
1180 uint32_t RESERVED29[1U];
1181 __IOM uint32_t FUNCTION14;
1182 uint32_t RESERVED30[1U];
1183 __IOM uint32_t COMP15;
1184 uint32_t RESERVED31[1U];
1185 __IOM uint32_t FUNCTION15;
1186 uint32_t RESERVED32[934U];
1188 uint32_t RESERVED33[1U];
1189 __IM uint32_t DEVARCH;
1193 #define DWT_CTRL_NUMCOMP_Pos 28U 1194 #define DWT_CTRL_NUMCOMP_Msk (0xFUL << DWT_CTRL_NUMCOMP_Pos) 1196 #define DWT_CTRL_NOTRCPKT_Pos 27U 1197 #define DWT_CTRL_NOTRCPKT_Msk (0x1UL << DWT_CTRL_NOTRCPKT_Pos) 1199 #define DWT_CTRL_NOEXTTRIG_Pos 26U 1200 #define DWT_CTRL_NOEXTTRIG_Msk (0x1UL << DWT_CTRL_NOEXTTRIG_Pos) 1202 #define DWT_CTRL_NOCYCCNT_Pos 25U 1203 #define DWT_CTRL_NOCYCCNT_Msk (0x1UL << DWT_CTRL_NOCYCCNT_Pos) 1205 #define DWT_CTRL_NOPRFCNT_Pos 24U 1206 #define DWT_CTRL_NOPRFCNT_Msk (0x1UL << DWT_CTRL_NOPRFCNT_Pos) 1208 #define DWT_CTRL_CYCDISS_Pos 23U 1209 #define DWT_CTRL_CYCDISS_Msk (0x1UL << DWT_CTRL_CYCDISS_Pos) 1211 #define DWT_CTRL_CYCEVTENA_Pos 22U 1212 #define DWT_CTRL_CYCEVTENA_Msk (0x1UL << DWT_CTRL_CYCEVTENA_Pos) 1214 #define DWT_CTRL_FOLDEVTENA_Pos 21U 1215 #define DWT_CTRL_FOLDEVTENA_Msk (0x1UL << DWT_CTRL_FOLDEVTENA_Pos) 1217 #define DWT_CTRL_LSUEVTENA_Pos 20U 1218 #define DWT_CTRL_LSUEVTENA_Msk (0x1UL << DWT_CTRL_LSUEVTENA_Pos) 1220 #define DWT_CTRL_SLEEPEVTENA_Pos 19U 1221 #define DWT_CTRL_SLEEPEVTENA_Msk (0x1UL << DWT_CTRL_SLEEPEVTENA_Pos) 1223 #define DWT_CTRL_EXCEVTENA_Pos 18U 1224 #define DWT_CTRL_EXCEVTENA_Msk (0x1UL << DWT_CTRL_EXCEVTENA_Pos) 1226 #define DWT_CTRL_CPIEVTENA_Pos 17U 1227 #define DWT_CTRL_CPIEVTENA_Msk (0x1UL << DWT_CTRL_CPIEVTENA_Pos) 1229 #define DWT_CTRL_EXCTRCENA_Pos 16U 1230 #define DWT_CTRL_EXCTRCENA_Msk (0x1UL << DWT_CTRL_EXCTRCENA_Pos) 1232 #define DWT_CTRL_PCSAMPLENA_Pos 12U 1233 #define DWT_CTRL_PCSAMPLENA_Msk (0x1UL << DWT_CTRL_PCSAMPLENA_Pos) 1235 #define DWT_CTRL_SYNCTAP_Pos 10U 1236 #define DWT_CTRL_SYNCTAP_Msk (0x3UL << DWT_CTRL_SYNCTAP_Pos) 1238 #define DWT_CTRL_CYCTAP_Pos 9U 1239 #define DWT_CTRL_CYCTAP_Msk (0x1UL << DWT_CTRL_CYCTAP_Pos) 1241 #define DWT_CTRL_POSTINIT_Pos 5U 1242 #define DWT_CTRL_POSTINIT_Msk (0xFUL << DWT_CTRL_POSTINIT_Pos) 1244 #define DWT_CTRL_POSTPRESET_Pos 1U 1245 #define DWT_CTRL_POSTPRESET_Msk (0xFUL << DWT_CTRL_POSTPRESET_Pos) 1247 #define DWT_CTRL_CYCCNTENA_Pos 0U 1248 #define DWT_CTRL_CYCCNTENA_Msk (0x1UL ) 1251 #define DWT_CPICNT_CPICNT_Pos 0U 1252 #define DWT_CPICNT_CPICNT_Msk (0xFFUL ) 1255 #define DWT_EXCCNT_EXCCNT_Pos 0U 1256 #define DWT_EXCCNT_EXCCNT_Msk (0xFFUL ) 1259 #define DWT_SLEEPCNT_SLEEPCNT_Pos 0U 1260 #define DWT_SLEEPCNT_SLEEPCNT_Msk (0xFFUL ) 1263 #define DWT_LSUCNT_LSUCNT_Pos 0U 1264 #define DWT_LSUCNT_LSUCNT_Msk (0xFFUL ) 1267 #define DWT_FOLDCNT_FOLDCNT_Pos 0U 1268 #define DWT_FOLDCNT_FOLDCNT_Msk (0xFFUL ) 1271 #define DWT_FUNCTION_ID_Pos 27U 1272 #define DWT_FUNCTION_ID_Msk (0x1FUL << DWT_FUNCTION_ID_Pos) 1274 #define DWT_FUNCTION_MATCHED_Pos 24U 1275 #define DWT_FUNCTION_MATCHED_Msk (0x1UL << DWT_FUNCTION_MATCHED_Pos) 1277 #define DWT_FUNCTION_DATAVSIZE_Pos 10U 1278 #define DWT_FUNCTION_DATAVSIZE_Msk (0x3UL << DWT_FUNCTION_DATAVSIZE_Pos) 1280 #define DWT_FUNCTION_ACTION_Pos 4U 1281 #define DWT_FUNCTION_ACTION_Msk (0x1UL << DWT_FUNCTION_ACTION_Pos) 1283 #define DWT_FUNCTION_MATCH_Pos 0U 1284 #define DWT_FUNCTION_MATCH_Msk (0xFUL ) 1301 __IM uint32_t SSPSR;
1302 __IOM uint32_t CSPSR;
1303 uint32_t RESERVED0[2U];
1304 __IOM uint32_t ACPR;
1305 uint32_t RESERVED1[55U];
1306 __IOM uint32_t SPPR;
1307 uint32_t RESERVED2[131U];
1309 __IOM uint32_t FFCR;
1310 __IOM uint32_t PSCR;
1311 uint32_t RESERVED3[809U];
1314 uint32_t RESERVED4[4U];
1316 __IM uint32_t DEVTYPE;
1320 #define TPI_ACPR_SWOSCALER_Pos 0U 1321 #define TPI_ACPR_SWOSCALER_Msk (0xFFFFUL ) 1324 #define TPI_SPPR_TXMODE_Pos 0U 1325 #define TPI_SPPR_TXMODE_Msk (0x3UL ) 1328 #define TPI_FFSR_FtNonStop_Pos 3U 1329 #define TPI_FFSR_FtNonStop_Msk (0x1UL << TPI_FFSR_FtNonStop_Pos) 1331 #define TPI_FFSR_TCPresent_Pos 2U 1332 #define TPI_FFSR_TCPresent_Msk (0x1UL << TPI_FFSR_TCPresent_Pos) 1334 #define TPI_FFSR_FtStopped_Pos 1U 1335 #define TPI_FFSR_FtStopped_Msk (0x1UL << TPI_FFSR_FtStopped_Pos) 1337 #define TPI_FFSR_FlInProg_Pos 0U 1338 #define TPI_FFSR_FlInProg_Msk (0x1UL ) 1341 #define TPI_FFCR_TrigIn_Pos 8U 1342 #define TPI_FFCR_TrigIn_Msk (0x1UL << TPI_FFCR_TrigIn_Pos) 1344 #define TPI_FFCR_FOnMan_Pos 6U 1345 #define TPI_FFCR_FOnMan_Msk (0x1UL << TPI_FFCR_FOnMan_Pos) 1347 #define TPI_FFCR_EnFCont_Pos 1U 1348 #define TPI_FFCR_EnFCont_Msk (0x1UL << TPI_FFCR_EnFCont_Pos) 1351 #define TPI_PSCR_PSCount_Pos 0U 1352 #define TPI_PSCR_PSCount_Msk (0x1FUL ) 1355 #define TPI_LSR_nTT_Pos 1U 1356 #define TPI_LSR_nTT_Msk (0x1UL << TPI_LSR_nTT_Pos) 1358 #define TPI_LSR_SLK_Pos 1U 1359 #define TPI_LSR_SLK_Msk (0x1UL << TPI_LSR_SLK_Pos) 1361 #define TPI_LSR_SLI_Pos 0U 1362 #define TPI_LSR_SLI_Msk (0x1UL ) 1365 #define TPI_DEVID_NRZVALID_Pos 11U 1366 #define TPI_DEVID_NRZVALID_Msk (0x1UL << TPI_DEVID_NRZVALID_Pos) 1368 #define TPI_DEVID_MANCVALID_Pos 10U 1369 #define TPI_DEVID_MANCVALID_Msk (0x1UL << TPI_DEVID_MANCVALID_Pos) 1371 #define TPI_DEVID_PTINVALID_Pos 9U 1372 #define TPI_DEVID_PTINVALID_Msk (0x1UL << TPI_DEVID_PTINVALID_Pos) 1374 #define TPI_DEVID_FIFOSZ_Pos 6U 1375 #define TPI_DEVID_FIFOSZ_Msk (0x7UL << TPI_DEVID_FIFOSZ_Pos) 1378 #define TPI_DEVTYPE_SubType_Pos 4U 1379 #define TPI_DEVTYPE_SubType_Msk (0xFUL ) 1381 #define TPI_DEVTYPE_MajorType_Pos 0U 1382 #define TPI_DEVTYPE_MajorType_Msk (0xFUL << TPI_DEVTYPE_MajorType_Pos) 1387 #if defined (__MPU_PRESENT) && (__MPU_PRESENT == 1U) 1401 __IOM uint32_t CTRL;
1403 __IOM uint32_t RBAR;
1404 __IOM uint32_t RLAR;
1405 __IOM uint32_t RBAR_A1;
1406 __IOM uint32_t RLAR_A1;
1407 __IOM uint32_t RBAR_A2;
1408 __IOM uint32_t RLAR_A2;
1409 __IOM uint32_t RBAR_A3;
1410 __IOM uint32_t RLAR_A3;
1411 uint32_t RESERVED0[1];
1413 __IOM uint32_t MAIR[2];
1415 __IOM uint32_t MAIR0;
1416 __IOM uint32_t MAIR1;
1421 #define MPU_TYPE_RALIASES 4U 1424 #define MPU_TYPE_IREGION_Pos 16U 1425 #define MPU_TYPE_IREGION_Msk (0xFFUL << MPU_TYPE_IREGION_Pos) 1427 #define MPU_TYPE_DREGION_Pos 8U 1428 #define MPU_TYPE_DREGION_Msk (0xFFUL << MPU_TYPE_DREGION_Pos) 1430 #define MPU_TYPE_SEPARATE_Pos 0U 1431 #define MPU_TYPE_SEPARATE_Msk (1UL ) 1434 #define MPU_CTRL_PRIVDEFENA_Pos 2U 1435 #define MPU_CTRL_PRIVDEFENA_Msk (1UL << MPU_CTRL_PRIVDEFENA_Pos) 1437 #define MPU_CTRL_HFNMIENA_Pos 1U 1438 #define MPU_CTRL_HFNMIENA_Msk (1UL << MPU_CTRL_HFNMIENA_Pos) 1440 #define MPU_CTRL_ENABLE_Pos 0U 1441 #define MPU_CTRL_ENABLE_Msk (1UL ) 1444 #define MPU_RNR_REGION_Pos 0U 1445 #define MPU_RNR_REGION_Msk (0xFFUL ) 1448 #define MPU_RBAR_BASE_Pos 5U 1449 #define MPU_RBAR_BASE_Msk (0x7FFFFFFUL << MPU_RBAR_BASE_Pos) 1451 #define MPU_RBAR_SH_Pos 3U 1452 #define MPU_RBAR_SH_Msk (0x3UL << MPU_RBAR_SH_Pos) 1454 #define MPU_RBAR_AP_Pos 1U 1455 #define MPU_RBAR_AP_Msk (0x3UL << MPU_RBAR_AP_Pos) 1457 #define MPU_RBAR_XN_Pos 0U 1458 #define MPU_RBAR_XN_Msk (01UL ) 1461 #define MPU_RLAR_LIMIT_Pos 5U 1462 #define MPU_RLAR_LIMIT_Msk (0x7FFFFFFUL << MPU_RLAR_LIMIT_Pos) 1464 #define MPU_RLAR_AttrIndx_Pos 1U 1465 #define MPU_RLAR_AttrIndx_Msk (0x7UL << MPU_RLAR_AttrIndx_Pos) 1467 #define MPU_RLAR_EN_Pos 0U 1468 #define MPU_RLAR_EN_Msk (1UL ) 1471 #define MPU_MAIR0_Attr3_Pos 24U 1472 #define MPU_MAIR0_Attr3_Msk (0xFFUL << MPU_MAIR0_Attr3_Pos) 1474 #define MPU_MAIR0_Attr2_Pos 16U 1475 #define MPU_MAIR0_Attr2_Msk (0xFFUL << MPU_MAIR0_Attr2_Pos) 1477 #define MPU_MAIR0_Attr1_Pos 8U 1478 #define MPU_MAIR0_Attr1_Msk (0xFFUL << MPU_MAIR0_Attr1_Pos) 1480 #define MPU_MAIR0_Attr0_Pos 0U 1481 #define MPU_MAIR0_Attr0_Msk (0xFFUL ) 1484 #define MPU_MAIR1_Attr7_Pos 24U 1485 #define MPU_MAIR1_Attr7_Msk (0xFFUL << MPU_MAIR1_Attr7_Pos) 1487 #define MPU_MAIR1_Attr6_Pos 16U 1488 #define MPU_MAIR1_Attr6_Msk (0xFFUL << MPU_MAIR1_Attr6_Pos) 1490 #define MPU_MAIR1_Attr5_Pos 8U 1491 #define MPU_MAIR1_Attr5_Msk (0xFFUL << MPU_MAIR1_Attr5_Pos) 1493 #define MPU_MAIR1_Attr4_Pos 0U 1494 #define MPU_MAIR1_Attr4_Msk (0xFFUL ) 1500 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 1513 __IOM uint32_t CTRL;
1515 #if defined (__SAUREGION_PRESENT) && (__SAUREGION_PRESENT == 1U) 1517 __IOM uint32_t RBAR;
1518 __IOM uint32_t RLAR;
1520 uint32_t RESERVED0[3];
1522 __IOM uint32_t SFSR;
1523 __IOM uint32_t SFAR;
1527 #define SAU_CTRL_ALLNS_Pos 1U 1528 #define SAU_CTRL_ALLNS_Msk (1UL << SAU_CTRL_ALLNS_Pos) 1530 #define SAU_CTRL_ENABLE_Pos 0U 1531 #define SAU_CTRL_ENABLE_Msk (1UL ) 1534 #define SAU_TYPE_SREGION_Pos 0U 1535 #define SAU_TYPE_SREGION_Msk (0xFFUL ) 1537 #if defined (__SAUREGION_PRESENT) && (__SAUREGION_PRESENT == 1U) 1539 #define SAU_RNR_REGION_Pos 0U 1540 #define SAU_RNR_REGION_Msk (0xFFUL ) 1543 #define SAU_RBAR_BADDR_Pos 5U 1544 #define SAU_RBAR_BADDR_Msk (0x7FFFFFFUL << SAU_RBAR_BADDR_Pos) 1547 #define SAU_RLAR_LADDR_Pos 5U 1548 #define SAU_RLAR_LADDR_Msk (0x7FFFFFFUL << SAU_RLAR_LADDR_Pos) 1550 #define SAU_RLAR_NSC_Pos 1U 1551 #define SAU_RLAR_NSC_Msk (1UL << SAU_RLAR_NSC_Pos) 1553 #define SAU_RLAR_ENABLE_Pos 0U 1554 #define SAU_RLAR_ENABLE_Msk (1UL ) 1559 #define SAU_SFSR_LSERR_Pos 7U 1560 #define SAU_SFSR_LSERR_Msk (1UL << SAU_SFSR_LSERR_Pos) 1562 #define SAU_SFSR_SFARVALID_Pos 6U 1563 #define SAU_SFSR_SFARVALID_Msk (1UL << SAU_SFSR_SFARVALID_Pos) 1565 #define SAU_SFSR_LSPERR_Pos 5U 1566 #define SAU_SFSR_LSPERR_Msk (1UL << SAU_SFSR_LSPERR_Pos) 1568 #define SAU_SFSR_INVTRAN_Pos 4U 1569 #define SAU_SFSR_INVTRAN_Msk (1UL << SAU_SFSR_INVTRAN_Pos) 1571 #define SAU_SFSR_AUVIOL_Pos 3U 1572 #define SAU_SFSR_AUVIOL_Msk (1UL << SAU_SFSR_AUVIOL_Pos) 1574 #define SAU_SFSR_INVER_Pos 2U 1575 #define SAU_SFSR_INVER_Msk (1UL << SAU_SFSR_INVER_Pos) 1577 #define SAU_SFSR_INVIS_Pos 1U 1578 #define SAU_SFSR_INVIS_Msk (1UL << SAU_SFSR_INVIS_Pos) 1580 #define SAU_SFSR_INVEP_Pos 0U 1581 #define SAU_SFSR_INVEP_Msk (1UL ) 1599 uint32_t RESERVED0[1U];
1600 __IOM uint32_t FPCCR;
1601 __IOM uint32_t FPCAR;
1602 __IOM uint32_t FPDSCR;
1603 __IM uint32_t MVFR0;
1604 __IM uint32_t MVFR1;
1605 __IM uint32_t MVFR2;
1609 #define FPU_FPCCR_ASPEN_Pos 31U 1610 #define FPU_FPCCR_ASPEN_Msk (1UL << FPU_FPCCR_ASPEN_Pos) 1612 #define FPU_FPCCR_LSPEN_Pos 30U 1613 #define FPU_FPCCR_LSPEN_Msk (1UL << FPU_FPCCR_LSPEN_Pos) 1615 #define FPU_FPCCR_LSPENS_Pos 29U 1616 #define FPU_FPCCR_LSPENS_Msk (1UL << FPU_FPCCR_LSPENS_Pos) 1618 #define FPU_FPCCR_CLRONRET_Pos 28U 1619 #define FPU_FPCCR_CLRONRET_Msk (1UL << FPU_FPCCR_CLRONRET_Pos) 1621 #define FPU_FPCCR_CLRONRETS_Pos 27U 1622 #define FPU_FPCCR_CLRONRETS_Msk (1UL << FPU_FPCCR_CLRONRETS_Pos) 1624 #define FPU_FPCCR_TS_Pos 26U 1625 #define FPU_FPCCR_TS_Msk (1UL << FPU_FPCCR_TS_Pos) 1627 #define FPU_FPCCR_UFRDY_Pos 10U 1628 #define FPU_FPCCR_UFRDY_Msk (1UL << FPU_FPCCR_UFRDY_Pos) 1630 #define FPU_FPCCR_SPLIMVIOL_Pos 9U 1631 #define FPU_FPCCR_SPLIMVIOL_Msk (1UL << FPU_FPCCR_SPLIMVIOL_Pos) 1633 #define FPU_FPCCR_MONRDY_Pos 8U 1634 #define FPU_FPCCR_MONRDY_Msk (1UL << FPU_FPCCR_MONRDY_Pos) 1636 #define FPU_FPCCR_SFRDY_Pos 7U 1637 #define FPU_FPCCR_SFRDY_Msk (1UL << FPU_FPCCR_SFRDY_Pos) 1639 #define FPU_FPCCR_BFRDY_Pos 6U 1640 #define FPU_FPCCR_BFRDY_Msk (1UL << FPU_FPCCR_BFRDY_Pos) 1642 #define FPU_FPCCR_MMRDY_Pos 5U 1643 #define FPU_FPCCR_MMRDY_Msk (1UL << FPU_FPCCR_MMRDY_Pos) 1645 #define FPU_FPCCR_HFRDY_Pos 4U 1646 #define FPU_FPCCR_HFRDY_Msk (1UL << FPU_FPCCR_HFRDY_Pos) 1648 #define FPU_FPCCR_THREAD_Pos 3U 1649 #define FPU_FPCCR_THREAD_Msk (1UL << FPU_FPCCR_THREAD_Pos) 1651 #define FPU_FPCCR_S_Pos 2U 1652 #define FPU_FPCCR_S_Msk (1UL << FPU_FPCCR_S_Pos) 1654 #define FPU_FPCCR_USER_Pos 1U 1655 #define FPU_FPCCR_USER_Msk (1UL << FPU_FPCCR_USER_Pos) 1657 #define FPU_FPCCR_LSPACT_Pos 0U 1658 #define FPU_FPCCR_LSPACT_Msk (1UL ) 1661 #define FPU_FPCAR_ADDRESS_Pos 3U 1662 #define FPU_FPCAR_ADDRESS_Msk (0x1FFFFFFFUL << FPU_FPCAR_ADDRESS_Pos) 1665 #define FPU_FPDSCR_AHP_Pos 26U 1666 #define FPU_FPDSCR_AHP_Msk (1UL << FPU_FPDSCR_AHP_Pos) 1668 #define FPU_FPDSCR_DN_Pos 25U 1669 #define FPU_FPDSCR_DN_Msk (1UL << FPU_FPDSCR_DN_Pos) 1671 #define FPU_FPDSCR_FZ_Pos 24U 1672 #define FPU_FPDSCR_FZ_Msk (1UL << FPU_FPDSCR_FZ_Pos) 1674 #define FPU_FPDSCR_RMode_Pos 22U 1675 #define FPU_FPDSCR_RMode_Msk (3UL << FPU_FPDSCR_RMode_Pos) 1678 #define FPU_MVFR0_FP_rounding_modes_Pos 28U 1679 #define FPU_MVFR0_FP_rounding_modes_Msk (0xFUL << FPU_MVFR0_FP_rounding_modes_Pos) 1681 #define FPU_MVFR0_Short_vectors_Pos 24U 1682 #define FPU_MVFR0_Short_vectors_Msk (0xFUL << FPU_MVFR0_Short_vectors_Pos) 1684 #define FPU_MVFR0_Square_root_Pos 20U 1685 #define FPU_MVFR0_Square_root_Msk (0xFUL << FPU_MVFR0_Square_root_Pos) 1687 #define FPU_MVFR0_Divide_Pos 16U 1688 #define FPU_MVFR0_Divide_Msk (0xFUL << FPU_MVFR0_Divide_Pos) 1690 #define FPU_MVFR0_FP_excep_trapping_Pos 12U 1691 #define FPU_MVFR0_FP_excep_trapping_Msk (0xFUL << FPU_MVFR0_FP_excep_trapping_Pos) 1693 #define FPU_MVFR0_Double_precision_Pos 8U 1694 #define FPU_MVFR0_Double_precision_Msk (0xFUL << FPU_MVFR0_Double_precision_Pos) 1696 #define FPU_MVFR0_Single_precision_Pos 4U 1697 #define FPU_MVFR0_Single_precision_Msk (0xFUL << FPU_MVFR0_Single_precision_Pos) 1699 #define FPU_MVFR0_A_SIMD_registers_Pos 0U 1700 #define FPU_MVFR0_A_SIMD_registers_Msk (0xFUL ) 1703 #define FPU_MVFR1_FP_fused_MAC_Pos 28U 1704 #define FPU_MVFR1_FP_fused_MAC_Msk (0xFUL << FPU_MVFR1_FP_fused_MAC_Pos) 1706 #define FPU_MVFR1_FP_HPFP_Pos 24U 1707 #define FPU_MVFR1_FP_HPFP_Msk (0xFUL << FPU_MVFR1_FP_HPFP_Pos) 1709 #define FPU_MVFR1_D_NaN_mode_Pos 4U 1710 #define FPU_MVFR1_D_NaN_mode_Msk (0xFUL << FPU_MVFR1_D_NaN_mode_Pos) 1712 #define FPU_MVFR1_FtZ_mode_Pos 0U 1713 #define FPU_MVFR1_FtZ_mode_Msk (0xFUL ) 1716 #define FPU_MVFR2_FPMisc_Pos 4U 1717 #define FPU_MVFR2_FPMisc_Msk (0xFUL << FPU_MVFR2_FPMisc_Pos) 1734 __IOM uint32_t DHCSR;
1735 __OM uint32_t DCRSR;
1736 __IOM uint32_t DCRDR;
1737 __IOM uint32_t DEMCR;
1738 uint32_t RESERVED0[1U];
1739 __IOM uint32_t DAUTHCTRL;
1740 __IOM uint32_t DSCSR;
1744 #define CoreDebug_DHCSR_DBGKEY_Pos 16U 1745 #define CoreDebug_DHCSR_DBGKEY_Msk (0xFFFFUL << CoreDebug_DHCSR_DBGKEY_Pos) 1747 #define CoreDebug_DHCSR_S_RESTART_ST_Pos 26U 1748 #define CoreDebug_DHCSR_S_RESTART_ST_Msk (1UL << CoreDebug_DHCSR_S_RESTART_ST_Pos) 1750 #define CoreDebug_DHCSR_S_RESET_ST_Pos 25U 1751 #define CoreDebug_DHCSR_S_RESET_ST_Msk (1UL << CoreDebug_DHCSR_S_RESET_ST_Pos) 1753 #define CoreDebug_DHCSR_S_RETIRE_ST_Pos 24U 1754 #define CoreDebug_DHCSR_S_RETIRE_ST_Msk (1UL << CoreDebug_DHCSR_S_RETIRE_ST_Pos) 1756 #define CoreDebug_DHCSR_S_LOCKUP_Pos 19U 1757 #define CoreDebug_DHCSR_S_LOCKUP_Msk (1UL << CoreDebug_DHCSR_S_LOCKUP_Pos) 1759 #define CoreDebug_DHCSR_S_SLEEP_Pos 18U 1760 #define CoreDebug_DHCSR_S_SLEEP_Msk (1UL << CoreDebug_DHCSR_S_SLEEP_Pos) 1762 #define CoreDebug_DHCSR_S_HALT_Pos 17U 1763 #define CoreDebug_DHCSR_S_HALT_Msk (1UL << CoreDebug_DHCSR_S_HALT_Pos) 1765 #define CoreDebug_DHCSR_S_REGRDY_Pos 16U 1766 #define CoreDebug_DHCSR_S_REGRDY_Msk (1UL << CoreDebug_DHCSR_S_REGRDY_Pos) 1768 #define CoreDebug_DHCSR_C_SNAPSTALL_Pos 5U 1769 #define CoreDebug_DHCSR_C_SNAPSTALL_Msk (1UL << CoreDebug_DHCSR_C_SNAPSTALL_Pos) 1771 #define CoreDebug_DHCSR_C_MASKINTS_Pos 3U 1772 #define CoreDebug_DHCSR_C_MASKINTS_Msk (1UL << CoreDebug_DHCSR_C_MASKINTS_Pos) 1774 #define CoreDebug_DHCSR_C_STEP_Pos 2U 1775 #define CoreDebug_DHCSR_C_STEP_Msk (1UL << CoreDebug_DHCSR_C_STEP_Pos) 1777 #define CoreDebug_DHCSR_C_HALT_Pos 1U 1778 #define CoreDebug_DHCSR_C_HALT_Msk (1UL << CoreDebug_DHCSR_C_HALT_Pos) 1780 #define CoreDebug_DHCSR_C_DEBUGEN_Pos 0U 1781 #define CoreDebug_DHCSR_C_DEBUGEN_Msk (1UL ) 1784 #define CoreDebug_DCRSR_REGWnR_Pos 16U 1785 #define CoreDebug_DCRSR_REGWnR_Msk (1UL << CoreDebug_DCRSR_REGWnR_Pos) 1787 #define CoreDebug_DCRSR_REGSEL_Pos 0U 1788 #define CoreDebug_DCRSR_REGSEL_Msk (0x1FUL ) 1791 #define CoreDebug_DEMCR_TRCENA_Pos 24U 1792 #define CoreDebug_DEMCR_TRCENA_Msk (1UL << CoreDebug_DEMCR_TRCENA_Pos) 1794 #define CoreDebug_DEMCR_MON_REQ_Pos 19U 1795 #define CoreDebug_DEMCR_MON_REQ_Msk (1UL << CoreDebug_DEMCR_MON_REQ_Pos) 1797 #define CoreDebug_DEMCR_MON_STEP_Pos 18U 1798 #define CoreDebug_DEMCR_MON_STEP_Msk (1UL << CoreDebug_DEMCR_MON_STEP_Pos) 1800 #define CoreDebug_DEMCR_MON_PEND_Pos 17U 1801 #define CoreDebug_DEMCR_MON_PEND_Msk (1UL << CoreDebug_DEMCR_MON_PEND_Pos) 1803 #define CoreDebug_DEMCR_MON_EN_Pos 16U 1804 #define CoreDebug_DEMCR_MON_EN_Msk (1UL << CoreDebug_DEMCR_MON_EN_Pos) 1806 #define CoreDebug_DEMCR_VC_HARDERR_Pos 10U 1807 #define CoreDebug_DEMCR_VC_HARDERR_Msk (1UL << CoreDebug_DEMCR_VC_HARDERR_Pos) 1809 #define CoreDebug_DEMCR_VC_INTERR_Pos 9U 1810 #define CoreDebug_DEMCR_VC_INTERR_Msk (1UL << CoreDebug_DEMCR_VC_INTERR_Pos) 1812 #define CoreDebug_DEMCR_VC_BUSERR_Pos 8U 1813 #define CoreDebug_DEMCR_VC_BUSERR_Msk (1UL << CoreDebug_DEMCR_VC_BUSERR_Pos) 1815 #define CoreDebug_DEMCR_VC_STATERR_Pos 7U 1816 #define CoreDebug_DEMCR_VC_STATERR_Msk (1UL << CoreDebug_DEMCR_VC_STATERR_Pos) 1818 #define CoreDebug_DEMCR_VC_CHKERR_Pos 6U 1819 #define CoreDebug_DEMCR_VC_CHKERR_Msk (1UL << CoreDebug_DEMCR_VC_CHKERR_Pos) 1821 #define CoreDebug_DEMCR_VC_NOCPERR_Pos 5U 1822 #define CoreDebug_DEMCR_VC_NOCPERR_Msk (1UL << CoreDebug_DEMCR_VC_NOCPERR_Pos) 1824 #define CoreDebug_DEMCR_VC_MMERR_Pos 4U 1825 #define CoreDebug_DEMCR_VC_MMERR_Msk (1UL << CoreDebug_DEMCR_VC_MMERR_Pos) 1827 #define CoreDebug_DEMCR_VC_CORERESET_Pos 0U 1828 #define CoreDebug_DEMCR_VC_CORERESET_Msk (1UL ) 1831 #define CoreDebug_DAUTHCTRL_INTSPNIDEN_Pos 3U 1832 #define CoreDebug_DAUTHCTRL_INTSPNIDEN_Msk (1UL << CoreDebug_DAUTHCTRL_INTSPNIDEN_Pos) 1834 #define CoreDebug_DAUTHCTRL_SPNIDENSEL_Pos 2U 1835 #define CoreDebug_DAUTHCTRL_SPNIDENSEL_Msk (1UL << CoreDebug_DAUTHCTRL_SPNIDENSEL_Pos) 1837 #define CoreDebug_DAUTHCTRL_INTSPIDEN_Pos 1U 1838 #define CoreDebug_DAUTHCTRL_INTSPIDEN_Msk (1UL << CoreDebug_DAUTHCTRL_INTSPIDEN_Pos) 1840 #define CoreDebug_DAUTHCTRL_SPIDENSEL_Pos 0U 1841 #define CoreDebug_DAUTHCTRL_SPIDENSEL_Msk (1UL ) 1844 #define CoreDebug_DSCSR_CDS_Pos 16U 1845 #define CoreDebug_DSCSR_CDS_Msk (1UL << CoreDebug_DSCSR_CDS_Pos) 1847 #define CoreDebug_DSCSR_SBRSEL_Pos 1U 1848 #define CoreDebug_DSCSR_SBRSEL_Msk (1UL << CoreDebug_DSCSR_SBRSEL_Pos) 1850 #define CoreDebug_DSCSR_SBRSELEN_Pos 0U 1851 #define CoreDebug_DSCSR_SBRSELEN_Msk (1UL ) 1868 __IOM uint32_t DHCSR;
1869 __OM uint32_t DCRSR;
1870 __IOM uint32_t DCRDR;
1871 __IOM uint32_t DEMCR;
1872 uint32_t RESERVED0[1U];
1873 __IOM uint32_t DAUTHCTRL;
1874 __IOM uint32_t DSCSR;
1878 #define DCB_DHCSR_DBGKEY_Pos 16U 1879 #define DCB_DHCSR_DBGKEY_Msk (0xFFFFUL << DCB_DHCSR_DBGKEY_Pos) 1881 #define DCB_DHCSR_S_RESTART_ST_Pos 26U 1882 #define DCB_DHCSR_S_RESTART_ST_Msk (0x1UL << DCB_DHCSR_S_RESTART_ST_Pos) 1884 #define DCB_DHCSR_S_RESET_ST_Pos 25U 1885 #define DCB_DHCSR_S_RESET_ST_Msk (0x1UL << DCB_DHCSR_S_RESET_ST_Pos) 1887 #define DCB_DHCSR_S_RETIRE_ST_Pos 24U 1888 #define DCB_DHCSR_S_RETIRE_ST_Msk (0x1UL << DCB_DHCSR_S_RETIRE_ST_Pos) 1890 #define DCB_DHCSR_S_SDE_Pos 20U 1891 #define DCB_DHCSR_S_SDE_Msk (0x1UL << DCB_DHCSR_S_SDE_Pos) 1893 #define DCB_DHCSR_S_LOCKUP_Pos 19U 1894 #define DCB_DHCSR_S_LOCKUP_Msk (0x1UL << DCB_DHCSR_S_LOCKUP_Pos) 1896 #define DCB_DHCSR_S_SLEEP_Pos 18U 1897 #define DCB_DHCSR_S_SLEEP_Msk (0x1UL << DCB_DHCSR_S_SLEEP_Pos) 1899 #define DCB_DHCSR_S_HALT_Pos 17U 1900 #define DCB_DHCSR_S_HALT_Msk (0x1UL << DCB_DHCSR_S_HALT_Pos) 1902 #define DCB_DHCSR_S_REGRDY_Pos 16U 1903 #define DCB_DHCSR_S_REGRDY_Msk (0x1UL << DCB_DHCSR_S_REGRDY_Pos) 1905 #define DCB_DHCSR_C_SNAPSTALL_Pos 5U 1906 #define DCB_DHCSR_C_SNAPSTALL_Msk (0x1UL << DCB_DHCSR_C_SNAPSTALL_Pos) 1908 #define DCB_DHCSR_C_MASKINTS_Pos 3U 1909 #define DCB_DHCSR_C_MASKINTS_Msk (0x1UL << DCB_DHCSR_C_MASKINTS_Pos) 1911 #define DCB_DHCSR_C_STEP_Pos 2U 1912 #define DCB_DHCSR_C_STEP_Msk (0x1UL << DCB_DHCSR_C_STEP_Pos) 1914 #define DCB_DHCSR_C_HALT_Pos 1U 1915 #define DCB_DHCSR_C_HALT_Msk (0x1UL << DCB_DHCSR_C_HALT_Pos) 1917 #define DCB_DHCSR_C_DEBUGEN_Pos 0U 1918 #define DCB_DHCSR_C_DEBUGEN_Msk (0x1UL ) 1921 #define DCB_DCRSR_REGWnR_Pos 16U 1922 #define DCB_DCRSR_REGWnR_Msk (0x1UL << DCB_DCRSR_REGWnR_Pos) 1924 #define DCB_DCRSR_REGSEL_Pos 0U 1925 #define DCB_DCRSR_REGSEL_Msk (0x7FUL ) 1928 #define DCB_DCRDR_DBGTMP_Pos 0U 1929 #define DCB_DCRDR_DBGTMP_Msk (0xFFFFFFFFUL ) 1932 #define DCB_DEMCR_TRCENA_Pos 24U 1933 #define DCB_DEMCR_TRCENA_Msk (0x1UL << DCB_DEMCR_TRCENA_Pos) 1935 #define DCB_DEMCR_MONPRKEY_Pos 23U 1936 #define DCB_DEMCR_MONPRKEY_Msk (0x1UL << DCB_DEMCR_MONPRKEY_Pos) 1938 #define DCB_DEMCR_UMON_EN_Pos 21U 1939 #define DCB_DEMCR_UMON_EN_Msk (0x1UL << DCB_DEMCR_UMON_EN_Pos) 1941 #define DCB_DEMCR_SDME_Pos 20U 1942 #define DCB_DEMCR_SDME_Msk (0x1UL << DCB_DEMCR_SDME_Pos) 1944 #define DCB_DEMCR_MON_REQ_Pos 19U 1945 #define DCB_DEMCR_MON_REQ_Msk (0x1UL << DCB_DEMCR_MON_REQ_Pos) 1947 #define DCB_DEMCR_MON_STEP_Pos 18U 1948 #define DCB_DEMCR_MON_STEP_Msk (0x1UL << DCB_DEMCR_MON_STEP_Pos) 1950 #define DCB_DEMCR_MON_PEND_Pos 17U 1951 #define DCB_DEMCR_MON_PEND_Msk (0x1UL << DCB_DEMCR_MON_PEND_Pos) 1953 #define DCB_DEMCR_MON_EN_Pos 16U 1954 #define DCB_DEMCR_MON_EN_Msk (0x1UL << DCB_DEMCR_MON_EN_Pos) 1956 #define DCB_DEMCR_VC_SFERR_Pos 11U 1957 #define DCB_DEMCR_VC_SFERR_Msk (0x1UL << DCB_DEMCR_VC_SFERR_Pos) 1959 #define DCB_DEMCR_VC_HARDERR_Pos 10U 1960 #define DCB_DEMCR_VC_HARDERR_Msk (0x1UL << DCB_DEMCR_VC_HARDERR_Pos) 1962 #define DCB_DEMCR_VC_INTERR_Pos 9U 1963 #define DCB_DEMCR_VC_INTERR_Msk (0x1UL << DCB_DEMCR_VC_INTERR_Pos) 1965 #define DCB_DEMCR_VC_BUSERR_Pos 8U 1966 #define DCB_DEMCR_VC_BUSERR_Msk (0x1UL << DCB_DEMCR_VC_BUSERR_Pos) 1968 #define DCB_DEMCR_VC_STATERR_Pos 7U 1969 #define DCB_DEMCR_VC_STATERR_Msk (0x1UL << DCB_DEMCR_VC_STATERR_Pos) 1971 #define DCB_DEMCR_VC_CHKERR_Pos 6U 1972 #define DCB_DEMCR_VC_CHKERR_Msk (0x1UL << DCB_DEMCR_VC_CHKERR_Pos) 1974 #define DCB_DEMCR_VC_NOCPERR_Pos 5U 1975 #define DCB_DEMCR_VC_NOCPERR_Msk (0x1UL << DCB_DEMCR_VC_NOCPERR_Pos) 1977 #define DCB_DEMCR_VC_MMERR_Pos 4U 1978 #define DCB_DEMCR_VC_MMERR_Msk (0x1UL << DCB_DEMCR_VC_MMERR_Pos) 1980 #define DCB_DEMCR_VC_CORERESET_Pos 0U 1981 #define DCB_DEMCR_VC_CORERESET_Msk (0x1UL ) 1984 #define DCB_DAUTHCTRL_INTSPNIDEN_Pos 3U 1985 #define DCB_DAUTHCTRL_INTSPNIDEN_Msk (0x1UL << DCB_DAUTHCTRL_INTSPNIDEN_Pos) 1987 #define DCB_DAUTHCTRL_SPNIDENSEL_Pos 2U 1988 #define DCB_DAUTHCTRL_SPNIDENSEL_Msk (0x1UL << DCB_DAUTHCTRL_SPNIDENSEL_Pos) 1990 #define DCB_DAUTHCTRL_INTSPIDEN_Pos 1U 1991 #define DCB_DAUTHCTRL_INTSPIDEN_Msk (0x1UL << DCB_DAUTHCTRL_INTSPIDEN_Pos) 1993 #define DCB_DAUTHCTRL_SPIDENSEL_Pos 0U 1994 #define DCB_DAUTHCTRL_SPIDENSEL_Msk (0x1UL ) 1997 #define DCB_DSCSR_CDSKEY_Pos 17U 1998 #define DCB_DSCSR_CDSKEY_Msk (0x1UL << DCB_DSCSR_CDSKEY_Pos) 2000 #define DCB_DSCSR_CDS_Pos 16U 2001 #define DCB_DSCSR_CDS_Msk (0x1UL << DCB_DSCSR_CDS_Pos) 2003 #define DCB_DSCSR_SBRSEL_Pos 1U 2004 #define DCB_DSCSR_SBRSEL_Msk (0x1UL << DCB_DSCSR_SBRSEL_Pos) 2006 #define DCB_DSCSR_SBRSELEN_Pos 0U 2007 #define DCB_DSCSR_SBRSELEN_Msk (0x1UL ) 2027 __IM uint32_t DAUTHSTATUS;
2028 __IM uint32_t DDEVARCH;
2029 __IM uint32_t DDEVTYPE;
2033 #define DIB_DLAR_KEY_Pos 0U 2034 #define DIB_DLAR_KEY_Msk (0xFFFFFFFFUL ) 2037 #define DIB_DLSR_nTT_Pos 2U 2038 #define DIB_DLSR_nTT_Msk (0x1UL << DIB_DLSR_nTT_Pos ) 2040 #define DIB_DLSR_SLK_Pos 1U 2041 #define DIB_DLSR_SLK_Msk (0x1UL << DIB_DLSR_SLK_Pos ) 2043 #define DIB_DLSR_SLI_Pos 0U 2044 #define DIB_DLSR_SLI_Msk (0x1UL ) 2047 #define DIB_DAUTHSTATUS_SNID_Pos 6U 2048 #define DIB_DAUTHSTATUS_SNID_Msk (0x3UL << DIB_DAUTHSTATUS_SNID_Pos ) 2050 #define DIB_DAUTHSTATUS_SID_Pos 4U 2051 #define DIB_DAUTHSTATUS_SID_Msk (0x3UL << DIB_DAUTHSTATUS_SID_Pos ) 2053 #define DIB_DAUTHSTATUS_NSNID_Pos 2U 2054 #define DIB_DAUTHSTATUS_NSNID_Msk (0x3UL << DIB_DAUTHSTATUS_NSNID_Pos ) 2056 #define DIB_DAUTHSTATUS_NSID_Pos 0U 2057 #define DIB_DAUTHSTATUS_NSID_Msk (0x3UL ) 2060 #define DIB_DDEVARCH_ARCHITECT_Pos 21U 2061 #define DIB_DDEVARCH_ARCHITECT_Msk (0x7FFUL << DIB_DDEVARCH_ARCHITECT_Pos ) 2063 #define DIB_DDEVARCH_PRESENT_Pos 20U 2064 #define DIB_DDEVARCH_PRESENT_Msk (0x1FUL << DIB_DDEVARCH_PRESENT_Pos ) 2066 #define DIB_DDEVARCH_REVISION_Pos 16U 2067 #define DIB_DDEVARCH_REVISION_Msk (0xFUL << DIB_DDEVARCH_REVISION_Pos ) 2069 #define DIB_DDEVARCH_ARCHVER_Pos 12U 2070 #define DIB_DDEVARCH_ARCHVER_Msk (0xFUL << DIB_DDEVARCH_ARCHVER_Pos ) 2072 #define DIB_DDEVARCH_ARCHPART_Pos 0U 2073 #define DIB_DDEVARCH_ARCHPART_Msk (0xFFFUL ) 2076 #define DIB_DDEVTYPE_SUB_Pos 4U 2077 #define DIB_DDEVTYPE_SUB_Msk (0xFUL << DIB_DDEVTYPE_SUB_Pos ) 2079 #define DIB_DDEVTYPE_MAJOR_Pos 0U 2080 #define DIB_DDEVTYPE_MAJOR_Msk (0xFUL ) 2099 #define _VAL2FLD(field, value) (((uint32_t)(value) << field ## _Pos) & field ## _Msk) 2107 #define _FLD2VAL(field, value) (((uint32_t)(value) & field ## _Msk) >> field ## _Pos) 2120 #define SCS_BASE (0xE000E000UL) 2121 #define ITM_BASE (0xE0000000UL) 2122 #define DWT_BASE (0xE0001000UL) 2123 #define TPI_BASE (0xE0040000UL) 2124 #define CoreDebug_BASE (0xE000EDF0UL) 2125 #define DCB_BASE (0xE000EDF0UL) 2126 #define DIB_BASE (0xE000EFB0UL) 2127 #define SysTick_BASE (SCS_BASE + 0x0010UL) 2128 #define NVIC_BASE (SCS_BASE + 0x0100UL) 2129 #define SCB_BASE (SCS_BASE + 0x0D00UL) 2131 #define SCnSCB ((SCnSCB_Type *) SCS_BASE ) 2132 #define SCB ((SCB_Type *) SCB_BASE ) 2133 #define SysTick ((SysTick_Type *) SysTick_BASE ) 2134 #define NVIC ((NVIC_Type *) NVIC_BASE ) 2135 #define ITM ((ITM_Type *) ITM_BASE ) 2136 #define DWT ((DWT_Type *) DWT_BASE ) 2137 #define TPI ((TPI_Type *) TPI_BASE ) 2138 #define CoreDebug ((CoreDebug_Type *) CoreDebug_BASE ) 2139 #define DCB ((DCB_Type *) DCB_BASE ) 2140 #define DIB ((DIB_Type *) DIB_BASE ) 2142 #if defined (__MPU_PRESENT) && (__MPU_PRESENT == 1U) 2143 #define MPU_BASE (SCS_BASE + 0x0D90UL) 2144 #define MPU ((MPU_Type *) MPU_BASE ) 2147 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 2148 #define SAU_BASE (SCS_BASE + 0x0DD0UL) 2149 #define SAU ((SAU_Type *) SAU_BASE ) 2152 #define FPU_BASE (SCS_BASE + 0x0F30UL) 2153 #define FPU ((FPU_Type *) FPU_BASE ) 2155 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 2156 #define SCS_BASE_NS (0xE002E000UL) 2157 #define CoreDebug_BASE_NS (0xE002EDF0UL) 2158 #define DCB_BASE_NS (0xE002EDF0UL) 2159 #define DIB_BASE_NS (0xE002EFB0UL) 2160 #define SysTick_BASE_NS (SCS_BASE_NS + 0x0010UL) 2161 #define NVIC_BASE_NS (SCS_BASE_NS + 0x0100UL) 2162 #define SCB_BASE_NS (SCS_BASE_NS + 0x0D00UL) 2164 #define SCnSCB_NS ((SCnSCB_Type *) SCS_BASE_NS ) 2165 #define SCB_NS ((SCB_Type *) SCB_BASE_NS ) 2166 #define SysTick_NS ((SysTick_Type *) SysTick_BASE_NS ) 2167 #define NVIC_NS ((NVIC_Type *) NVIC_BASE_NS ) 2168 #define CoreDebug_NS ((CoreDebug_Type *) CoreDebug_BASE_NS) 2169 #define DCB_NS ((DCB_Type *) DCB_BASE_NS ) 2170 #define DIB_NS ((DIB_Type *) DIB_BASE_NS ) 2172 #if defined (__MPU_PRESENT) && (__MPU_PRESENT == 1U) 2173 #define MPU_BASE_NS (SCS_BASE_NS + 0x0D90UL) 2174 #define MPU_NS ((MPU_Type *) MPU_BASE_NS ) 2177 #define FPU_BASE_NS (SCS_BASE_NS + 0x0F30UL) 2178 #define FPU_NS ((FPU_Type *) FPU_BASE_NS ) 2207 #ifdef CMSIS_NVIC_VIRTUAL 2208 #ifndef CMSIS_NVIC_VIRTUAL_HEADER_FILE 2209 #define CMSIS_NVIC_VIRTUAL_HEADER_FILE "cmsis_nvic_virtual.h" 2211 #include CMSIS_NVIC_VIRTUAL_HEADER_FILE 2213 #define NVIC_SetPriorityGrouping __NVIC_SetPriorityGrouping 2214 #define NVIC_GetPriorityGrouping __NVIC_GetPriorityGrouping 2215 #define NVIC_EnableIRQ __NVIC_EnableIRQ 2216 #define NVIC_GetEnableIRQ __NVIC_GetEnableIRQ 2217 #define NVIC_DisableIRQ __NVIC_DisableIRQ 2218 #define NVIC_GetPendingIRQ __NVIC_GetPendingIRQ 2219 #define NVIC_SetPendingIRQ __NVIC_SetPendingIRQ 2220 #define NVIC_ClearPendingIRQ __NVIC_ClearPendingIRQ 2221 #define NVIC_GetActive __NVIC_GetActive 2222 #define NVIC_SetPriority __NVIC_SetPriority 2223 #define NVIC_GetPriority __NVIC_GetPriority 2224 #define NVIC_SystemReset __NVIC_SystemReset 2227 #ifdef CMSIS_VECTAB_VIRTUAL 2228 #ifndef CMSIS_VECTAB_VIRTUAL_HEADER_FILE 2229 #define CMSIS_VECTAB_VIRTUAL_HEADER_FILE "cmsis_vectab_virtual.h" 2231 #include CMSIS_VECTAB_VIRTUAL_HEADER_FILE 2233 #define NVIC_SetVector __NVIC_SetVector 2234 #define NVIC_GetVector __NVIC_GetVector 2237 #define NVIC_USER_IRQ_OFFSET 16 2243 #define FNC_RETURN (0xFEFFFFFFUL) 2246 #define EXC_RETURN_PREFIX (0xFF000000UL) 2247 #define EXC_RETURN_S (0x00000040UL) 2248 #define EXC_RETURN_DCRS (0x00000020UL) 2249 #define EXC_RETURN_FTYPE (0x00000010UL) 2250 #define EXC_RETURN_MODE (0x00000008UL) 2251 #define EXC_RETURN_SPSEL (0x00000004UL) 2252 #define EXC_RETURN_ES (0x00000001UL) 2255 #if defined (__FPU_PRESENT) && (__FPU_PRESENT == 1U) 2256 #define EXC_INTEGRITY_SIGNATURE (0xFEFA125AUL) 2258 #define EXC_INTEGRITY_SIGNATURE (0xFEFA125BUL) 2274 uint32_t PriorityGroupTmp = (PriorityGroup & (uint32_t)0x07UL);
2276 reg_value =
SCB->AIRCR;
2278 reg_value = (reg_value |
2281 SCB->AIRCR = reg_value;
2304 if ((int32_t)(IRQn) >= 0)
2307 NVIC->ISER[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
2323 if ((int32_t)(IRQn) >= 0)
2325 return((uint32_t)(((
NVIC->ISER[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2342 if ((int32_t)(IRQn) >= 0)
2344 NVIC->ICER[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
2361 if ((int32_t)(IRQn) >= 0)
2363 return((uint32_t)(((
NVIC->ISPR[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2380 if ((int32_t)(IRQn) >= 0)
2382 NVIC->ISPR[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
2395 if ((int32_t)(IRQn) >= 0)
2397 NVIC->ICPR[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
2412 if ((int32_t)(IRQn) >= 0)
2414 return((uint32_t)(((
NVIC->IABR[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2423 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 2434 if ((int32_t)(IRQn) >= 0)
2436 return((uint32_t)(((
NVIC->ITNS[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2455 if ((int32_t)(IRQn) >= 0)
2457 NVIC->ITNS[(((uint32_t)IRQn) >> 5UL)] |= ((uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL)));
2458 return((uint32_t)(((
NVIC->ITNS[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)
IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2477 if ((int32_t)(IRQn) >= 0)
2479 NVIC->ITNS[(((uint32_t)IRQn) >> 5UL)] &= ~((uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL)));
2480 return((uint32_t)(((
NVIC->ITNS[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)
IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2501 if ((int32_t)(IRQn) >= 0)
2503 NVIC->IPR[((uint32_t)IRQn)] = (uint8_t)((priority << (8U -
__NVIC_PRIO_BITS)) & (uint32_t)0xFFUL);
2507 SCB->SHPR[(((uint32_t)IRQn) & 0xFUL)-4UL] = (uint8_t)((priority << (8U -
__NVIC_PRIO_BITS)) & (uint32_t)0xFFUL);
2524 if ((int32_t)(IRQn) >= 0)
2548 uint32_t PriorityGroupTmp = (PriorityGroup & (uint32_t)0x07UL);
2549 uint32_t PreemptPriorityBits;
2550 uint32_t SubPriorityBits;
2553 SubPriorityBits = ((PriorityGroupTmp + (uint32_t)(
__NVIC_PRIO_BITS)) < (uint32_t)7UL) ? (uint32_t)0UL : (uint32_t)((PriorityGroupTmp - 7UL) + (uint32_t)(
__NVIC_PRIO_BITS));
2556 ((PreemptPriority & (uint32_t)((1UL << (PreemptPriorityBits)) - 1UL)) << SubPriorityBits) |
2557 ((SubPriority & (uint32_t)((1UL << (SubPriorityBits )) - 1UL)))
2575 uint32_t PriorityGroupTmp = (PriorityGroup & (uint32_t)0x07UL);
2576 uint32_t PreemptPriorityBits;
2577 uint32_t SubPriorityBits;
2580 SubPriorityBits = ((PriorityGroupTmp + (uint32_t)(
__NVIC_PRIO_BITS)) < (uint32_t)7UL) ? (uint32_t)0UL : (uint32_t)((PriorityGroupTmp - 7UL) + (uint32_t)(
__NVIC_PRIO_BITS));
2582 *pPreemptPriority = (Priority >> SubPriorityBits) & (uint32_t)((1UL << (PreemptPriorityBits)) - 1UL);
2583 *pSubPriority = (Priority ) & (uint32_t)((1UL << (SubPriorityBits )) - 1UL);
2598 uint32_t *vectors = (uint32_t *)
SCB->VTOR;
2614 uint32_t *vectors = (uint32_t *)
SCB->VTOR;
2638 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 2648 __STATIC_INLINE void TZ_NVIC_SetPriorityGrouping_NS(uint32_t PriorityGroup)
2651 uint32_t PriorityGroupTmp = (PriorityGroup & (uint32_t)0x07UL);
2653 reg_value = SCB_NS->AIRCR;
2655 reg_value = (reg_value |
2658 SCB_NS->AIRCR = reg_value;
2681 if ((int32_t)(IRQn) >= 0)
2683 NVIC_NS->ISER[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
2698 if ((int32_t)(IRQn) >= 0)
2700 return((uint32_t)(((NVIC_NS->ISER[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2717 if ((int32_t)(IRQn) >= 0)
2719 NVIC_NS->ICER[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
2734 if ((int32_t)(IRQn) >= 0)
2736 return((uint32_t)(((NVIC_NS->ISPR[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2753 if ((int32_t)(IRQn) >= 0)
2755 NVIC_NS->ISPR[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
2768 if ((int32_t)(IRQn) >= 0)
2770 NVIC_NS->ICPR[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
2785 if ((int32_t)(IRQn) >= 0)
2787 return((uint32_t)(((NVIC_NS->IABR[(((uint32_t)IRQn) >> 5UL)] & (1UL << (((uint32_t)IRQn) & 0x1FUL))) != 0UL) ? 1UL : 0UL));
2807 if ((int32_t)(IRQn) >= 0)
2809 NVIC_NS->IPR[((uint32_t)IRQn)] = (uint8_t)((priority << (8U -
__NVIC_PRIO_BITS)) & (uint32_t)0xFFUL);
2813 SCB_NS->SHPR[(((uint32_t)IRQn) & 0xFUL)-4UL] = (uint8_t)((priority << (8U -
__NVIC_PRIO_BITS)) & (uint32_t)0xFFUL);
2829 if ((int32_t)(IRQn) >= 0)
2831 return(((uint32_t)NVIC_NS->IPR[((uint32_t)IRQn)] >> (8U -
__NVIC_PRIO_BITS)));
2835 return(((uint32_t)SCB_NS->SHPR[(((uint32_t)IRQn) & 0xFUL)-4UL] >> (8U -
__NVIC_PRIO_BITS)));
2844 #if defined (__MPU_PRESENT) && (__MPU_PRESENT == 1U) 2891 #if ((defined (__ICACHE_PRESENT) && (__ICACHE_PRESENT == 1U)) || \ 2892 (defined (__DCACHE_PRESENT) && (__DCACHE_PRESENT == 1U))) 2893 #include "cachel1_armv7.h" 2905 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 2913 SAU->CTRL |= (SAU_CTRL_ENABLE_Msk);
2924 SAU->CTRL &= ~(SAU_CTRL_ENABLE_Msk);
2952 DCB->DAUTHCTRL = value;
2965 return (
DCB->DAUTHCTRL);
2969 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 2979 DCB_NS->DAUTHCTRL = value;
2992 return (DCB_NS->DAUTHCTRL);
3017 return (
DIB->DAUTHSTATUS);
3021 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 3029 return (DIB_NS->DAUTHSTATUS);
3046 #if defined (__Vendor_SysTickConfig) && (__Vendor_SysTickConfig == 0U) 3066 SysTick->LOAD = (uint32_t)(ticks - 1UL);
3075 #if defined (__ARM_FEATURE_CMSE) && (__ARM_FEATURE_CMSE == 3U) 3095 SysTick_NS->LOAD = (uint32_t)(ticks - 1UL);
3097 SysTick_NS->VAL = 0UL;
3120 #define ITM_RXBUFFER_EMPTY ((int32_t)0x5AA55AA5U) 3131 __STATIC_INLINE uint32_t ITM_SendChar (uint32_t ch) 3134 ((
ITM->TER & 1UL ) != 0UL) )
3136 while (
ITM->PORT[0U].u32 == 0UL)
3140 ITM->PORT[0U].u8 = (uint8_t)ch;
Structure type to access the Floating Point Unit (FPU).
Definition: core_armv81mml.h:2480
#define FPU_MVFR0_Single_precision_Msk
Definition: core_armv8mml.h:1697
#define ITM
Definition: core_armv8mml.h:2135
Structure type to access the Data Watchpoint and Trace Register (DWT).
Definition: core_armv81mml.h:1176
Structure type to access the Debug Identification Block Registers (DIB).
Definition: core_armv81mml.h:2983
#define SCB_AIRCR_PRIGROUP_Msk
Definition: core_armv8mml.h:627
#define DCB
Definition: core_armv8mml.h:2139
__STATIC_INLINE uint32_t __NVIC_GetEnableIRQ(IRQn_Type IRQn)
Get Interrupt Enable status.
Definition: core_armv81mml.h:3298
#define __NOP()
No Operation.
Definition: cmsis_gcc.h:903
#define __STATIC_INLINE
Definition: hw_types.h:57
#define FPU
Definition: core_armv8mml.h:2153
#define SCB_AIRCR_VECTKEY_Msk
Definition: core_armv8mml.h:612
#define SysTick
Definition: core_armv8mml.h:2133
#define ITM_RXBUFFER_EMPTY
Definition: core_armv8mml.h:3120
__STATIC_INLINE uint32_t __NVIC_GetVector(IRQn_Type IRQn)
Get Interrupt Vector.
Definition: core_armv81mml.h:3589
__STATIC_INLINE void __NVIC_EnableIRQ(IRQn_Type IRQn)
Enable Interrupt.
Definition: core_armv81mml.h:3279
__STATIC_INLINE uint32_t __NVIC_GetPendingIRQ(IRQn_Type IRQn)
Get Pending Interrupt.
Definition: core_armv81mml.h:3336
volatile int32_t ITM_RxBuffer
__STATIC_INLINE int32_t ITM_ReceiveChar(void)
ITM Receive Character.
Definition: core_armv81mml.h:4173
__STATIC_INLINE void DCB_SetAuthCtrl(uint32_t value)
Set Debug Authentication Control Register.
Definition: core_armv81mml.h:3969
#define FPU_MVFR0_Double_precision_Msk
Definition: core_armv8mml.h:1694
__STATIC_INLINE void __NVIC_SetPendingIRQ(IRQn_Type IRQn)
Set Pending Interrupt.
Definition: core_armv81mml.h:3355
Union type to access the Interrupt Program Status Register (IPSR).
Definition: core_armv81mml.h:367
Structure type to access the Trace Port Interface Register (TPI).
Definition: core_armv81mml.h:1362
__STATIC_INLINE int32_t ITM_CheckChar(void)
ITM Check Character.
Definition: core_armv81mml.h:4193
__STATIC_INLINE uint32_t SCB_GetFPUType(void)
get FPU type
Definition: core_armv81mml.h:3851
__STATIC_INLINE void NVIC_DecodePriority(uint32_t Priority, uint32_t PriorityGroup, uint32_t *const pPreemptPriority, uint32_t *const pSubPriority)
Decode Priority.
Definition: core_armv81mml.h:3550
#define NVIC
Definition: core_armv8mml.h:2134
__STATIC_FORCEINLINE void __DSB(void)
Data Synchronization Barrier.
Definition: cmsis_gcc.h:944
CMSIS Core(M) Version definitions.
IRQn
Definition: cc35xx.h:39
Definition: core_armv81mml.h:2621
Structure type to access the System Control Block (SCB).
Definition: core_armv81mml.h:511
#define ITM_TCR_ITMENA_Msk
Definition: core_armv8mml.h:1088
#define SCB
Definition: core_armv8mml.h:2132
Structure type to access the Instrumentation Trace Macrocell Register (ITM).
Definition: core_armv81mml.h:1075
#define __IOM
Definition: core_armv8mml.h:288
__STATIC_INLINE void __NVIC_SetVector(IRQn_Type IRQn, uint32_t vector)
Set Interrupt Vector.
Definition: core_armv81mml.h:3573
__STATIC_INLINE uint32_t __NVIC_GetPriorityGrouping(void)
Get Priority Grouping.
Definition: core_armv81mml.h:3267
__STATIC_INLINE void __NVIC_DisableIRQ(IRQn_Type IRQn)
Disable Interrupt.
Definition: core_armv81mml.h:3317
#define SCB_AIRCR_PRIGROUP_Pos
Definition: core_armv8mml.h:626
Structure type to access the System Control and ID Register not in the SCB.
Definition: core_armv81mml.h:998
Structure type to access the Nested Vectored Interrupt Controller (NVIC).
Definition: core_armv81mml.h:475
Structure type to access the System Timer (SysTick).
Definition: core_armv81mml.h:1023
#define SCB_AIRCR_VECTKEY_Pos
Definition: core_armv8mml.h:611
__STATIC_INLINE uint32_t __NVIC_GetActive(IRQn_Type IRQn)
Get Active Interrupt.
Definition: core_armv81mml.h:3387
#define __COMPILER_BARRIER()
Definition: cmsis_gcc.h:117
__STATIC_INLINE uint32_t DIB_GetAuthStatus(void)
Get Debug Authentication Status Register.
Definition: core_armv81mml.h:4036
#define NVIC_SetPriority
Definition: core_armv8mml.h:2222
__STATIC_INLINE void __NVIC_SetPriority(IRQn_Type IRQn, uint32_t priority)
Set Interrupt Priority.
Definition: core_armv81mml.h:3476
#define DIB
Definition: core_armv8mml.h:2140
#define SCB_AIRCR_SYSRESETREQ_Msk
Definition: core_armv8mml.h:633
CMSIS compiler generic header file.
Union type to access the Application Program Status Register (APSR).
Definition: core_armv81mml.h:328
#define SysTick_LOAD_RELOAD_Msk
Definition: core_armv8mml.h:984
#define __OM
Definition: core_armv8mml.h:287
__STATIC_INLINE void __NVIC_ClearPendingIRQ(IRQn_Type IRQn)
Clear Pending Interrupt.
Definition: core_armv81mml.h:3370
#define __IM
Definition: core_armv8mml.h:286
Structure type to access the Debug Control Block Registers (DCB).
Definition: core_armv81mml.h:2792
Union type to access the Control Registers (CONTROL).
Definition: core_armv81mml.h:436
#define __NVIC_PRIO_BITS
Definition: cc35xx.h:114
#define SysTick_CTRL_CLKSOURCE_Msk
Definition: core_armv8mml.h:974
#define SysTick_CTRL_ENABLE_Msk
Definition: core_armv8mml.h:980
#define NVIC_USER_IRQ_OFFSET
Definition: core_armv8mml.h:2237
__STATIC_INLINE uint32_t NVIC_EncodePriority(uint32_t PriorityGroup, uint32_t PreemptPriority, uint32_t SubPriority)
Encode Priority.
Definition: core_armv81mml.h:3523
__NO_RETURN __STATIC_INLINE void __NVIC_SystemReset(void)
System Reset.
Definition: core_armv81mml.h:3600
Union type to access the Special-Purpose Program Status Registers (xPSR).
Definition: core_armv81mml.h:385
__STATIC_INLINE uint32_t DCB_GetAuthCtrl(void)
Get Debug Authentication Control Register.
Definition: core_armv81mml.h:3984
__STATIC_FORCEINLINE void __ISB(void)
Instruction Synchronization Barrier.
Definition: cmsis_gcc.h:933
__STATIC_INLINE uint32_t __NVIC_GetPriority(IRQn_Type IRQn)
Get Interrupt Priority.
Definition: core_armv81mml.h:3498
#define SysTick_CTRL_TICKINT_Msk
Definition: core_armv8mml.h:977
__STATIC_INLINE void __NVIC_SetPriorityGrouping(uint32_t PriorityGroup)
Set Priority Grouping.
Definition: core_armv81mml.h:3248
#define __NO_RETURN
Definition: cmsis_gcc.h:53