CC35xxDriverLibrary
cmsis_version.h
Go to the documentation of this file.
1 /**************************************************************************/
7 /*
8  * Copyright (c) 2009-2019 ARM Limited. All rights reserved.
9  *
10  * SPDX-License-Identifier: Apache-2.0
11  *
12  * Licensed under the Apache License, Version 2.0 (the License); you may
13  * not use this file except in compliance with the License.
14  * You may obtain a copy of the License at
15  *
16  * www.apache.org/licenses/LICENSE-2.0
17  *
18  * Unless required by applicable law or agreed to in writing, software
19  * distributed under the License is distributed on an AS IS BASIS, WITHOUT
20  * WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
21  * See the License for the specific language governing permissions and
22  * limitations under the License.
23  */
24 
25 #if defined ( __ICCARM__ )
26  #pragma system_include /* treat file as system include file for MISRA check */
27 #elif defined (__clang__)
28  #pragma clang system_header /* treat file as system include file */
29 #endif
30 
31 #ifndef __CMSIS_VERSION_H
32 #define __CMSIS_VERSION_H
33 
34 /* CMSIS Version definitions */
35 #define __CM_CMSIS_VERSION_MAIN ( 5U)
36 #define __CM_CMSIS_VERSION_SUB ( 4U)
37 #define __CM_CMSIS_VERSION ((__CM_CMSIS_VERSION_MAIN << 16U) | \
38  __CM_CMSIS_VERSION_SUB )
39 #endif