======================================
SimpleLink Wi-Fi Toolbox Startup Guide
======================================

Overview
********

SimpleLink Wi-Fi Toolbox is a cross-platform software kit, that provides all required tools for fast and easy ramp-up of the CC33XX and CC35XX family of devices. SimpleLink Wi-Fi Toolbox provides as visual control as a command line control of the device.

Prerequisites
*************

* Windows 10 64Bit 
* Ubuntu 20 (or higher) 64 bit
* Latest Chrome Web Browser

SimpleLink Wi-Fi Toolbox Installation
*************************************

Windows
-------

Double click on the installer file and follow the setup steps.

.. note::
   It is recommended not to change "Installation Directory" from the default of ``c:\ti\simplelink_wifi_toolbox_x.x.x``

Ubuntu
------

In some cases, execution permission for the Ubuntu installer is required to be added to the installer. To add such permission open the terminal in the installer file location and type:

.. code-block:: bash

   chmod +x simplelink_wifi_toolbox_x_x_x.run

Execute the installer and follow the setup steps

.. code-block:: bash

   ./simplelink_wifi_toolbox_x_x_x.run

.. note:: 
   It is recommended not to change "Installation Directory" from the default of ``/home/${USER}/ti/simplelink_wifi_toolbox_x.x.x``

Run SimpleLink Wi-Fi Toolbox
****************************

Windows
-------

Open Windows File Explorer at ``c:\ti\simplelink_wifi_toolbox_x.x.x`` and double click on ``simplelink_wifi_toolbox_x_x_x.exe``. The terminal will be opened and a couple of seconds after Chrome will be opened on URL ``http://127.0.0.1:7777``.

.. note::
   If Chrome isn't the default browser on your PC we recommend closing opened default browser, opening  Chrome, and typing ``http://127.0.0.1:7777`` in the URL.


Ubuntu
------

Open Terminal and navigate into the SimpleLink Wi-Fi Toolbox installation folder 

.. code-block:: bash

   cd /home/${USER}/ti/simplelink_wifi_toolbox_x.x.x

Execute SimpleLink Wi-Fi Toolbox

.. code-block:: bash

   ./simplelink-wifi-toolbox

After a couple of seconds, the Chrome web browser should open on ``http://127.0.0.1:7777`` in the URL.

.. note:: 
   If Chrome isn't the default browser on your PC we recommend closing opened default browser, opening  Chrome, and typing ``http://127.0.0.1:7777`` in the URL.


SimpleLink Wi-Fi Toolbox Intro
******************************

The intro page of the toolbox displays all available tools for the current version.

For the first time / each new version, a user should get a force to reload message. To continue user should hit the key combination depending on OS / Web Browser. This step will insure that users align to the latest update of the SimpleLink Wi-Fi Toolbox interface (refer to :numref:`simplelink-wifi-toolbox_force_reload`).


.. _simplelink-wifi-toolbox_force_reload:

.. figure:: resources/simplelink-wifi-toolbox_force_reload.png
   :align: center
   :alt: simplelink-wifi-toolbox_force_reload
   :scale: 50

   SimpleLink Wi-Fi Toolbox hard Reload

After hitting the key combination for force reloading, a user should see the intro page of the SimpleLink Wi-Fi Toolbox (refer to :numref:`simplelink-wifi-toolbox_intro`).

.. _simplelink-wifi-toolbox_intro:

.. figure:: resources/activation-1.png
   :align: center
   :alt: simplelink-wifi-toolbox_intro
   :scale: 50

   SimpleLink Wi-Fi Toolbox intro page