CC35X1E
=======

The Programmer tool is used to activate and program the CC35XX family of devices. It is currently still in development
with new features being added.


.. attention::
    Please note that throughout the activation and initial programming the window should **NOT be refreshed at any
    point**. Additionally, the activation and initial programming process **should only be done ONCE** for each new |DEVICE|.


In the home page click on the **Programmer** tool.

    .. _fig_activation-1:

    .. figure:: resources/activation-1.png
        :align: center
        :scale: 50

        Toolbox Application Home Page

This will open a window that will allow you to see any XDS connected device.
Select the connected XDS110 device from a drop-down list of XDS-devices
connected to the PC.

    .. _fig_activation-2:

    .. figure:: resources/activation-2.png
        :align: center
        :scale: 50

        XDS110 Select Page

Next select the flash option

    .. figure:: resources/flash-options.png
            :align: center
            :scale: 50

            Flash Select

.. warning::
    The flash option with the yellow triangle next to them are "Experimental Flashes" which have not been fully system tested

.. note::
    If you are using a Revision A Launchpad, select IS25WJ064F. For Launchpads Revision E4 or earlier revisions, select IS25WJ032F

After, select the appropriate PSRAM connected to the device

    .. figure:: resources/psram-options.png
        :align: center
        :scale: 50

        PSRAM Select

There will also be an Enable OTA and Custom Memory Map checkbox 

    .. figure:: resources/programmer-checkboxes.png
        :align: center
        :scale: 50

* The `Enable OTA` checkbox will configure the memory map to make room for 2 image slots

* The  `Custom Memory Map` checkbox will allow changing the size of NVS, Key Storage, and any extra Vendor dedicated memory region

Based on the |DEVICE| state (activated or deactivated) you will have different options

.. tabs::
    .. tab:: Deactivated

        Before your device is activated, you are presented three options in the Wi-Fi Toolbox: 

        .. figure:: resources/deactivated_toolbox.png 
            :align: center 

        You can choose to activate the device, set the fuses, or conduct a memory validation test. Note that if you decide to activate the device, you will end up needing to program the fuses as well.

        .. tabs::
            .. tab:: Activation
                
                The following step will require you to select the activation method. 
                There are 3 options for activating the device:

                - **Vendor Key** - Images will be verified using Vendors personal key
                
                - **SDK Example Key** - Emulate the full vendor operation using an emulation key (TI-provided 'debug' key).

                - **Authentication Bypass** - Enable the vendor to load and execute unauthenticated images.

                .. _fig_activation-3:

                .. figure:: resources/activation-options.png
                    :align: center
                    :scale: 50

                Activation Type Page

                **Vendor Key**
                
                Choosing `Vendor Key` will require to do a onetime setup in the `sign.py` script located
                in `simplelink_wifi_toolbox_x_x_x/flash-images-builder/signing_module`  

                .. code-block:: python

                    import pathlib
                    import requests
                    
                    from cryptography.hazmat.primitives.serialization import (
                        load_pem_public_key,
                        Encoding,
                        PublicFormat,
                    )
                    from OpenSSL.crypto import FILETYPE_PEM
                    from OpenSSL.crypto import sign, load_privatekey
                    
                    PUBLIC_KEY = None
                    PRIVATE_KEY = None
                    
                    
                    def buffer_sign(buffer_for_sign: bytes) -> bytes:
                        if PRIVATE_KEY is not None:
                            with open(PRIVATE_KEY, "rb") as f:
                                priv_key_data = f.read()
                    
                            pkey = load_privatekey(FILETYPE_PEM, priv_key_data)
                            signature = sign(pkey, buffer_for_sign, "sha256")
                    
                            return signature
                        else:
                            return b""
                
                This script is used by the Wi-Fi toolbox each time it programs the CC35xx device that was activated via "vendor key".

                You will see a PUBLIC_KEY and PRIVATE_KEY field and there are two options to set that up. 

                1. Provide the public and private keys to the script 
                2. Update the signing buffer and public key retrieval functions such that they can access these keys (or a signed application image altogether) from somewhere else (ie. server via API call, etc). How you choose to implement this is up to you.

                This is what you will see when choosing the "Vendor Key" without the proper key setup.

                .. figure:: resources/update-vendor-sign.png
                    :align: center
                    :scale: 50

                **SDK Example Key**
                
                Since the SDK example key was selected the "Root of Trust" key will be pre-selected. 
                The key is not pre-selected if the Authentication Bypass activation method is chosen. 
                
            
                .. _fig_activation-4:

                .. figure:: resources/activation-4.png
                    :align: center
                    :scale: 50

                    Activation Page

                At the end of the activation process the tool will report a summary for review. 
                In case of failed RoT fuse-programming, the activation/programming process 
                will be halted.

                .. _fig_activation-5:

                .. figure:: resources/activation-5.png
                    :align: center
                    :scale: 50

                    Review Page

                **Initial Programming**

                Once the activation process has concluded, the Initial Programming process will start 
                automatically in the next window. During this process you will download 
                an example image to the |DEVICE| 
                in addition to flash configuration. As a reminder, please be sure **not to refresh the page** during this process.

                .. attention::
                    During early access, initial programming will be done with predefined 
                    images and configurations. You will not be able to change the 
                    pre-selected inputs.

                * **Image selectionBoot Sector** - Flash partition, calibration, and flash high-speed configuration.
                * **TI Bootloader** - RAM-bootloader (2nd stage BL provided by TI).
                * **Vendor Demo Image** - for FCS versions the image will program the Network Terminal example.

                .. _fig_programming-1:

                    .. figure:: resources/programming-1.png
                        :align: center

                        Initial Programming Page

                Press the program button to begin Initial Programming. Once programmed you will be met with the following screen.

                .. figure:: resources/programming-2.png
                    :align: center

                    Initial Programming Page
            
            .. tab:: Fuses 

                Before you program your device for the first time, there fuse settings you must configure before they are locked in place and can never be altered again. 

                * Authentication Enable 
                * Flash Reset Type 
                * Restrict INI 
                * App OTP 
                * Country Code 
                * MAC Address Override 
                * Wi-Fi 6 Configuration 
                .. The first two (auth enable & flash reset type) will have default values that are mandatorily set based on activation type. 

                The images below show the default values of the fuses based on activation type. The authentication enable and flash reset type settings **must NOT be changed,**
                but you are free to tinker with anything else.

                .. tabs::
                    .. tab:: Vendor Key 

                        .. figure:: resources/vendor-key-fuses.png
                            :align: center

                        Use cases of the fuses that you can customize: 

                        * Restrict INI: Gives users the opportunity to require authorization (key) to update RF and regulatory settings.
                        * App OTP: Reserve section for storing vendor defined data in the OTP.
                        * Country Code: Restricts the device to only accept a conf file with the corresponding country code.
                        * MAC Address Override: Gives users the opportunity to program the device with their own MAC address. 
                        * Wi-Fi 6 Configuration: Gives users a one-time decision to either enable or disable Wi-Fi 6.

                    .. tab:: SDK Example Key 

                        .. figure:: resources/sdk-key-fuses.png
                            :align: center

                        Use cases of the fuses that you can customize: 

                        * Restrict INI: Gives users the opportunity to require authorization (key) to update RF and regulatory settings.
                        * App OTP: Reserve section for storing vendor defined data in the OTP.
                        * Country Code: Restricts the device to only accept a conf file with the corresponding country code.
                        * MAC Address Override: Gives users the opportunity to program the device with their own MAC address. 
                        * Wi-Fi 6 Configuration: Gives users a one-time decision to either enable or disable Wi-Fi 6.

                    .. tab:: Authentication Bypass

                        .. figure:: resources/auth-bypass-fuses.png
                            :align: center

                        Use cases of the fuses that you can customize: 

                        * Restrict INI: Gives users the opportunity to require authorization (key) to update RF and regulatory settings.
                        * App OTP: Reserve section for storing vendor defined data in the OTP.
                        * Country Code: Restricts the device to only accept a conf file with the corresponding country code.
                        * MAC Address Override: Gives users the opportunity to program the device with their own MAC address. 
                        * Wi-Fi 6 Configuration: Gives users a one-time decision to either enable or disable Wi-Fi 6.
                    
                    .. tab:: Partial Fuse Programming

                        .. figure:: resources/separate-fuse-programming.png 
                            :align: center
                
                        Use cases of the fuses that you can customize: 

                        * Restrict INI: Gives users the opportunity to require authorization (key) to update RF and regulatory settings.
                        * App OTP: Reserve section for storing vendor defined data in the OTP.
                        * Country Code: Restricts the device to only accept a conf file with the corresponding country code.
                        * MAC Address Override: Gives users the opportunity to program the device with their own MAC address. 
                        * Wi-Fi 6 Configuration: Gives users a one-time decision to either enable or disable Wi-Fi 6.

                .. note::
                    Note that the above images are only presented when you choose to activate your device. If you decide to undergo partial fuse programming, you will only see the five fuses that you are allowed to change as presented below.
                    Once you set the fuses here, you cannot change them again during the activation process.

            .. tab:: Memory Validation Test

                If you choose memory validation test(optional but good practice), you can either validate the flash or the PSRAM as shown below. The purpose is to validate memory connection and integrity to the CC35xxE devices. 

                .. figure:: resources/calibrator-test-options.png 
                    :align: center
                
    .. tab:: Activated

        After your device is activated, you may choose to program it via either the Wi-Fi toolbox or using CCS. 

        .. tabs::

            .. tab:: Wi-Fi Toolbox 

                When connecting your toolbox to an activated device, you may see and fill out a menu like this:

                .. figure:: resources/connect-to-device.png
                    :align: center

                Please note the "Activate By" field. What you set there must match how your device was activated.

                You will then be taking to the Programming Page

                .. figure:: resources/ProgrammingHome.png
                        :align: center
                        :scale: 50

                        Programming Top Level Screen

                The default binaries will be selected which will program the `Network Terminal` example. The option
                to load custom binaries is available by pressing on the `+` sign on the right of each binary. The following
                pop ups will appear. Starting with Vendor Image

                .. figure:: resources/custom_image.png
                        :align: center
                        :scale: 50

                        Adding custom vendor image

                If OTA is enabled, you will have the option to save the image in either Slot 0 or Slot 1. If you would like to have
                the image be unsecured choose the `Vendor Activation Bypass` otherwise use the SDK Example Key. This assumes the devices was activated with the default key,
                if it was not, select the pre-built image option with an image created using the vendor key.


                Changing `TI Wireless Firmware`

                .. figure:: resources/custom_fw.png
                        :align: center
                        :scale: 50

                        Adding custom firmware image

                If OTA is enabled, you will have the option to save the image in either Slot 0 or Slot 1. To switch FW version, find the `cc35xx_fw.bin` you would like to use.

                .. note::

                    There is a dependency between the Wifi Driver and the `cc35xx_fw.bin`. Make sure you only load the firmware that came with the SDK from which 
                    the driver is being used.
                    
                Other binaries should be kept to default binaries.
                If all the images have been chosen and the device is ready to be programmed, click on the `Program` button on the bottom right corner.
                Once the Programming process has been completed you will be met with a summary for review

                .. figure:: resources/ProgrammingEnd.png
                        :align: center
                        :scale: 50

                        Programming End
            
            .. tab:: CCS 

                If using CCS, you must select the correct activation type in SYSCFG based on how you activated your device as shown below:

                .. figure:: resources/ccs-set-activation-type.png
                    :align: center