Radio Tool Command Line Interface User’s Guide¶
Overview¶
The command line interface (CLI) provides a way to interact with RadioTool using only text based commands entered through a terminal or command prompt. You can see help text and optional arguments for the commands by adding “-h”.
To start navigate to the Simplelink Wi-Fi Toolbox install directory:
- For Windows:
cd c:\ti\simplelink_wifi_toolbox_X.X.X
- For Linux:
cd /home/YOUR_USER/ti/simplelink_wifi_toolbox_X.X.X
- For Mac OS X:
cd /Users/YOUR_USER/ti/simplelink_wifi_toolbox_X.X.X
Note
The install paths shown above are examples of the typical default path. Make sure to edit the command to reflect the install path for your use case.
Loading Containers¶
Note
The command mentioned in this section is an example. Make sure to substitute parts of the commands depending on your setup. This can include the file path and the device part number (i.e. replace “CC33xx” with your specific part number). It is especially important to substitute for your actual Debug Probe Serial Number instead of “12345678”, refer to Detect_XDS110_Serial_Number.
To load the firmware to the device use the command below;
Load the device bootloader:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 auto common load_radio_tool --tbl <2nd_loader path> --firmware <fw path> --conf_bin <cc33xx-conf path> --device_family CC33XX --tbl_dl_index 23 --firmware_dl_index 1 --conf_bin_dl_index 1 --sleep_tbl_fw 0 --sleep_fw_confbin 0
Note
If you are receiving errors, check the binary file paths. Make sure to change file path depending on simplelink_wifi_toolbox_X.X.X version and device (e.g. binaries/CC3301/cc33xx_fw.bin).
Hint
If you are using MAC or Linux, change the “.” to “./” to execute commands.
WLAN PLT¶
The CC35xx/CC33xx devices feature 2.4GHz & 5GHz Wi-Fi 6 with 20 MHz, single spatial stream, MAC, baseband, and RF transceiver supporting IEEE 802.11 b/g/n/ax. This section explains what CLI commands to use for testing Wi-Fi.
Once the containers have been loaded to the device (refer to Loading Containers) the commands below should be run before conducting Wi-Fi testing.
Turn on WLAN PLT:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan plt --onarguments: --on Enables PLT --off Disable PLT
Important
It is required that WLAN PLT be ON before doing any WLAN testing
Tune and Calibrate¶
For optimal performance it is important to Tune and Calibrate before transmitting every time the selected channel or band is changed.
Tune channel¶
To get optimal RF performance, use the Tune Channel command for the desired channel and band that will be tested.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan channel_tune --channel "1" --band "b24Ghz"
Note
Make sure that your channel and band selection match correctly (Channels 1-13 are 2.4GHz channels, and Channels 36-165 are 5GHz channels)
Calibration¶
To get optimal performance, use the calibrate command anytime the desired channel and band are changed.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 common calibration start --all
Hint
The plt commands may have optional arguments to tune and calibrate before running. If this option is used for those commands, calibration and channel tuning can be skipped.
Generating Transmit parameters¶
To specify transmit parameters for the device, a .json file is needed. This file will alow the device to transmit according to the specified values, the command below is used to generate example files for each available preamble type option;
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan tx gen_tx_params_json --preamble_type "PREAMBLE_TYPE" --output_dir DESIRED_OUTPUT_PATH
Example of generating transmit parameter .json file for preamble type “11b Long Preamble” ;
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan tx gen_tx_params_json --preamble_type "11b Long Preamble" --output_dir C:\ti\simplelink_wifi_toolbox_x.x.x
Contents of generated “tx_parameters_p_11b_long_preamble.json” file;
"bitmask": 4294967295, "delay": 3000, "packet_mode": "continuous", "number_of_packets": 300, "data_mode": "random_value", "data_const_value": 85, "src_addr": "22:22:33:44:55:66", "dst_addr": "02:02:03:04:05:06", "packet_length_start": 100, "packet_length_end": 100, "preamble_type": "p_11b_long_preamble", "phy_rate": "r_1_mbps", "tx_power": 0, "enable_cca": true, "_options_": { "delay_options": "50 .. 1000000", "packet_mode_options": [ "continuous", "single_packet", "multi_packet" ], "number_of_packets_options": "1 .. 10000", "data_mode_options": [ "constant_value", "increment", "random_value" ], "data_const_value_options": "0 .. 255", "packet_length_start_options": "0 .. 16000", "packet_length_end_options": "0 .. 16000", "phy_rate_options": [ "r_1_mbps", "r_2_mbps", "r_5p5_mbps", "r_11_mbps" ], "tx_power_options": "-10 .. 21" }
Note
Once the parameter file is generated you may edit the file as needed. Reference the arguments mentioned after line “_options_” to modify according to the available settings.
Hint
The generated .json file has many of the same parameters that can be exported from Radio Tool GUI directly. If unsure of what options to use, try exporting a file from RadioTool GUI with the desired settings to compare parameters.
Wi-Fi TX¶
Once the desired TX parameters file exists on a known path (refer to Generating Transmit parameters), the device can be set to transmit.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan tx start --channel "1" --band "b24Ghz" --calibrate --tx_parameters_file C:\ti\simplelink_wifi_toolbox_x.x.x/tx_parameters_p_11b_long_preamble.json
You may repeat the commands shown as needed, make sure to stop current Wi-Fi TX test before doing a another Wi-Fi transmission.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan tx stop
Once WLAN testing is complete, make sure to stop the test and turn PLT off.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan plt --off
Important
It is required that WLAN PLT be ON before starting TX testing, and any previous testing is stopped before running another test.
Before transmitting the device should always be tuned to the desired channel and band, then calibrated. This can be done when the optional arguments --channel, --band, and --calibrate are used in the command. The seperate Tune channel and calibrate commands can also be used (refer to Tune and Calibrate ).
Wi-Fi RX¶
RX testing is used for gathering Wi-Fi statistics within a specified channel.
Once the desired TX parameters file exists on a known path (refer to Generating Transmit parameters), the commands below shows how to run the Wi-Fi RX test.
Example of Starting Wi-Fi RX test for 2.4Ghz:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan rx start --ack_disable --preamble_type "All" --phy_rate "All" --mac_address "FF:FF:FF:FF:FF:FF" --channel "1" --band "b24Ghz" --calibrate
Note
When testing for 5Ghz the Association Index must be specified by adding optiona argument --aid.
Important
It is required that WLAN PLT be ON before starting Wi-Fi RX test, and any previous testing should stopped before running another test.
Before doing receiver testing the device should always be tuned to the desired channel and band, then calibrated. This can be done when the optional arguments --channel, --band, and --calibrate are used in the command. The separate Tune channel and calibrate commands can also be used (refer to Tune and Calibrate ).
Optional arguments for command ‘wlan rx’
arguments: start Start Receiver Test stop Stop Receiver Test stats Read Receiver Statistics
Optional arguments for command ‘wlan rx start’
Arguments: --ack_enable Response with ACK --ack_disable Don not respond with ACK --preamble_type Choose preamble Type Options: "All" (recommended option) "11b Short Preamble" "11b Long Preamble" "11ag Legacy OFDM" "11n Mixed Mode" "11ac VHT" "11ax SU" "11ax SU ER" "11ax TB" --phy_rate Choose the Phy Rate Options: [All (recommended option) , 1Mbps, 2Mbps, 5p5Mbps, 11Mbps, 6Mbps, 9Mbps, 12Mbps, 18Mbps, 24Mbps, 36Mbps, 48Mbps, 54Mbps, MCS0, MCS1, MCS2, MCS3, MCS4, MCS5, MCS6, MCS7] --mac_address MAC Address, Default: FF:FF:FF:FF:FF:FF --aid Association Index, Default: 65535 --channel Channel to tune before receiver test starts Options: [1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13] [36, 40, 44, 48, 52, 56, 60, 64, 100, 104, 108, 112, 116, 120, 124, 128, 132, 136, 140, 144, 149, 153, 157, 161, 165] --band Band of channel to tune before receiver test start Options: ["b24Ghz", "b5Ghz"] --calibrate Full calibration before receiver test start
Optional arguments for command ‘wlan rx stats’
Arguments: --get Read current statistics data --reset Reset statistics data --interval_sec Read statistics every specified interval, in seconds --samples Read statistics a specified amount of times
Example command to read statistics;
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan rx stats --get --interval_sec "1" --samples "1"
Example output from the “wlan rx stats” command.
Sample [1/1] Requesting For Statistics ... +-----------------------------+-------+ | Key | Value | +-----------------------------+-------+ | total_packet_number | 1 | | fcs_error_packet_number | 0 | | addr_mismatch_packet_number | 0 | | good_packet_number | 1 | | average_data_ctrl_rssi | -73 | +-----------------------------+-------+ Statistics got successfully In order to stop this task press on CTRL+C or wait for all samples done.
You may repeat the commands shown as needed, make sure to stop current Wi-Fi RX test before doing another Wi-Fi test.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan rx stop
Once WLAN testing is complete, make sure to stop the test and turn PLT off.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan plt --off
Wi-Fi TX Tone¶
When using the following command the user may create and transmit the Carrier Wave of a signal with selected tone options.
Example of running the Wi-Fi TX Tone command;
$ ./simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan tx_tone start --mode single_tone --offset -10 --channel "1" --band "b24Ghz" --calibrateArguments: start Start TX Tone stop Stop TX ToneArguments: --mode Tone mode Options:"single_tone" --offset Tone offset, Options: -10[Mhz] to +10[Mhz], with steps of 0.25[Mhz] --channel Channel to tune before TX Tone start Options: [1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13] [36, 40, 44, 48, 52, 56, 60, 64, 100, 104, 108, 112, 116, 120, 124, 128, 132, 136, 140, 144, 149, 153, 157, 161, 165] --band Band of channel to tune before TX Tone starts Options: ["b24Ghz"] --calibrate Full calibration before TX Tone start
You may repeat the commands shown as needed, make sure to stop current TX Tone test before doing a different test.
Example for stopping the current Wi-Fi TX Tone test;
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan tx_tone stop
Once testing is complete, make sure to stop the test and turn PLT off.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 wlan plt --off
Important
It is required that WLAN PLT be ON before starting RX, and any previous testing is stopped before running another test.
Before transmitting the device should always be tuned to the desired channel and band, then calibrated. This can be done with seperate commands (refer to Tune and Calibrate), but it is also done when the argument ‘–channel’, ‘–band’, and –calibrate are used with the appropiate commands.
Antenna Select¶
The following command is used to select the antenna
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 common antenna_selection set --antenna_number "0"
Optional arguments for command ‘common antenna_selection’
Arguments: set Set transmit antenna number get Get transmit antenna number
Optional arguments for command ‘common antenna_selection set’
arguments: --antenna_number Antenna number] Options: ["0", "1"]
BLE PLT¶
Bluetooth ® Low Energy 5.4 is only used with CC35x1/CC33x1 devices. This sections explains the CLI commands to use for testing BLE.
Once the containers have been loaded to the device (refer to Loading Containers) and the below commands are run you may start running BLE tests.
Enable the BLE Radio:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 common ble_enable
Turn on BLE PLT:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble plt --on
Note
It is required that BLE PLT be ON before doing any testing
Transmitting BLE Packets¶
The below commands are used to test BLE packet transmissions
Example of starting BLE TX with parameters:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble packet_tx start --phy_mode "LE_1_Mbps" --tx_power 0 --channel 17 --no_whitening --packet_number 100 --packet_interval_ms 10 --sequence_number_enable --packet_type OZOZ --packet_length 37 --calibrate
Example of starting BLE TX with infinite number of packets:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble packet_tx start --phy_mode LE_1_Mbps --tx_power 0 --channel 17 --whitening --packet_number 0 --packet_interval_ms 10 --sequence_number_enable --packet_type Hex --packet_payload_data "05 a2 11 22" --calibrate
Optional arguments for command ‘ble’
Arguments: plt Enable/Disable Production Line Test (PLT) packet_tx Packet Transmitter Test packet_rx Packet Receiver Test
- Optional arguments for command ‘ble packet_tx’
Arguments: start Start Packet Transmitter Test stop Stop Packet Transmitter Test stat Read Transmitter Statistics
Optional arguments for command ‘ble packet_tx start’
Arguments: --phy_mode Transmit PHY Mode Options: [LE_1_Mbps, LE_2_Mbps, LE_Coded_500_kbps, LE_Coded_125_kbps] --tx_power Transmit Power, between -10 and 22 dBm with 1 dBm available step --channel Transmit channel number Options: [0 to 39] --whitening Scrambled packet payload before transmission --no_whitening Do not scramble packet payload before transmission --packet_number Number of packet to transmit, set 0 for infinite number of packets --packet_type Transmit packet type Options: [Text, Hex, PRBS9, FOFO, ZOZO, PRBS15, ALLONES, ALLZEROS, OFOF, OZOZ] --packet_length Packet length to transmit, in bytes, required for non 'Hex'/'Text' packet type --packet_payload_data Packet payload data, required for 'Hex'/'Text' packet type --packet_interval_ms Interval between transmitted packets, in mSec --sequence_number_enable Include sequence number as part of payload, will include as two first bytes in payload --calibrate Calibrate before transmission
Use this command to read transmitter statistics
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble packet_tx stat --get --packet_type OZOZ--get Read current statistics data --reset Reset statistics data --packet_type Select transmitted packet type Options: ['Text', 'Hex', 'PRBS9', 'FOFO', 'ZOZO', 'PRBS15', 'ALLONES', 'ALLZEROS', 'OFOF', 'OZOZ']Use the following command to stop transmission testing. This is needed before a different transmission can be started.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble packet_tx stop
You can repeat the commands mentioned above with different parameters as desired. Once testing is complete, make sure to stop the test and turn PLT off.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble plt --off
Important
It is required that BLE PLT be ON before any BLE testing, and any previous testing is stopped before running another test with different parameters.
Before transmitting the device should always be tuned to the desired channel and band, then calibrated. This can be done with when the optional arguments --channel, --band, and --calibrate are used in the command. The separate Tune channel and calibrate commands can also be used (refer to Tune and Calibrate).
BLE Receive packets¶
The below commands are used to test receiving BLE packets
Optional arguments for command ‘ble packet_rx’
Arguments: start Start Packet Receiver Test stop Stop Packet Receiver Test stat Read Receiver Statistics
Example of starting BLE RX:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble packet_rx start --phy_mode "LE_2_Mbps" --channel 11 --no_whitening --calibrate
Optional arguments for command ‘ble packet_rx start’
Arguments: --phy_mode Receive PHY Mode Options: [LE_1_Mbps, LE_2_Mbps, LE_Coded_500_kbps, LE_Coded_125_kbps] --channel Transmit channel number Options: [0 to 39] --whitening Packet payload was scrambled before transmission --no_whitening Packet payload was not scrambled before transmission --access_address Access address, default: 8e89bed6 --only_statistics Collect packet statistics without packet payload --calibrate Calibrate before receiving packet
Use the following command to stop transmission testing. This is needed before a different transmission can be started.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble packet_rx stop
Use this command to geet BLE RX statistics:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble packet_rx stat --get
Optional arguments for command ‘ble packet_rx stat’
Arguments: --get Read current statistics data --reset Reset statistics data --view_format Display received payload as, available choices: ['Hex', 'Text'] --sequence_number Contains sequence number in payload --only_statistics Statistics without packet payload
You can repeat the commands mentioned above with different parameters as desired. Once testing is complete, make sure to stop the test and turn PLT off.
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble packet_rx stop$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 ble plt --off
Important
It is required that BLE PLT be ON before testing, and any previous testing is stopped before running another test with different parameters.
Before transmitting the device should be calibrated, this is done with the optional argument –calibrate.
More CLI Options¶
When using CLI you can use the following help command:
$ .\simplelink-wifi-toolbox.exe radio-tool -h
Output:
usage: .\simplelink-wifi-toolbox.exe radio-tool [-h] [--version] -i {XDS110} [-param1 INTERFACE_PARAMETER_1] [-param2 INTERFACE_PARAMETER_2] {firmware,phy,cpe,mce,mac_address,wlan,ble} positional arguments: {firmware,phy,cpe,mce,mac_address,wlan,ble} firmware Firmware phy Phy cpe CPE mce MCE mac_address Mac Address wlan WLAN ble BLE optional arguments: -h, --help show this help message and exit --version show program's version number and exit -i {XDS110}, --interface {XDS110} Interface -param1 INTERFACE_PARAMETER_1, --interface_parameter_1 INTERFACE_PARAMETER_1 Interface -param2 INTERFACE_PARAMETER_2, --interface_parameter_2 INTERFACE_PARAMETER_2 Interface
Device Information Commands¶
Bellow are command examples to get the version from device for firmware, PHY, CPE, and MCE
Get Firmware version:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 firmware -v
Get PHY version:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 phy -v
Get CPE version:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 cpe -v
Get MCE version:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 mce -v
Get device MAC address:
$ .\simplelink-wifi-toolbox.exe radio-tool -i XDS110 -param1 12345678 mac_address -a
Communicator Commands¶
To use the communicator (XDS110) with CLI you can use the following help command:
$ .\simplelink-wifi-toolbox.exe communicator -h
Outputs:
usage: .\simplelink-wifi-toolbox.exe communicator [-h] [--version] -i {XDS110} -param1 INTERFACE_PARAMETER_1 [-param2 INTERFACE_PARAMETER_2] {container,general,memory_read,memory_write,rma} ... positional arguments: {container,general,memory_read,memory_write,rma} container Download container from binary file general Get general information from Jtag memory_read Read from memory space using M3 memory_write Write into memory space using M3 rma Rma command optional arguments: -h, --help show this help message and exit --version show program's version number and exit -i {XDS110}, --interface {XDS110} Interface -param1 INTERFACE_PARAMETER_1, --interface_parameter_1 INTERFACE_PARAMETER_1 serial numberws interface -param2 INTERFACE_PARAMETER_2, --interface_parameter_2 INTERFACE_PARAMETER_2 Interface
$ .\simplelink-wifi-toolbox.exe communicator container -h
Outputs;
optional arguments:
-h, --help show this help message and exit
--container_file Path to container binary file
--timeout Set timeout for error detection
--write_delay Set delay between data send
--reset_device Reset device before download container
--dwnld_speed Configure download speed, avaliable options: ['low', 'mid', 'mid_high', 'high']
$ .\simplelink-wifi-toolbox.exe communicator general -h
Outputs;
positional arguments:
{device_reset,device_status,device_info}
device_reset get device status
device_status get device status
device_info get device information
Reset device¶
Instead of power cycling the device you may use the following command to reset the device:
$ .\simplelink-wifi-toolbox.exe communicator -i XDS110 -param1 12345678 general device_reset
To verify that the device was reset the following command may be used to verify the current status of the device:
$ .\simplelink-wifi-toolbox.exe communicator -i XDS110 -param1 12345678 general device_status
It should output a table with remark “WAITING_FOR_CONTAINER”, which means the device is waiting for the containers to be loaded ( refer to Loading Containers ).
Example Output below:
+-------------------+--------+-----------------+-----------------+-----------------------+ | Reg Name | Offset | Reg Value (DEC) | Reg Value (HEX) | Remark | +-------------------+--------+-----------------+-----------------+-----------------------+ | DEVICE_ID | 0 | 196612143 | 0xbb8102f | | | DEVICE_USER_CODE | 4 | 0 | 0x0 | | | DEBUG_SS_VERSION | 8 | 1073741968 | 0x40000090 | | | SYS | 12 | 0 | 0x0 | | | BOOT_DIAG | 16 | 11 | 0xb | WAITING_FOR_CONTAINER | | LIFE_CYCLE_STATE | 20 | 3 | 0x3 | | | DFT_EN | 24 | 0 | 0x0 | | | UNIQUE_DEVICE_ID0 | 40 | 287703744 | 0x112602c0 | | | UNIQUE_DEVICE_ID1 | 44 | 337784908 | 0x1422304c | | +-------------------+--------+-----------------+-----------------+-----------------------+
How to detect my XDS110 Serial Number¶
When the XDS110 debug probe is connected to PC you may confirm the serial number by doing the following.
Windows¶
Open Windows Command Line ( CMD ) and navigate into the XDS110 updates directory with this command:
cd c:\ti\simplelink_wifi_toolbox_x.x.x\utility\xds110
Execute the following command to show information of connected devices.
$ .\xdsdfu -e
output should look like this:
Ubuntu¶
Open terminal and navigate into the XDS110 updates directory with this command:
cd /home/${USER}/ti/simplelink_wifi_toolbox_x.x.x/utility/xds110
Execute the xdsdfu application to see all connected devices
./xdsdfu -e