WiFi F3 SimpleLink Core SDK 9.20.00.23 Release Notes

Table of Contents

Introduction

This is a Production (GA) release of the Core SDK 9.20.00.23 for WiFi F3 devices.

Documentation

Open the Documentation Overview file in the docs/ folder for a full list of documentation.

What’s New

Upgrade and Compatibility Information

Host Support

See the SDK release notes for a description of which host operating systems are supported in this release.

Dependencies

See the SDK release notes for a description of which components and tools are required to work with this product.

Device Support

See the SDK release notes for a list of TI devices that are supported in this product.

Validation Information

The Core SDK was validated with the following components:

New Features

ID Summary
LPRFSEC-256 Enable usage of hash length > curve length in ECDSA Driver

Fixed Issues

ID Summary
TIDRIVERS-7639 Fixed bit Misalignment in ExceptionArmV8M.c within the Exception module
LPRFSEC-253 Fixed an issue where psa_mac_abort() would return an error instead of invoking mbedtls when using SW crypto

Known Issues

ID Summary
TIDRIVERS-7249 [CC35XX] ROV is not functional

Customer Support

Versioning

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

Prior Release Changes

A summary of changes made in previous releases of this product can be found in the product Change Log.