HTTP Client and Server

Introduction

The lightweight TCP/IP (LwIP) stack is an open-source TCP IP stack used in embedded systems. The LwIP stack is designed to reduce memory usage and code size. LwIP network stack includes built-in support for HTTP web client and server. The implementation of LwIP includes HTTP GET only and is missing implementation for HTTP POST. Since LwIP does not have any HTML parsing (e.g. not loading any items inside HTML, page redirection, etc), it is mainly aimed to work with servers that serve basic GET services (e.g. static pages).

The implementation of HTTP server in LwIP includes a basic list of static pages and in addition two dynamic mechanisms, CGI (Common Gateway Interface) and SSI (Server Side Includes). CGI mechanism allows clients to hook functions to particular request URIs. This can be useful in cases where the client want to modify the state of a resource on the server, e.g. toggle a led. SSI mechanism allows clients to replace a well defined tag or token on an HTML page with a value from application. This can be useful in cases where the client want to fetch the state of a resource on the server, e.g. read a temperature. To enable SSI support, define label LWIP_HTTPD_SSI in lwipopts.h. To enable CGI support, define label LWIP_HTTPD_CGI in lwipopts.h.

Note

Next SDK releases would include examples of both, HTTP client and HTTP server.

HTTP client

HTTPS

In order to secure the TLS layer in HTTP (also known as HTTPS), an external mbedTLS library is used. The current implementation of HTTP client in LwIP does not include any hooks for a secured HTTP client. Nevertheless, the user can add support for a secured client by referring to HTTPS server implementation (see next section) and MQTT client.

HTTP Server

CGI Notes

  1. The simple CGI support offered works with GET method requests only.
  2. Can handle up to LWIP_HTTPD_MAX_CGI_PARAMETERS parameters encoded into the URI, currently 16 parameters, but it can be modified in httpd_opts.h.
  3. The handler function may not write directly to the HTTP output but must return a filename that the HTTP server will send to the browser as a response to the incoming CGI request.

SSI Notes

  1. No tag may contain ‘-’ or whitespace characters within the tag name.
  2. Whitespace is allowed between the tag lead-in "<!--#" and the start of the tag name and between the tag name and the lead-out string "-->".
  3. The maximum tag name length is LWIP_HTTPD_MAX_TAG_NAME_LEN, currently 8 characters, but it can be modified in httpd_opts.h.

HTTPS

In order to secure the TLS layer in HTTP (also known as HTTPS), an external mbedTLS library is used. Mbed TLS is a C library that implements cryptographic primitives, X.509 certificate manipulation and the SSL/TLS and DTLS protocols. It is distributed under the Apache License version 2.0. Its small code footprint makes it suitable for embedded systems. It is known to be easy to understand, use, integrate and expand. The library is designed to integrate with existing (embedded) applications and to provide the building blocks for secure communication, cryptography and key management. It is designed to be as loosely coupled as possible, allowing you to only integrate the parts you need without having overhead from the rest.

LwIP and mbedTLS

The LwIP project already has inbuilt support for MbedTLS. With MbedTLS being enabled, the data which passes through the default TCP layer now takes an alternate route and is processed by an Alternate TCP/IP layer (also referred to as ALTCP layer). These layers have callback functions set. The callback functions determine the behavior of application on establishing connection, sending data, receiving data, closing connection, handling errors, and so forth. The mbedTLS implementation in LwIP is mainly done in a single file, altcp_tls_mbedtls.c. To have mbedTLS support with LwIP, the user need to enable the LWIP_HAVE_MBEDTLS in lwipopt.h header file.

LwIP implementation of HTTPS

LwIP already includes a secured HTTP server implementation using the httpd_inits() API instead of httpd_init(). In addition, the certificates and keys must be registered for security to work. This is done by using the altcp_tls_create_config_server_privkey_cert() API. Please note that LwIP implementation does not use the CA certificate (hard-coded) so by definition there is no client authentication. To also disable client authentication in LwIP, the authentication mode should be set to either MBEDTLS_SSL_VERIFY_OPTIONAL or MBEDTLS_SSL_VERIFY_NONE and not MBEDTLS_SSL_VERIFY_REQUIRED. This setting can be found under altcp_tls_mbedtls.c. To enable HTTPS, HTTPD_ENABLE_HTTPS needs to be define under httpd_opts.h.

TLS certificates

As for generating certificates and keys for the HTTPS demo, the following openssl commands can be used: * Create Key pair for Certificate authority (CA).

oopenssl genrsa -des3 -out ca.key 2048
  • Generate certificate for CA using above key
openssl req -new -x509 -days 1826 -key ca.key -out ca.crt
  • Create server key pair for the server, to be used by the broker
openssl genrsa -out server.key 2048
  • Create a Certificate Sign Request (csr) for the server
openssl req -new -out server.csr -key server.key
  • Self sign the Server certificates using CA key
openssl x509 -req -in server.csr -CA ca.crt -CAkey ca.key -CAcreateserial -out server.crt -days 360
  • To convert certificates from PEM to DER format. Convert both CA and server certificates
openssl x509 -outform der -in ca.pem -out ca.crt
openssl rsa -outform der -in ca.key -out ca.key
  • To convert DER certificates to binary data, this data is used in client_info.h
xxd -i filename.der filename.h