Network Layer Security¶
The CC35xx device is a Wi-Fi-based device, which supports 802.11 security protocols for the local segment of the network (between the node and the AP) and TLS/SSL for the transport layer when using TCP/IP for nodeto-node communication. TLS/SSL can address confidentiality, data integrity, and authenticity between nodes across the network.
WiFi Security¶
The Wi-Fi layer of the SimpleLink device complies with 802.11 security to ensure the integrity and confidentiality of the frames (L2 data units) in transactions between AP and STA, or between two peers in the case of Wi-Fi direct mode. The security protocols are described in the IEEE 802.11 specifications and its extensions. The Wi-Fi subsystem of the SimpleLink device provides support for both personal and enterprise security paradigms, including RADIUS-based authentication (802.1X)
The SimpleLink device is Wi-Fi-CERTIFIED™ and complies with Wi-Fi Alliance (WFA) security standards and test suites.
Secure Socket Layer¶
The SimpleLink device provides a secure transport layer (secure sockets) based on a standard-complaint implementation of SSL and TLS protocols, which are network protocols that involve cryptographic paradigms designed to provide communications security over a TCP/IP connection.
The SSL/TLS runs on the network processor subsystem. By design, the architecture of the device is such that the networking processor is a physically separate process subsystem, creating a separate execution environment. Hardware accelerators are used to offload the intense arithmetic calculations involved in the cryptographic algorithms.
After establishing a TCP connection between two peers, the SSL protocol takes place in negotiating the session security parameters and authenticating the peers. A short description of this handshake process follows. This handshake is performed by the SimpleLink device, and remains transparent to the user: #. A client hello message is sent with the following parameters:
- Protocol version to be used
- Cipher suites supported by the client
- Extensions, used for different applications of the SSL
- The server chooses the protocol version and a cipher suite from the client hello cipher list, and sends a ServerHello message to the client.
- The server sends the certificate chain (except for the root CA) to the client.
- The client may verify the chain by checking the signature of each certificate in the chain, starting with the root CA held by the client. The server may request a certificate from the client for a client authentication.
- The client and server establish session (symmetric) keys and can then start transferring encrypted data.