Migration from 9.13.01.14 → 9.20.00.07

This page will go over the main changes between SDK version 9.13.01.14 and 9.20.00.07

CCS

The SDK now works with the latest CCS 20.3. This provides a more seamless experience as no patching is necessary.

Examples

Networking examples are now located under examples/rtos/LP_EM_CC35X1/demos.

Wlan Driver

conf_cc35xx.h has been renamed to conf.h