Migration from 9.10.00.01 → 9.13.00.13¶
This page will go over the main changes between SDK version 9.10.00.01 and 9.13.00.13
WLAN Driver¶
Wlan_RoleUp¶
- Added RoleUpStaCmd_t type, API will now use this type instead RoleUpApCmd_t type.
- Added new WPS params to RoleUpStaCmd_t and RoleUpApCmd_t
Cryptography Driverlibs¶
All the cryptographic drivers have changed naming convention
For example the HSM driver changed from HSMLPF3 to HSMXXF3 all APIs and functions have similarly changed names
Please update accordingly to your project
Build System¶
CCS_projects directory was removed and with it replaced by cmake configuration to now build all libraries.