ALL VERSIONS¶
For each SDK release, do the following steps to update SDK version on existing projects
Attention
If you have an already activated device, you will need to perform “Factory Programming” with the toolbox provided in the sdk before being flashing via CCS.
Open CCS and verify that the latest versions of
SimpleLink Wifi Toolbox,SimpleLink Wi-Fi SDK, andSysConfigare detected as a productThis can be done by going to
File→Preferences→Code Composer Studio SettingsNext go into
General→ProductsImport Project from the new SDK by going to
File→Import ProjectsBrowse for the example
Verify
SimpleLink Wifi Toolbox,SimpleLink Wi-Fi SDK, andSysConfigis in the product dependencies. Right click on the Project and navigate toPropertiesIn the Project Properties go to
General→Dependencies→Product DependenciesIf the
SimpleLink Wifi Toolboxis not in the list. Click on the Plus icon and select theSimpleLink Wifi Toolboxand latest version.
Open CCS and verify that the latest versions of
SimpleLink Wifi Toolbox,SimpleLink Wi-Fi SDK, andSysConfigare detected as a productThis can be done by going to
File→Preferences→Code Composer Studio SettingsImport Project from the new SDK by going to
File→Import Projects- On pop up dialog select “Code Composer Studio” and then “CCS Project” and “Next”.
- Click on “Browse …” and navigate into examples.
SDK_INSTALL_DIR/examples/rtos/CC35X1_LAUNCHXLfor driver examples/CC35xx_network_terminalfor the WiFi network terminal example
- Click “Select Folder” and selected projects should appear in “Discovered projects”. Make sure “Copy projects into workspace” is checked before clicking “Finish”.
Verify
SimpleLink Wifi Toolbox,SimpleLink Wi-Fi SDK, andSysConfigis in the product dependencies.
Right click on the Project and navigate to Properties
If the SimpleLink Wifi Toolbox is not in the list. Click on the Plus icon and select the
SimpleLink Wifi Toolbox and latest version.