HCI_EXT_SetRxGainDone

Opcode:0x0400
Event Description:
 This event is sent to indicate the RF receiver gain has been set, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_SetTxPowerDone

Opcode:0x0401
Event Description:
 This event is sent to indicate the RF transmitter power has been set, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_OnePacketPerEventDone

Opcode:0x0402
Event Description:
 This event is sent to indicate the One Packet Per Event feature has been enabled or disabled, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_DecryptCommandDone

Opcode:0x0405
Event Description:
 This event is sent to indicate Decryption has completed.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table
Decrypted Data:

128 bit decrypted data block. The most significant octet of plainTextData corresponds to plainTextData using the notation specified in FIPS 197.

Size:16 byte(s)
Range:Any 16 byte value

HCI_EXT_WriteLocalFeatureSupportDone

Opcode:0x0406
Event Description:
 This event is sent to indicate the Set Local Supported Features command has completed.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_SetFastTxResponseTimeDone

Opcode:0x0407
Event Description:
 This event is sent to indicate the Set Fast Transmit Response Time feature has been enabled or disabled, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_SetBDADDRDone

Opcode:0x040C
Event Description:
 This event is sent to indicate the devices BLE address has been set, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_SetSCADone

Opcode:0x040D
Event Description:
 This event is sent to indicate the devices SCA has been set, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_DisconnectImmedDone

Opcode:0x0413
Event Description:
 This event is sent to indicate the Disconnect Immediate command has completed, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_PER

Opcode:0x0414
Event Description:
 This event is sent to indicate the Packet Error Rate Reset or Read command has completed, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table
PER Command Type:
 

Read or Reset

Size:

1 byte(s)

Range:
Value Description
0 Reset PER Counters
1 Read PER Counters
RX Pkts:

Number of received packets.

Condition:( cmdVal!=0x00 && cmdStat==0x00)
Size:2 byte(s)
Range:Any 2 byte value
RX CRC Fails:

Number of received packets with CRC error.

Condition:( cmdVal!=0x00 && cmdStat==0x00)
Size:2 byte(s)
Range:Any 2 byte value
Events:

Number of connection events.

Condition:( cmdVal!=0x00 && cmdStat==0x00)
Size:2 byte(s)
Range:Any 2 byte value
Missed Events:

Number of missed connection events.

Condition:( cmdVal!=0x00 && cmdStat==0x00)
Size:2 byte(s)
Range:Any 2 byte value

HCI_EXT_ResetSystemDone

Opcode:0x041D
Event Description:
 This event is sent to indicate the Reset System command has completed, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_NumComplPktsLimitDone

Opcode:0x041F
Event Description:
 This event is sent to indicate the Number Completed Packets Limit command has completed, or that there was an error.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_GetConnInfoDone

Opcode:0x0420
Event Description:
 This event is sent to indicate the Get Connection Information command has completed.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table
Alloc Conns:

Total number of allocated connections

Size:1 byte(s)
Range:
Active Conns:

Number of currently active connections

Size:1 byte(s)
Range:

An array of size “numConn” will be returned containing the parameters starting here:

Conn Handle:

Connection Handle

Size:1 byte(s)
Range:
Conn Role:
Size:

1 byte(s)

Range:
Value Description
0x22 LMP/LL Response Timeout
0x23 LMP Error Transaction Collision
0x24 LMP PDU Not Allowed
0x25 Encryption Mode Not Acceptable
0x26 Link Key Can Not be Changed
0x27 Requested QoS Not Supported
0x28 Instant Passed
0x29 Pairing With Unit Key Not Supported
0x2A Different Transaction Collision
0x2B Reserved
0x2C QoS Unacceptable Parameter
0x2D QoS Rejected
0x2E Channel Assessment Not Supported
0x2F Insufficient Security
0x30 Parameter Out Of Mandatory Range
0x31 Reserved
0x32 Role Switch Pending
0x33 Reserved
0x34 Reserved Slot Violation
0x35 Role Switch Failed
0x36 Extended Inquiry Response Too Large
0x37 Simple Pairing Not Supported By Host
0x38 Host Busy ^ Pairing
0x39 Connection Rejected Due To No Suitable Channel Found
0x3A Controller Busy
0x3B Unacceptable Connection Interval
0x3C Directed Advertising Timeout
0x3D Connection Terminated Due To MIC Failure
0x3E Connection Failed To Be Established
0x3F MAC Connection Failed
0x40 Coarse Clock Adjust Rejected
0x41 Type0 Submap Not Defined
0x42 Unknown Advertising Identifier
0x43 Limit Reached
0x44 Operation Cancelled by Host
Peer Addr:
Size:6 byte(s)
Range:
Peer Addr Type:
Size:

1 byte(s)

Range:
Value Description
0x00 Public
0x01 Random
0x02 Public Identity
0x03 Random Identity

The array of parameters ends here.

HCI_EXT_SetMaxDataLengthDone

Opcode:0x0421
Event Description:
 This event is sent to indicate the Set Max Data Length command has completed.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table

HCI_EXT_LLTestModeDone

Opcode:0x0470
Event Description:
 LL Test Mode event.

Event Parameters

Status:
Size:1 byte(s)
Range:See Status Table
Command Opcode:
Size:2 byte(s)
Range:See Command Table