.. _sec-wifi-sockets:

Sockets
========

Introduction
-------------

LwIP network stack includes built-in support BSD style sockets, allowing developers to use the familiar socket programming API.
Using familiar socket APIs abstract the inner implementation from the user, allowing migration of networking code more easily.
In LwIP there are two main types of sockets, BSD sockets API and Netconn APIs.
There is also a RAW socket API that is used mostly when in no-OS mode but this would not be covered.

BSD style APIs
---------------

This is a high-level API that provides a familiar interface for network programming, similar to what you'd find in standard Unix/Linux systems.
The BSD sockets API provides a more standard, POSIX-like interface, than Netconn.

The APIs for using BSD sockets are mainly under ``socket.h`` header file.
These BSD socket APIs would call ``lwip_xxx()`` with the ``xxx`` defined as the API operation itself.
To enable LwIP sockets, user must define label ``LWIP_SOCKET`` in ``lwipopts.h``.

The full set of BSD Socket APIs can be found at `socket.html <https://www.nongnu.org/lwip/2_1_x/group__socket.html>`_.

Netconn style APIs
-------------------

lwIP uses the Netconn API to implement the BSD Sockets API internally, but it can also be called directly from applications.
The Netconn API is a higher-level, lwIP-specific interface for socket programming, and as such, it is not portable as a BSD socket API.

The APIs for using Netconn start with ``netconn_xxx()``.
To enable LwIP sockets and also Netconn support, user must define label ``LWIP_SOCKET`` and ``LWIP_NETCONN`` in ``lwipopts.h``.

The full set of Netconn APIs can be found at `netconn.html <https://www.nongnu.org/lwip/2_1_x/group__netconn.html>`_.

Socket APIs used in SDK examples
---------------------------------

The SDK includes currently two examples, ``CC35xx_network_terminal`` and ``CC35xx_MQTT_client``
``CC35xx_network_terminal`` example uses the ``lwip_xxx()`` which are eventually calling the ``netconn_xxx()`` APIs.
It can be seen that the default configuration in ``lwipopts.h`` includes both, ``LWIP_SOCKET`` and ``LWIP_NETCONN``.
``CC35xx_MQTT_client`` example, like other built-in protocols, exposes protocol specific APIs so there is no need to call directly any socket APIs.
In MQTT example specifically, LwIP provides some specific MQTT APIs (starting with ``mqtt_xxx()``), which handle the socket internally and transparently.
More specifically, it uses ALTCP layer (Application Layered TCP) which is an abstraction layer that prevents applications linking directly against the tcp.h.
This way, an application can make use of other application layer protocols on top of TCP without knowing the details. A good example is the TLS implementation with mbedTLS stack.
The ALTCP is used internally in MQTT as well as in HTTP and applications can also use it.


Code examples
--------------

The following code snippet illustrates a TCP server allowing connection from a peer device, receiving and printing the received message and sending a pre-defined response.

.. code-block:: bash

    #include "lwip/sockets.h"

    #define SERVER_PORT 8080
    #define BUFFER_SIZE 1024

    void tcp_server(void *arg) {
        int server_fd, client_fd;
        struct sockaddr_in server_addr, client_addr;
        socklen_t addr_len = sizeof(client_addr);
        char buffer[BUFFER_SIZE];

        // Create socket
        server_fd = lwip_socket(AF_INET, SOCK_STREAM, 0);
        if (server_fd < 0) {
            printf("Socket creation failed\n");
            return;
        }

        // Bind socket to port
        server_addr.sin_family = AF_INET;
        server_addr.sin_port = htons(SERVER_PORT);
        server_addr.sin_addr.s_addr = INADDR_ANY;

        if (lwip_bind(server_fd, (struct sockaddr*)&server_addr, sizeof(server_addr)) < 0) {
            printf("Bind failed\n");
            lwip_close(server_fd);
            return;
        }

        // Listen for connections
        if (lwip_listen(server_fd, 5) < 0) {
            printf("Listen failed\n");
            lwip_close(server_fd);
            return;
        }

        printf("Server listening on port %d\n", SERVER_PORT);

        while (1) {
            // Accept client connection
            client_fd = lwip_accept(server_fd, (struct sockaddr*)&client_addr, &addr_len);
            if (client_fd < 0) {
                printf("Accept failed\n");
                continue;
            }

            printf("Client connected\n");

            // Receive data
            int len = lwip_recv(client_fd, buffer, BUFFER_SIZE, 0);
            if (len > 0) {
                buffer[len] = '\0';
                printf("Received: %s\n", buffer);

                // Send response
                lwip_send(client_fd, "Hello from server", 17, 0);
            }

            // Close client connection
            lwip_close(client_fd);
        }

        lwip_close(server_fd);
    }

The following code snippet illustrates a TCP client connecting to a server, sending a pre-defined data, receiving a response and presenting it.

.. code-block:: bash

    #include "lwip/sockets.h"

    #define SERVER_IP "192.168.1.100"
    #define SERVER_PORT 8080

    void tcp_client(void *arg) {
        int client_fd;
        struct sockaddr_in server_addr;
        char buffer[1024] = "Hello from client";

        // Create socket
        client_fd = lwip_socket(AF_INET, SOCK_STREAM, 0);
        if (client_fd < 0) {
            printf("Socket creation failed\n");
            return;
        }

        // Server address
        server_addr.sin_family = AF_INET;
        server_addr.sin_port = htons(SERVER_PORT);
        server_addr.sin_addr.s_addr = inet_addr(SERVER_IP);

        // Connect to server
        if (lwip_connect(client_fd, (struct sockaddr*)&server_addr, sizeof(server_addr)) < 0) {
            printf("Connection failed\n");
            lwip_close(client_fd);
            return;
        }

        // Send data
        lwip_send(client_fd, buffer, strlen(buffer), 0);

        // Receive response
        int len = lwip_recv(client_fd, buffer, sizeof(buffer), 0);
        if (len > 0) {
            buffer[len] = '\0';
            printf("Received: %s\n", buffer);
        }

        // Close socket
        lwip_close(client_fd);
    }