.. _sec-wifi-sntp:

SNTP
========

Introduction
-------------

SNTP (Simple Network Time Protocol) is a protocol used to synchronize the clocks of computers over a network. SNTP is designed for
applications that do not require the full complexity of the Network Time Protocol (NTP) such as embedded devices and microcontrollers.
SNTP uses a client-server model over UDP.

SNTP Feature Description
---------------

Network Terminal Example project (``CC35xx_network_terminal``) included in the SDK uses SNTP. This example project uses SNTP
to synchronize the device's clock with an NTP server. The APIs for SNTP are declared in the ``sntp_wrapper.h`` file and implemented
in the ``sntp_wrapper.c`` file. To enable SNTP in the example, the user must define the label ``SNTP_SUPPORT`` in the project properties.
Using the SNTP is a two step process where the first step is to configure the SNTP Servers and the second step is to update the Date and Time.

SNTP APIs
-------------------

To configure the SNTP servers, the user can use ``sntpWrapper_store_servers()`` API. This API takes the number of servers (maximum 3) and an
array of server addresses as input. To update the Date and Time from the SNTP servers, the user can use ``sntpWrapper_update_time()`` API.
This API takes no input and returns 0 on success and -1 on failure. As discussed above, the SDK includes ``CC35xx_network_terminal``
example project that demonstrates the use of these APIs.

Code examples
--------------

The following code snippet illustrates the use of storing SNTP servers and updating the date and time from the SNTP servers.

.. code-block:: bash

    #ifdef SNTP_SUPPORT
    #include "sntp_wrapper.h"
    #endif


    #ifdef SNTP_SUPPORT
    int32_t cmdSntpConfigServers(void *arg)
    {
        int32_t ret  = 0;
        char  *serverIp[3];
        uint32_t numOfServers;
        int i;
        ret = ParseSntpConfigServersCmd(arg, &numOfServers,serverIp);
        if(ret < 0)
        {
            printSntpConfigServersUsage(arg);
            return(0);
        }
        sntpWrapper_store_servers(numOfServers,serverIp[0],serverIp[1], serverIp[2]);
        for(i=0; i<numOfServers; i++)
        {
            os_free(serverIp[i]);
        }
        return ret;
    }
    // Command to update date and time from SNTP server
    // It will start a task that runs in the background every 30 minutes to
    // synchronize the local time with the actual time from SNTP server
    int32_t cmdSntpUpdateDateTime(void *arg)
    {
        int32_t ret  = 0;

        if (((!IS_BIT_SET(ActiveNetIfBitMap, NET_IF_STA_BIT)) || (!IS_STA_CONNECTED(app_CB.Status)))
                && (!IS_BIT_SET(ActiveNetIfBitMap, NET_IF_AP_BIT)))
        {
            Report("\n\rSTA/AP role is not up or connected.\n\r");
            return -1;
        }

        ret = sntpWrapper_updateDateTime();
        return ret;
    }
    #endif