.. _sec-wifi-basic-operations:

Basic Operations
================

Each of these WLAN commands eventually calls an API in the lower layer that is represented by the ``wlan_if.c`` file.
This file is part of the ``wifi_stack.a`` library.
Following is a detailed explanation of each WLAN command and its API in the ``wifi_stack.a`` library.

wlan_start
----------

This command turns on the WLAN device, initialize the several threads (like CME, transport, event, etc), and initialize the host interface.
During the process, the containers (FW, bootloader and configuration binaries) are loaded from the NVMEM and programmed to the MAC layer.
This step should be the first, otherwise there will be no communication with the device.

An eventHandler Callback must be passed as a parameter, see the example below.

The API to start WLAN in the ``wifi_stack.a`` library:

.. code-block:: c

        void WlanStackEventHandler(WlanEvent_t *pWlanEvent)
        {
                void *staif = NULL;

                if(!pWlanEvent)
                {
                        return;
                }
                switch(pWlanEvent->Id)
                {
                        case WLAN_EVENT_CONNECT:
                        {
                        }
                        break;
                        case WLAN_EVENT_DISCONNECT:
                        {
                        }
                        break;
                        case WLAN_EVENT_SCAN_RESULT:
                        {
                        }
                        break;
                        default:
                        {
                                UART_PRINT("\n\r[WLAN EVENT HANDLER] Unexpected event [%d]\n\r",
                                        pWlanEvent->Id);
                        }
                        break;
                }
        }

.. code-block:: c

        int32_t ret = 0;

        ret = Wlan_Start(WlanStackEventHandler);

        if (ret == OSI_OK)
        {
                Report("\n\rWlan start success!");
        }
        else
        {
                Report("\n\rWlan start failed: %d. please refer errors.h \n\r", ret);
        }

wlan_stop
---------

This command turns off the WLAN device and deactivates the host interface.
During the process, the threads are deleted and queues and semaphores destroyed.
This step should be the last.
The API to stop WLAN in the ``wifi_stack.a`` library:

.. code-block:: c

        ret = Wlan_Stop(void);
        if (0 == ret)
        {
                Report("\n\r   Wlan stop success!");
        }
        else
        {
                Report("\n\r   Wlan stop failed: %d. please refer errors.h\n\r", ret);
        }


wlan_sta_role_up
----------------

This command adds and starts a station role. 

.. note::
        
        Be sure to call the correct Wlan_Set(WLAN_SET_STA_WIFI_BAND, &sta_wifi_band) to select 5GHz or else 5GHz will not work! 

The API to add a network interface in the ``wifi_stack.a`` library:

.. code-block:: c

        int32_t ret = 0;
        RoleUpStaCmd_t RoleUpStaParams;
        memset(&RoleUpStaParams, 0x0, sizeof(RoleUpStaCmd_t));

        //Set 2.4G and 5G
        uint8_t sta_wifi_band =  (uint8_t)BAND_SEL_BOTH;
        Wlan_Set(WLAN_SET_STA_WIFI_BAND, &sta_wifi_band);

        RoleUpStaParams.wpsDisabled = TRUE; /* WPS is enabled by default */

        ret = Wlan_RoleUp(WLAN_ROLE_STA, &RoleUpStaParams, WLAN_WAIT_FOREVER);

wlan_sta_role_down
------------------

This command stops and removes a station role.
If the station is connected to an AP, the connection is first terminated.
During the process, a network interface is removed from the network stack (LwIP) and eventually a station role is removed.

The API to remove a network interface in the ``wifi_stack.a`` library:

.. code-block:: c

        int32_t ret = 0;
        
        if(connected)
        {
                ret = Wlan_Disconnect(WLAN_ROLE_STA,NULL);
        }
        
        if(OSI_OK != ret)
        {
                Report("WlanDisconnect() failed");
                return ret;
        }

        ret = Wlan_RoleDown(WLAN_ROLE_STA, WLAN_WAIT_FOREVER);

wlan_ap_role_up
---------------

This command adds and starts an AP role.
During the process, a network interface is added to the network stack (LwIP) and eventually an AP role is added.

The API to add a network interface in the ``network_lwip.c``  library::

.. code-block:: c

        void network_stack_add_if_ap()

The API in the ``wifi_stack.a`` library:

.. code-block:: c

        int32_t      ret = 0;
        RoleUpApCmd_t RoleUpApParams;
        
        /* Call the command parser */
        memset(&RoleUpApParams, 0x0, sizeof(RoleUpApParams));
        
        /* Set default parameters */
        RoleUpApParams.sta_limit = 4;
        RoleUpApParams.hidden = FALSE;
        RoleUpApParams.tx_pow = 0;
        RoleUpApParams.channel = 1;
        RoleUpApParams.sae_pwe = 2;
        RoleUpApParams.hidden = FALSE;
        RoleUpApParams.channel = 6;

        //prepare configuration for WPS connection
        RoleUpApParams.wpsParams.deviceName = (char *) g_modelName;
        RoleUpApParams.wpsParams.configMethods = (char *) g_wpsConfigMethods;
        RoleUpApParams.wpsParams.manufacturer = (char *) g_manufacturer;
        RoleUpApParams.wpsParams.modelName = (char *) g_modelName;
        RoleUpApParams.wpsParams.modelNumber = (char *) g_modelNumber;
        RoleUpApParams.wpsParams.serialNumber = (char *) g_serialNumber;
        RoleUpApParams.wpsParams.uuid = (uint8_t *) g_uuid_string;
        RoleUpApParams.wpsParams.deviceType = (uint8_t *) g_primaryDeviceType;
        
        Report("AP %s channel: %d", RoleUpApParams.ssid,RoleUpApParams.channel);
        
        ret = Wlan_RoleUp(WLAN_ROLE_AP,&RoleUpApParams , OSI_WAIT_FOR_SECOND * 10);


wlan_ap_role_down
-----------------

This command stops and removes an AP role.
During the process, a network interface is removed from the network stack (LwIP) and eventually an AP role is removed.

The API to remove a network interface in the ``network_lwip.c``  library::

.. code-block:: c

        void network_stack_remove_if_ap()

The API in the ``wifi_stack.a`` library:

.. code-block:: c

        int32_t ret = 0;
        ret = Wlan_RoleDown(WLAN_ROLE_AP, WLAN_WAIT_FOREVER);

wlan_scan
---------

This command allows to retrieve scan results from network processor.
During the process, the application initiates a scan request in an unsolicited manner.
When the scan results are ready, a scan event is triggered back to the application through an event callback registration.

The following is the API for WLAN scan in the ``wifi_stack.a`` library:

.. code-block:: c

        ScanCmd_t ScanParams;
        int32_t ret = 0;
        
        /* Call the command parser */
        memset(&ScanParams, 0x0, sizeof(ScanParams));
        ScanParams.numOfentries = MAX_SSID_ENTRIES;
        
        /* Clear the results buffer */
        memset(&app_CB.gDataBuffer, 0x0, sizeof(app_CB.gDataBuffer));
        scanCommon_t scanCommo;
        WlanRole_e      role;

        os_memset(&scanCommo, 0x0, sizeof(scanCommon_t));
        scanCommo.Band = BAND_SEL_BOTH;//options are BAND_SEL_ONLY_2_4GHZ , BAND_SEL_ONLY_5GHZ , BAND_SEL_BOTH
        
        role = WLAN_ROLE_STA;
        ScanParams.index = 0;
        ret = Wlan_Scan(role, &scanCommo, ScanParams.numOfentries);

wlan_connect
------------

This command initiates WLAN connection to an AP.
The parameters required for connection are the SSID, security type and the password.
The demos have a blocking timeout where the default is 40 seconds but can be modified by the application (via the ``WLAN_EVENT_TOUT`` define).
The expected events are triggered back to the application through an event callback registration.
Events could be ``WLAN_EVENT_CONNECT`` when initially disconnected and ``WLAN_EVENT_DISCONNECT`` prior to ``WLAN_EVENT_CONNECT`` when already connected.

The following is the API for WLAN connect in the ``wifi_stack.a`` library:

.. code-block:: c

        int32_t ret = 0;
        ConnectCmd_t ConnectParams;
        ConnectParams.secParams.Type = WLAN_SEC_TYPE_OPEN;

        ConnectParams.ssid = ssid;

        /* Connect to AP */
        ret = Wlan_Connect((const signed char *)(ConnectParams.ssid),
                        strlen((const char *)(ConnectParams.ssid)),
                        ConnectParams.bssid,//macAddr, empty by default
                        ConnectParams.secParams.Type,
                        (const char *)(ConnectParams.secParams.Key),
                        ((ConnectParams.secParams.Key != NULL) ? strlen((const char *)ConnectParams.secParams.Key) : 0),
                        0);

wlan_disconnect
---------------

This command initiates WLAN disconnection from an AP.
The expected event is triggered back to the application through an event callback registration.
Events should be ``WLAN_EVENT_DISCONNECT``.

The following is the API for WLAN disconnect in the ``wifi_stack.a`` library:

.. code-block:: c
        
        int32_t ret = 0;
        if(Connected)
        {
                ret = Wlan_Disconnect(WLAN_ROLE_STA,NULL);
        }

GET and SET
===========

wlan_get_fw
-----------

This command allows to retrieve the FW version of the radio core.

The following is the API for WLAN get in the ``wifi_stack.a`` library:

.. code-block:: c

        WlanFWVersions_t wlanFwVersions = {0};

        status = Wlan_Get(WLAN_GET_FWVERSION, (void *)&wlanFwVersions);
        if (status < 0)
        {
            return -1;
        }

        UART_PRINT("\t MAC:  %d.%d.%d.%d",
               wlanFwVersions.major_version, wlanFwVersions.minor_version,
               wlanFwVersions.api_version, wlanFwVersions.build_version);
        
        UART_PRINT("\t PHY:  %d.%d.%d.%d",
               wlanFwVersions.phy_version[0], wlanFwVersions.phy_version[1],
               wlanFwVersions.phy_version[2], wlanFwVersions.phy_version[3],
               wlanFwVersions.phy_version[4], wlanFwVersions.phy_version[5],
               wlanFwVersions.phy_version[6], wlanFwVersions.phy_version[7]);

wlan_get_mac
------------

This command allows to retrieve the mac address of the device.
The mac address is different for each role and the role needs to be up in order for this command to execute.

The following is the API for WLAN get in the ``wifi_stack.a`` library:

.. code-block:: c

        WlanMacAddress_t macAddressParams = {0};
        int8_t status = -1;

        /* Print device Mac address */
        status = Wlan_Get(WLAN_GET_MACADDRESS, (void *)&macAddressParams);
        if (status < 0)
        {
                return -1;
        }

        UART_PRINT("\t MAC address: %02x:%02x:%02x:%02x:%02x:%02x",
               macAddressParams.pMacAddress[0], macAddressParams.pMacAddress[1],
               macAddressParams.pMacAddress[2], macAddressParams.pMacAddress[3],
               macAddressParams.pMacAddress[4], macAddressParams.pMacAddress[5]);

wlan_set_mac
------------

This command allows to set the mac address of the device.
The mac address is different for each role and the role needs to be up in order for this command to execute.

The following is the API for WLAN set in the ``wifi_stack.a`` library:

.. code-block:: c

        WlanMacAddress_t macAddressParams;
        int16_t    ret = 0;
        memset(&macAddressParams, 0, sizeof(WlanMacAddress_t));

        /* Call the command parser */
        uint32_t tmpRoleId;
        ret = ParseSetMacAddressCmd(arg, macAddressParams.pMacAddress, &tmpRoleId);

        if (0 == ret)
        {
                macAddressParams.roleType = tmpRoleId;
        }

        ret = Wlan_Set(WLAN_SET_MACADDRESS, (void *)&macAddressParams);

        return (ret);

wlan_get_ps
-----------

This command allows to retrieve the power save of the device.
The power save can be either power save mode, Active mode or Automatic mode.

The following is the API for WLAN get in the ``wifi_stack.a`` library:

.. code-block:: c

        int16_t         ret = 0;
        WlanPowerSave_e currentPsMode;

        ret = Wlan_Get(WLAN_GET_POWER_SAVE,(void *)&currentPsMode);

        char *psMode;

        if(!ret)
        {
        switch(currentPsMode)
        {
        case WLAN_STATION_AUTO_PS_MODE:
        {
                psMode = "Auto Power save";
        }break;
        case WLAN_STATION_ACTIVE_MODE:
        {
                psMode = "Active mode";
        }break;
        case WLAN_STATION_POWER_SAVE_MODE:
        {
                psMode = "Power save mode";
        }break;
        default:
        {
                Report("\n\rPower save mode invalid!\n\r");
                return ret;
        }

        }
        Report("\n\r[PS MODE] current PS mode is %s", psMode);
        }

        return (ret);

wlan_set_ps
-----------

This command allows to set the power save of the device.
The power save can be either power save mode, Active mode or Automatic mode.

The following is the API for WLAN set in the ``wifi_stack.a`` library:

.. code-block:: c

        int16_t         ret = 0;
        WlanPowerSave_e PsMode;

        if(ret < 0)
        {
                return ret;
        }

        ret = Wlan_Set(WLAN_SET_POWER_SAVE, (void *)&PsMode);

        if(ret < 0)
        {
                Report("\n\r[PS MODE] Failed to set PS mode %d\n\r", PsMode);
        }
        else
        {
                Report("\n\r[PS MODE] Successfully set PS mode %d\n\r", PsMode);
        }

        return (ret);


wlan_set_pm
-----------

This command allows to set the power management mode of the device.
The power save can be either ELP mode (Extreme Low Power), Active mode (fully awake) or Power Down mode (hybrid).

The following is the API for WLAN set in the ``wifi_stack.a`` library:

.. code-block:: c

        int16_t               ret = 0;
        WlanPowerManagement_e PmMode;

        if(ret < 0)
        {
                return ret;
        }

        ret = Wlan_Set(WLAN_SET_POWER_MANAGEMENT, (void *)&PmMode);

        if(ret < 0)
        {
                Report("\n\r[PM MODE] Failed to set PM mode %d\n\r", PmMode);
        }
        else
        {
                Report("\n\r[PM MODE] Successfully set PM mode %d\n\r", PmMode);
        }

        return (ret);


wlan_set_LSI
------------

This command allows to set the LSI (Long Sleep Interval) mode of the device.
In LSI mode, the device will only wake up for a single broadcast period within the time interval specified in this command.
Therefore, the device is able to reduce power consumption with the tradeoff of possibly missing broadcast data on the network.

The following is the API for WLAN set in the ``wifi_stack.a`` library:

.. code-block:: c

        int16_t               ret = 0;
        WlanLongSleepInterval LsiParams;

        if(ret < 0)
        {
                return ret;
        }

        ret = Wlan_Set(WLAN_SET_LSI, (void *)&LsiParams);

        if(ret < 0)
        {
                Report("\n\r[SET LSI] Failed to set LSI %d\n\r", LsiParams.ListenInterval);
        }
        else
        {
                Report("\n\r[SET LSI] Successfully set LSI to %d\n\r", LsiParams.ListenInterval);
        }

        return (ret);