Using FreeRTOS with CCS
-----------------------

The FreeRTOS Kernel is configured through the SysConfig tool. This is used to enable and disable modules as well as configure device-specific settings. SysConfig will generate three files, and contribute to one more as part of the application project:

#.  `ti_freertos_config.c` : Contains the source code that is to be compiled for FreeRTOS. This is done by inserting preprocessor statements to `#include` the C files of all selected modules. The file
    also contains several hooks used to enable and disable FreeRTOS features such as Queue registration in TI code.

#.  `ti_freertos_portable_config.c` : This file contains all C code for the application's architecture and toolchain specific port.

#.  `ti_utils_build_linker.cmd.genlibs` : The ports of some architecture and toolchain combinations use assembly files. We compile these into prebuilt libraries. This is because we cannot `#include` assembly files safely. These libraries are then added to the linker invocation through an entry in the ti_utils_build_linker.cmd.genlibs file.

#.  `FreeRTOSConfig.h` : This is the standard FreeRTOS configuration header file that your application will typically `#include`. The entries in this file will change depending on the device and settings selected in SysConfig. You no longer need to edit FreeRTOSConfig.h
yourself. SysConfig will maintain it for you.
If you would like to change a FreeRTOS feature or setting that is not exposed in SysConfig, you can remove this file from SysConfig and maintain it yourself.

Changing the FreeRTOS Configuration
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

As with all SysConfig modules, you can either edit their configuration via the SysConfig GUI or by editing the .syscfg file directly in a text editor.

Since the FreeRTOS configuration is stored in a project's .syscfg file, each project has its own FreeRTOS configuration. Changing one project's configuration will not impact another project's configuration.

Why might you want to change the default FreeRTOS configuration?

    * Reduce the code footprint. For example, you might decrease the heap size or disable Software Timers.
    * Enable debug options. For example, you might add Assert checking to the configuration.