WiFi F3 SimpleLink Core SDK Change Log
Table of Contents
- Core SDK 9.20.01 GA (Jan, 2026)
- Fixed Issues
- Core SDK 9.20.00 GA (Dec, 2025)
- Fixed Issues
- Core SDK 9.10.00 EA (Mar, 2025)
- Fixed Issues
- Core SDK 8.41.00 EA (Dec, 2024)
- Fixed Issues
- Core SDK 8.40.00 GA (Dec, 2024)
- Fixed Issues
- Core SDK 8.30.00 EA (Oct, 2024)
- Fixed Issues
- Core SDK 8.21.00 EA (August, 2024)
- Fixed Issues
- Known Issues
- Core SDK 8.20.00 EA (June, 2024)
- Fixed Issues
- Known Issues
Core SDK 9.20.01 GA (Jan, 2026)
New Features
| ID | Summary |
|---|---|
| LPRFSEC-256 | Enable usage of hash length > curve length in ECDSA Driver |
Fixed Issues
| ID | Summary |
|---|---|
| TIDRIVERS-7639 | Fixed bit Misalignment in ExceptionArmV8M.c within the Exception module |
| LPRFSEC-253 | Fixed an issue where psa_mac_abort() would return an error instead of invoking mbedtls when using SW crypto |
Core SDK 9.20.00 GA (Dec, 2025)
New Features
| ID | Summary |
|---|---|
| TIDRIVERS-7539 | Update linker file for CC35X1E |
| TIDRIVERS-7503 | [CC35XX] Update number of Interrupt levels and priorities |
| TIDRIVERS-7502 | [CC35XX] Enable support for longer ADC sample duration |
| TIDRIVERS-7501 | [CC35XX] Enable the 3rd instance of the UART module |
| TIDRIVERS-7481 | [CC35XX] Clear ADC int. event flags before starting ADC convert |
| TIDRIVERS-7470 | Fix XMEM write post verify operation |
| TIDRIVERS-7387 | [CC35xx]: Expand XMEM and FLASH driver configuration and add multi-handler support“ |
| TIDRIVERS-7246 | Add ITM driver for CC35XX |
| TIDRIVERS-6778 | [CC35XX] Implement SDMMC driver |
| LPRFXXWARE-1074 | CC35XX: Align cc35xx.h with hw_ints.h |
| LPRFXXWARE-1065 | [CC35XX] ADC sample clock must be enabled for device revision 2.0 |
| LPRFXXWARE-1052 | [CC35XX] Remove HIF driverlib module |
| LPRFSEC-229 | PSA APIs accept unaligned addresses |
| LPRFSEC-215 | Unenforce psa_set_key_bits() before psa_import_key() |
| LPRFSEC-212 | Support concurrent PSA drivers for non-AES + AESECB |
| LPRFSEC-206 | Remove HSM Firewall Register write in HSMXXF3_init() |
| LPRFSEC-201 | Allow creation of HSM Asset Store keys without key ID input |
| LPRFSEC-197 | Force KeyStore SysConfig module when any Crypto Driver is added |
| LPRFSEC-195 | Rename HSMLPF3_provisionHUK() to HSMXXF3_provisionHUK() |
| LPRFSEC-194 | Enable various mbedTLS SW Crypto algs via PSA |
| LPRFSEC-193 | Reduce KeyStore DRAM usage |
| LPRFSEC-105 | Change some crypto driver prefixes to XXF3 from LPF3 to support both LPF3 and WFF3 |
| LPRFSEC-104 | Enable EdDSA driver for CC35XX devices |
Fixed Issues
| ID | Summary |
|---|---|
| TIDRIVERS-7557 | Application is unstable and may crash when CM33 exits deep sleep while Wi-Fi is connected. |
| TIDRIVERS-7552 | [CC35XX] Update device name used in the board file for LP_EM_CC35X1 |
| TIDRIVERS-7525 | [CC35XX] XMEM Init needs to be atomic |
| TIDRIVERS-7504 | Copy of RAM functions from flash to RAM in GCC |
| TIDRIVERS-7289 | Rename board CC35X1_LAUNCHXL to LP_EM_CC35X1 |
| LPRFXXWARE-1073 | CC35XX: Wrong interrupt priority bit number in cc35xx.h and hw_ints.h |
| LPRFXXWARE-1013 | CC35XX: Top level register documentation overview is missing |
| LPRFSEC-250 | PSA EDDSA+AES CBC,CCM,GCM,CMAC,CTR lack concurrent operation support |
| LPRFSEC-219 | psa_xxx_abort() fails before any call to psa_xxx_setup() |
| LPRFSEC-216 | ECDSA verification fails with PSA_ALG_ECDSA_ANY |
Core SDK 9.10.00 EA (Mar, 2025)
New Features
| ID | Summary |
|---|---|
| TIDRIVERS-7241 | Update LED-driver documentation |
| TIDRIVERS-7110 | Enable AES CMAC driver for CC35XX |
| TIDRIVERS-7100 | Enable SHA2 driver for CC35XX |
| TIDRIVERS-7099 | Enable AES CTR driver for CC35XX |
| TIDRIVERS-7097 | Add Watchdog driver for CC35XX |
| TIDRIVERS-7059 | Add SDIO driver for CC35XX |
| TIDRIVERS-7006 | Enable AES CCM driver to CC35XX |
| TIDRIVERS-6681 | Add ADC driver for CC35XX |
| TIDRIVERS-6249 | Enable CC23xx/CC27xx display example |
| TIDRIVERS-5830 | Enable Link Time Optimization in all CoreSDK libraries |
Fixed Issues
| ID | Summary |
|---|---|
| TIDRIVERS-7252 | Display SysConfig module allows selection of unsupported Display Type |
| TIDRIVERS-7232 | Selecting RAM as NVS type does not generate CONFIG_NVS_N identifier |
| TIDRIVERS-7221 | WFF3 post-build steps should not contain semicolons |
| TIDRIVERS-7157 | UART2_open() does not use default parameters if params pointer is NULL |
| TIDRIVERS-7146 | APU: Jacobi EVD returns the correct eigenvalues but not accurate enough eigenvectors for smaller eigenvalues |
Core SDK 8.41.00 EA (Dec, 2024)
New Features
| ID | Summary |
|---|---|
| TIDRIVERS-7025 | Use LPF3 AES CBC driver for CC35XX |
| TIDRIVERS-7024 | Use LPF3 AES GCM driver for CC35XX |
| TIDRIVERS-7000 | Use LPF3 AES ECB driver for CC35XX |
| TIDRIVERS-6549 | [CC35xx] Add FLASH capabilities |
Fixed Issues
| ID | Summary |
|---|---|
| None | None |
Core SDK 8.40.00 GA (Dec, 2024)
New Features
| ID | Summary |
|---|---|
| TIDRIVERS-6188 | Add support for instrumented exception handlers |
Fixed Issues
| ID | Summary |
|---|---|
| FREERTOS-41 | [CC27XX] Incorrect BASEPRI settings during critical section for IAR |
Core SDK 8.30.00 EA (Oct, 2024)
New Features
| ID | Summary |
|---|---|
| TIUTILS-135 | Add tilogger support for saving LogPackets to file and replaying from file |
| TIUTILS-112 | Add tilogger support for writing decoded Log records to stdout |
| TIPOSIX-30 | Return error when POSIX timer overflows FreeRTOS ticks |
| TIDRIVERS-6641 | Add BP-EM-CS Boosterpack |
| TIDRIVERS-6562 | Update GCC version to 12.3 |
| TIDRIVERS-6543 | Create a crystal hardware component definition |
| TIDRIVERS-6509 | Hide GPIO Configurations in SysConfig module if marked as do not configure. |
| TIDRIVERS-6342 | Add support for 64-bit getSystemTicks API |
| TIDRIVERS-6250 | CC27xx: Enable portable and portableNative demos |
| TIDRIVERS-6232 | Add optional temperature compensation for CLKSVT on CC27XX (SWTCXO) |
| TIDRIVERS-6018 | Add ADCBuf support for LPF3 |
| FREERTOS-34 | Add ability to define priority of the FreeRTOS timer task |
Fixed Issues
| ID | Summary |
|---|---|
| TIDRIVERS-7010 | LP_EM_CC2674P10: Wrong RF antenna switch pin muxing in board metadata |
| TIDRIVERS-6893 | The type (uint8_t) for the PWM Timer Prescaler can't hold max value of 256 |
| TIDRIVERS-6735 | UART2_EVENT_TX_BEGIN called several times in one transmit |
| TIDRIVERS-6127 | Add new power constraint to disallow/pause SWTCXO |
| TIDRIVERS-6008 | I2C_close causing glitch on SDA and SCL lines |
| FREERTOS-37 | Lowest interrupt priority is miscalculated |
Core SDK 8.21.00 EA (August, 2024)
New Features
| ID | Summary |
|---|---|
| TIDRIVERS-6717 | CC35XX: Add post build steps to examples for generating final image |
| TIDRIVERS-6666 | CC35XX: Port AES CCM driver |
| TIDRIVERS-6576 | CC35XX: Port ECDSA driver |
| TIDRIVERS-6574 | CC35XX: Port AES CBC driver |
| TIDRIVERS-6573 | CC35XX: Port AES GCM driver |
| TIDRIVERS-6564 | CC35XX: Add sleep policy function |
Fixed Issues
| ID | Summary |
|---|---|
| None | None |
Known Issues
| ID | Summary |
|---|---|
| None | None |
Core SDK 8.20.00 EA (June, 2024)
New Features
| ID | Summary |
|---|---|
| None | None |
Fixed Issues
| ID | Summary |
|---|---|
| None | None |
Known Issues
| ID | Summary |
|---|---|
| None | None |