Data Fields
EDDSAXXF3HSM_HWAttrs Struct Reference

EDDSAXXF3HSM Hardware Attributes. More...

#include <EDDSAXXF3HSM.h>

Data Fields

uint16_t reserved1
 

Detailed Description

EDDSAXXF3HSM Hardware Attributes.

EDDSAXXF3HSM hardware attributes should be included in the board file and pointed to by the EDDSA_config struct.

Field Documentation

§ reserved1

uint16_t EDDSAXXF3HSM_HWAttrs::reserved1

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale