![]() |
![]() |
AESECBXXF3 Object. More...
#include <AESECBXXF3.h>

Data Fields | |
| AESCommonXXF3_Object | common |
| AESECB_Operation * | operation |
| AESECB_CallbackFxn | callbackFxn |
| AESECB_OperationType | operationType |
| bool | threadSafe |
| const uint8_t * | input |
| uint8_t * | output |
| size_t | inputLength |
| size_t | totalDataLength |
| volatile size_t | totalDataLengthRemaining |
| int_fast16_t | hsmStatus |
| The status of the HSM Boot up process if HSMXXF3_STATUS_SUCCESS, the HSM booted properly. if HSMXXF3_STATUS_ERROR, the HSM did not boot properly. More... | |
| uint32_t | keyAssetID |
| uint32_t | keyLocation |
| bool | segmentedOperationInProgress |
AESECBXXF3 Object.
The application must not access any member variables of this structure!
| AESCommonXXF3_Object AESECBXXF3_Object::common |
| AESECB_Operation* AESECBXXF3_Object::operation |
| AESECB_CallbackFxn AESECBXXF3_Object::callbackFxn |
| AESECB_OperationType AESECBXXF3_Object::operationType |
| bool AESECBXXF3_Object::threadSafe |
| const uint8_t* AESECBXXF3_Object::input |
| uint8_t* AESECBXXF3_Object::output |
| size_t AESECBXXF3_Object::inputLength |
| size_t AESECBXXF3_Object::totalDataLength |
| volatile size_t AESECBXXF3_Object::totalDataLengthRemaining |
| int_fast16_t AESECBXXF3_Object::hsmStatus |
The status of the HSM Boot up process if HSMXXF3_STATUS_SUCCESS, the HSM booted properly. if HSMXXF3_STATUS_ERROR, the HSM did not boot properly.
| uint32_t AESECBXXF3_Object::keyAssetID |
| uint32_t AESECBXXF3_Object::keyLocation |
| bool AESECBXXF3_Object::segmentedOperationInProgress |