![]() |
![]() |
AESCommonXXF3 Object. More...
#include <AESCommonXXF3.h>

Data Fields | |
| uint32_t | semaphoreTimeout |
| CryptoKey | key |
| volatile int_fast16_t | returnStatus |
| AES_ReturnBehavior | returnBehavior |
| bool | isOpen |
| volatile bool | cryptoResourceLocked |
| volatile bool | operationInProgress |
| volatile bool | powerConstraintSet |
AESCommonXXF3 Object.
The application must not access any member variables of this structure!
| uint32_t AESCommonXXF3_Object::semaphoreTimeout |
| CryptoKey AESCommonXXF3_Object::key |
| volatile int_fast16_t AESCommonXXF3_Object::returnStatus |
| AES_ReturnBehavior AESCommonXXF3_Object::returnBehavior |
| bool AESCommonXXF3_Object::isOpen |
| volatile bool AESCommonXXF3_Object::cryptoResourceLocked |
| volatile bool AESCommonXXF3_Object::operationInProgress |
| volatile bool AESCommonXXF3_Object::powerConstraintSet |