Data Fields
AESCommonXXF3_HWAttrs Struct Reference

AESCommonXXF3 Hardware Attributes. More...

#include <AESCommonXXF3.h>

Data Fields

uint8_t intPriority
 Crypto Peripheral's interrupt priority. More...
 

Detailed Description

AESCommonXXF3 Hardware Attributes.

Field Documentation

§ intPriority

uint8_t AESCommonXXF3_HWAttrs::intPriority

Crypto Peripheral's interrupt priority.

The Low Power F3 devices use either three or two priority bits, depending on the device. That means ~0 has the same effect as (7 << 5) or (3 << 6), respectively.

Setting the priority to 0 is not supported by this driver.

HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale