Data Fields
AESCBC_OneStepOperation Struct Reference

Struct containing the parameters required for encrypting/decrypting a message in a single-step operation. More...

#include <AESCBC.h>

Collaboration diagram for AESCBC_OneStepOperation:
Collaboration graph
[legend]

Data Fields

CryptoKeykey
 
uint8_t * input
 
uint8_t * output
 
uint8_t * iv
 
size_t inputLength
 
bool ivInternallyGenerated
 

Detailed Description

Struct containing the parameters required for encrypting/decrypting a message in a single-step operation.

Field Documentation

§ key

CryptoKey* AESCBC_OneStepOperation::key

Pointer to a previously initialized CryptoKey.

§ input

uint8_t* AESCBC_OneStepOperation::input
  • Encryption: The plaintext buffer to be encrypted in the CBC operation.
  • Decryption: The ciphertext to be decrypted.

§ output

uint8_t* AESCBC_OneStepOperation::output
  • Encryption: The output ciphertext buffer that the encrypted plaintext is copied to.
  • Decryption: The plaintext derived from the decrypted ciphertext is copied here.

For CC27XX devices with _HSM-suffixed key encoding, the output buffer needs to be 32-bit aligned.

§ iv

uint8_t* AESCBC_OneStepOperation::iv

A buffer containing an IV. IVs must be unique to each CBC operation and may not be reused. If ivInternallyGenerated is set, the IV will be generated by AESCBC_oneStepEncrypt() and copied to this buffer.

§ inputLength

size_t AESCBC_OneStepOperation::inputLength

Length of the input buffer in bytes for one-step AES CBC operations. Must be a multiple of the AES block size (16 bytes). Also, the output buffer must be large enough to receive the same number of bytes. The user or application should take care of necessary padding. Max length supported may be limited depending on the return behavior.

§ ivInternallyGenerated

bool AESCBC_OneStepOperation::ivInternallyGenerated

When true, the IV buffer passed into AESCBC_oneStepEncrypt() will be overwritten with a randomly generated IV. Not supported by all implementations.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale