Functions | Variables
CryptoResourceXXF3.h File Reference

Detailed Description

Shared resources to arbitrate access to the AES engine.

============================================================================

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/dpl/HwiP.h>
Include dependency graph for CryptoResourceXXF3.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Functions

void CryptoResourceXXF3_constructRTOSObjects (void)
 
void CryptoResourceXXF3_destructRTOSObjects (void)
 
bool CryptoResourceXXF3_acquireLock (uint32_t timeout)
 
void CryptoResourceXXF3_releaseLock (void)
 

Variables

SemaphoreP_Struct CryptoResourceXXF3_accessSemaphore
 
SemaphoreP_Struct CryptoResourceXXF3_operationSemaphore
 
volatile bool CryptoResourceXXF3_pollingFlag
 
HwiP_Struct CryptoResourceXXF3_hwi
 

Function Documentation

§ CryptoResourceXXF3_constructRTOSObjects()

void CryptoResourceXXF3_constructRTOSObjects ( void  )

§ CryptoResourceXXF3_destructRTOSObjects()

void CryptoResourceXXF3_destructRTOSObjects ( void  )

§ CryptoResourceXXF3_acquireLock()

bool CryptoResourceXXF3_acquireLock ( uint32_t  timeout)

§ CryptoResourceXXF3_releaseLock()

void CryptoResourceXXF3_releaseLock ( void  )

Variable Documentation

§ CryptoResourceXXF3_accessSemaphore

SemaphoreP_Struct CryptoResourceXXF3_accessSemaphore

§ CryptoResourceXXF3_operationSemaphore

SemaphoreP_Struct CryptoResourceXXF3_operationSemaphore

§ CryptoResourceXXF3_pollingFlag

volatile bool CryptoResourceXXF3_pollingFlag

§ CryptoResourceXXF3_hwi

HwiP_Struct CryptoResourceXXF3_hwi
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale