Data Structures | Macros | Functions | Variables
CryptoKeyKeyStore_PSA_helpers.h File Reference

Detailed Description

CryptoKeyKeyStore driver header.


Overview

The CryptoKeyKeyStore driver provides API to initialize keys and get plaintext keys from KeyStore. This file provides definitions that are only available to the the secure side, in both TF-M disabled and TF-M enabled environments.

#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKeyKeyStore_PSA.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/devices/DeviceFamily.h>
#include <third_party/mbedtls/library/psa_crypto_core.h>
#include <third_party/mbedtls/library/psa_crypto_slot_management.h>
#include <third_party/mbedtls/library/psa_crypto_storage.h>
Include dependency graph for CryptoKeyKeyStore_PSA_helpers.h:

Go to the source code of this file.

Data Structures

struct  KeyStore_accessSemaphoreObject
 

Macros

#define FLETCHER_CHECKSUM_ALGORITHM   32 /* FLETCHER-32 */
 

Functions

int_fast16_t KeyStore_PSA_getKey (KeyStore_PSA_KeyFileId key, uint8_t *data, size_t dataSize, size_t *dataLength, KeyStore_PSA_Algorithm alg, KeyStore_PSA_KeyUsage usage)
 Get the plaintext key in binary format. More...
 
bool KeyStore_acquireLock (void)
 Attempt to acquire lock to access KeyStore. This function is used to synchronize drivers and the application when both are attempting to use KeyStore. For example, if a driver is retrieving key material from a key slot to perform an operation, it must be protected from the application making a call to psa_destroy_key() on that same slot. More...
 
void KeyStore_releaseLock (void)
 Release lock to access KeyStore. More...
 
int_fast16_t KeyStore_PSA_retrieveFromKeyStore (const CryptoKey *key, uint8_t *keyBuffer, size_t keyBufferSize, uint32_t *keyAssetID, KeyStore_PSA_Algorithm targetAlg, KeyStore_PSA_KeyUsage targetUsage)
 Retrieve the key in either plaintext format or as an Asset ID. More...
 
int_fast16_t KeyStore_PSA_getKeyAssetId (KeyStore_PSA_KeyFileId key, uint32_t *const pAssetId, KeyStore_PSA_Algorithm targetAlg, KeyStore_PSA_KeyUsage targetUsage)
 Get the asset ID for a given key ID. More...
 
int_fast16_t KeyStore_PSA_init (void)
 Initialize the Key Store. More...
 

Variables

KeyStore_accessSemaphoreObject KeyStore_semaphoreObject
 

Macro Definition Documentation

§ FLETCHER_CHECKSUM_ALGORITHM

#define FLETCHER_CHECKSUM_ALGORITHM   32 /* FLETCHER-32 */

Function Documentation

§ KeyStore_PSA_getKey()

int_fast16_t KeyStore_PSA_getKey ( KeyStore_PSA_KeyFileId  key,
uint8_t *  data,
size_t  dataSize,
size_t *  dataLength,
KeyStore_PSA_Algorithm  alg,
KeyStore_PSA_KeyUsage  usage 
)

Get the plaintext key in binary format.

This function can only be called on secure side of SPM. It is used by SL crypto drivers to obtain plaintext keys, using keyIDs provided by non-secure application, which will be loaded onto crypto engine

Implementations must reject an attempt to import a certificate of size 0.

Parameters
[in]keyThe key ID for the key in keystore.
[out]dataOn success, the buffer contains the plaintext key
[in]dataSizeSize of the data buffer in bytes. It must be greater than or equal to the plaintext key material
[out]dataLengthSize of the returned key material in bytes.
[in]algAlgorithm the key will be used for, it should match the orignal alg used to import the key.
[in]usageKey usage, it must match the original usage used to import the key.
Return values
KEYSTORE_PSA_STATUS_SUCCESSSuccess. If the key ID exists, matches the alg and usage , and the dataSize is sufficient the key is returned in data
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLEIf the KeyStore lock cannot be acquired, the KeyStore module is in use elsewhere.
KEYSTORE_PSA_STATUS_INVALID_KEY_IDThe key identifier does not exist.
KEYSTORE_PSA_STATUS_NOT_PERMITTEDThe key does not have matching alg and usage
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_acquireLock()

bool KeyStore_acquireLock ( void  )

Attempt to acquire lock to access KeyStore. This function is used to synchronize drivers and the application when both are attempting to use KeyStore. For example, if a driver is retrieving key material from a key slot to perform an operation, it must be protected from the application making a call to psa_destroy_key() on that same slot.

Return values
trueSuccessfully acquired lock
falseFailed to acquire lock

§ KeyStore_releaseLock()

void KeyStore_releaseLock ( void  )

Release lock to access KeyStore.

Once done accessing KeyStore, either the CryptoKeyKeyStore_PSA_helpers APIs or the PSA Crypto APIs should release this lock so that other entities can use KeyStore.

§ KeyStore_PSA_retrieveFromKeyStore()

int_fast16_t KeyStore_PSA_retrieveFromKeyStore ( const CryptoKey key,
uint8_t *  keyBuffer,
size_t  keyBufferSize,
uint32_t *  keyAssetID,
KeyStore_PSA_Algorithm  targetAlg,
KeyStore_PSA_KeyUsage  targetUsage 
)

Retrieve the key in either plaintext format or as an Asset ID.

This function handles the logic of retrieving a key from CC27XX/CC35XX KeyStore, which depends both on the CryptoKey encoding and the key lifetime/location. If the key location is KEYSTORE_PSA_KEY_LOCATION_HSM_ASSET_STORE, then the key will be returned via asset ID. If the requested key was not already in the asset store upon request, it will be loaded before the asset ID is returned.

Parameters
[in]keyPointer to the CryptoKey object containing the encoding and keyID
[out]keyBufferBuffer in which to place the key if it is retrievable in plaintext
[in]keyBufferSizeSize of the provided buffer
[out]keyAssetIDPointer to keyAssetID output, if the key location is HSM_ASSET_STORE
[in]targetAlgDesired algorithm to use the key for. Before retrieving the key material, it must be verified that it is allowed to be used for a given algorithm.
[in]targetUsageDesired usage of the resulting key - only necessary for symmetric keys that will be returned as HSM assets. Must be one of KEYSTORE_PSA_KEY_USAGE_ENCRYPT or KEYSTORE_PSA_KEY_USAGE_DECRYPT.
Return values
KEYSTORE_PSA_STATUS_SUCCESS
KEYSTORE_PSA_STATUS_GENERIC_ERRORThe key length retrieved from KeyStore doesn't match the expected length. Or, other generic error.
KEYSTORE_PSA_STATUS_NOT_SUPPORTEDThe CryptoKey encoding has an unexpected/unsupported value.
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLE
KEYSTORE_PSA_STATUS_INVALID_KEY_IDThe key identifier does not exist.
KEYSTORE_PSA_STATUS_NOT_PERMITTEDThe key does not have matching alg and usage
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_PSA_getKeyAssetId()

int_fast16_t KeyStore_PSA_getKeyAssetId ( KeyStore_PSA_KeyFileId  key,
uint32_t *const  pAssetId,
KeyStore_PSA_Algorithm  targetAlg,
KeyStore_PSA_KeyUsage  targetUsage 
)

Get the asset ID for a given key ID.

This function can only be called on secure side of SPM. It is used by SL crypto drivers to obtain assetIDs to refer to keys in the HSM, using keyIDs provided by non-secure application. The asset ID can then be used directly with the HSM for a crypto operation.

If the key is not already stored in the HSM's Asset Store, this function will perform that allocation and load before returning the new asset ID.

Parameters
[in]keyThe key ID for the key in keystore.
[out]pAssetIdOn success, the asset ID for the corresponding key ID
[in]targetAlgDesired algorithm to use the key for. Before retrieving the key asset, it must be verified that it is allowed to be used for a given algorithm.
[in]targetUsageDesired usage of the resulting asset - only used for symmetric keys. Must be one of KEYSTORE_PSA_KEY_USAGE_ENCRYPT or KEYSTORE_PSA_KEY_USAGE_DECRYPT.
Return values
KEYSTORE_PSA_STATUS_SUCCESSSuccess. If the key ID exists, the asset ID is returned in pAssetId
KEYSTORE_PSA_STATUS_RESOURCE_UNAVAILABLEIf the KeyStore lock cannot be acquired, the KeyStore module is in use elsewhere.
KEYSTORE_PSA_STATUS_INVALID_KEY_IDThe key identifier does not exist.
KEYSTORE_PSA_STATUS_NOT_PERMITTEDThe provided pAssetId is NULL
KEYSTORE_PSA_STATUS_BAD_STATEThe library has not been previously initialized by KeyStore_PSA_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ KeyStore_PSA_init()

int_fast16_t KeyStore_PSA_init ( void  )

Initialize the Key Store.

Applications must call this function before calling any other function in this module. This function will initialize key slot memory and load the key IDs of any preprovisioned keys.

Return values
KEYSTORE_PSA_STATUS_SUCCESSSuccess.
KEYSTORE_PSA_STATUS_GENERIC_ERRORtfm_its_init() failed
KEYSTORE_PSA_STATUS_DOES_NOT_EXISTKeyStore_PSA_getPreProvisionedKeyIDs() failed

Variable Documentation

§ KeyStore_semaphoreObject

KeyStore_accessSemaphoreObject KeyStore_semaphoreObject
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale