Data Structures | Macros | Typedefs
AESCTRXXF3.h File Reference

Detailed Description

AESCTR driver implementation for the Low Power F3 family.

==========================================================================

Hardware Accelerator

The Low Power F3 and WiFi F3 families of devices have dedicated hardware accelerators. CC23XX devices have one dedicated accelerator whereas CC27XX devices have two (Primary and Secondary). Combined they can perform AES encryption operations with 128-bit, 192-bit and 256-bit keys. CC35XX devices have only one dedicated hardware accelerator. Only one operation can be carried out on the accelerator at a time. Mutual exclusion is implemented at the driver level and coordinated between all drivers relying on the accelerator. It is transparent to the application and only noted to ensure sensible access timeouts are set.

Implementation Limitations

Runtime Parameter Validation

The driver implementation does not perform runtime checks for most input parameters. Only values that are likely to have a stochastic element to them are checked (such as whether a driver is already open). Higher input parameter validation coverage is achieved by turning on assertions when compiling the driver.

#include <stdbool.h>
#include <stdint.h>
#include <ti/drivers/AESCTR.h>
#include <ti/drivers/cryptoutils/aes/AESCommonXXF3.h>
#include <ti/drivers/cryptoutils/sharedresources/CryptoResourceXXF3.h>
#include <ti/devices/DeviceFamily.h>
Include dependency graph for AESCTRXXF3.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  AESCTRXXF3_Object
 AESCTRXXF3 Object. More...
 

Macros

#define AESCTRXXF3_DEFAULT_AUTOCFG
 
#define AESCTRXXF3_LAST_BLOCK_AUTOCFG
 

Typedefs

typedef AESCommonXXF3_HWAttrs AESCTRXXF3_HWAttrs
 AESCTRXXF3 Hardware Attributes. More...
 

Macro Definition Documentation

§ AESCTRXXF3_DEFAULT_AUTOCFG

#define AESCTRXXF3_DEFAULT_AUTOCFG
Value:
((uint32_t)AES_AUTOCFG_AESSRC_BUF | (uint32_t)AES_AUTOCFG_TRGAES_WRBUF3S | \
(uint32_t)AES_AUTOCFG_TRGAES_RDTXT3 | (uint32_t)AES_AUTOCFG_CTRSIZE_CTR128 | \
(uint32_t)AES_AUTOCFG_CTRENDN_BIGENDIAN | (uint32_t)AES_AUTOCFG_BUSHALT_EN)

§ AESCTRXXF3_LAST_BLOCK_AUTOCFG

#define AESCTRXXF3_LAST_BLOCK_AUTOCFG
Value:
((uint32_t)AES_AUTOCFG_AESSRC_BUF | (uint32_t)AES_AUTOCFG_TRGAES_WRBUF3S | \
(uint32_t)AES_AUTOCFG_CTRSIZE_CTR128 | (uint32_t)AES_AUTOCFG_CTRENDN_BIGENDIAN | \
(uint32_t)AES_AUTOCFG_BUSHALT_EN)

Typedef Documentation

§ AESCTRXXF3_HWAttrs

AESCTRXXF3 Hardware Attributes.

AESCTRXXF3 hardware attributes should be included in the board file and pointed to by the AESCTR_config struct.

© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale