Data Fields
psa_cipher_operation_s Struct Reference

#include <crypto_struct.h>

Collaboration diagram for psa_cipher_operation_s:
Collaboration graph
[legend]

Data Fields

unsigned int id
 
unsigned int iv_required:1
 
unsigned int iv_set:1
 
unsigned int is_encrypt:1
 
unsigned int in_error_state:1
 
size_t default_iv_length
 
psa_algorithm_t alg
 
size_t unprocessed_len
 
uint8_t unprocessed_data [PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE]
 
uint8_t * curr_unprocessed_data
 
CryptoKey cryptoKey
 

Field Documentation

§ id

unsigned int psa_cipher_operation_s::id

Unique ID indicating which driver got assigned to do the operation. Since driver contexts are driver-specific, swapping drivers halfway through the operation is not supported. ID values are auto-generated in psa_crypto_driver_wrappers.h ID value zero means the context is not valid or not assigned to any driver (i.e. none of the driver contexts are active).

§ iv_required

unsigned int psa_cipher_operation_s::iv_required

§ iv_set

unsigned int psa_cipher_operation_s::iv_set

§ is_encrypt

unsigned int psa_cipher_operation_s::is_encrypt

§ in_error_state

unsigned int psa_cipher_operation_s::in_error_state

§ default_iv_length

size_t psa_cipher_operation_s::default_iv_length

§ alg

psa_algorithm_t psa_cipher_operation_s::alg

§ unprocessed_len

size_t psa_cipher_operation_s::unprocessed_len

Number of bytes that have not been processed yet

§ unprocessed_data

uint8_t psa_cipher_operation_s::unprocessed_data[PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE]

§ curr_unprocessed_data

uint8_t* psa_cipher_operation_s::curr_unprocessed_data

§ cryptoKey

CryptoKey psa_cipher_operation_s::cryptoKey

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale