Data Fields
psa_aead_operation_s Struct Reference

#include <crypto_struct.h>

Collaboration diagram for psa_aead_operation_s:
Collaboration graph
[legend]

Data Fields

unsigned int id
 
psa_algorithm_t alg
 
unsigned int iv_set:1
 
unsigned int in_error_state:1
 
size_t adLength
 
size_t plaintextLength
 
size_t runningADLength
 
size_t runningPlaintextLength
 
size_t tagSize
 
uint8_t unprocessedData [PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE]
 
uint8_t * curr_unprocessed_data
 
size_t unprocessed_len
 
CryptoKey cryptoKey
 
bool done_updating_ad
 
bool length_set
 

Field Documentation

§ id

unsigned int psa_aead_operation_s::id

Unique ID indicating which driver got assigned to do the operation. Since driver contexts are driver-specific, swapping drivers halfway through the operation is not supported. ID values are auto-generated in psa_driver_wrappers.h ID value zero means the context is not valid or not assigned to any driver (i.e. none of the driver contexts are active).

§ alg

psa_algorithm_t psa_aead_operation_s::alg

§ iv_set

unsigned int psa_aead_operation_s::iv_set

§ in_error_state

unsigned int psa_aead_operation_s::in_error_state

§ adLength

size_t psa_aead_operation_s::adLength

§ plaintextLength

size_t psa_aead_operation_s::plaintextLength

§ runningADLength

size_t psa_aead_operation_s::runningADLength

§ runningPlaintextLength

size_t psa_aead_operation_s::runningPlaintextLength

§ tagSize

size_t psa_aead_operation_s::tagSize

§ unprocessedData

uint8_t psa_aead_operation_s::unprocessedData[PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE]

§ curr_unprocessed_data

uint8_t* psa_aead_operation_s::curr_unprocessed_data

§ unprocessed_len

size_t psa_aead_operation_s::unprocessed_len

§ cryptoKey

CryptoKey psa_aead_operation_s::cryptoKey

§ done_updating_ad

bool psa_aead_operation_s::done_updating_ad

§ length_set

bool psa_aead_operation_s::length_set

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale