Macros
Interruptible operations

Macros

#define PSA_INTERRUPTIBLE_MAX_OPS_UNLIMITED   UINT32_MAX
 

Detailed Description

Macro Definition Documentation

§ PSA_INTERRUPTIBLE_MAX_OPS_UNLIMITED

#define PSA_INTERRUPTIBLE_MAX_OPS_UNLIMITED   UINT32_MAX

Maximum value for use with psa_interruptible_set_max_ops() to determine the maximum number of ops allowed to be executed by an interruptible function in a single call.

© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale