Value:(!(((aead_alg_1) ^ (aead_alg_2)) & \
#define PSA_ALG_AEAD_TAG_LENGTH_MASK
Definition: crypto_values.h:1343
#define PSA_ALG_AEAD_AT_LEAST_THIS_LENGTH_FLAG
Definition: crypto_values.h:1352
Check if two AEAD algorithm identifiers refer to the same AEAD algorithm regardless of the tag length they encode.
- Parameters
-
| aead_alg_1 | An AEAD algorithm identifier. |
| aead_alg_2 | An AEAD algorithm identifier. |
- Returns
- 1 if both identifiers refer to the same AEAD algorithm, 0 otherwise. Unspecified if neither
aead_alg_1 nor aead_alg_2 are a supported AEAD algorithm.