![]() |
![]() |
Macros | |
| #define | PSA_HASH_OPERATION_INIT |
Typedefs | |
| typedef struct psa_hash_operation_s | psa_hash_operation_t |
Functions | |
| psa_status_t | psa_hash_compute (psa_algorithm_t alg, const uint8_t *input, size_t input_length, uint8_t *hash, size_t hash_size, size_t *hash_length) |
| psa_status_t | psa_hash_compare (psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *hash, size_t hash_length) |
| static psa_hash_operation_t | psa_hash_operation_init (void) |
| psa_status_t | psa_hash_setup (psa_hash_operation_t *operation, psa_algorithm_t alg) |
| psa_status_t | psa_hash_update (psa_hash_operation_t *operation, const uint8_t *input, size_t input_length) |
| psa_status_t | psa_hash_finish (psa_hash_operation_t *operation, uint8_t *hash, size_t hash_size, size_t *hash_length) |
| psa_status_t | psa_hash_verify (psa_hash_operation_t *operation, const uint8_t *hash, size_t hash_length) |
| psa_status_t | psa_hash_abort (psa_hash_operation_t *operation) |
| psa_status_t | psa_hash_clone (const psa_hash_operation_t *source_operation, psa_hash_operation_t *target_operation) |
| #define PSA_HASH_OPERATION_INIT |
This macro returns a suitable initializer for a hash operation object of type psa_hash_operation_t.
Referenced by psa_hash_operation_init().
| typedef struct psa_hash_operation_s psa_hash_operation_t |
The type of the state data structure for multipart hash operations.
Before calling any function on a hash operation object, the application must initialize it by any of the following means:
This is an implementation-defined struct. Applications should not make any assumptions about the content of this structure. Implementation details can change in future versions without notice.
| psa_status_t psa_hash_compute | ( | psa_algorithm_t | alg, |
| const uint8_t * | input, | ||
| size_t | input_length, | ||
| uint8_t * | hash, | ||
| size_t | hash_size, | ||
| size_t * | hash_length | ||
| ) |
Calculate the hash (digest) of a message.
| alg | The hash algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(alg) is true). | |
| [in] | input | Buffer containing the message to hash. |
| input_length | Size of the input buffer in bytes. | |
| [out] | hash | Buffer where the hash is to be written. |
| hash_size | Size of the hash buffer in bytes. | |
| [out] | hash_length | On success, the number of bytes that make up the hash value. This is always PSA_HASH_LENGTH(alg). |
| PSA_SUCCESS | Success. |
| PSA_ERROR_NOT_SUPPORTED | alg is not supported or is not a hash algorithm. |
| PSA_ERROR_INVALID_ARGUMENT | |
| PSA_ERROR_BUFFER_TOO_SMALL | hash_size is too small |
| PSA_ERROR_INSUFFICIENT_MEMORY | |
| PSA_ERROR_COMMUNICATION_FAILURE | |
| PSA_ERROR_HARDWARE_FAILURE | |
| PSA_ERROR_CORRUPTION_DETECTED | |
| PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_hash_compare | ( | psa_algorithm_t | alg, |
| const uint8_t * | input, | ||
| size_t | input_length, | ||
| const uint8_t * | hash, | ||
| size_t | hash_length | ||
| ) |
Calculate the hash (digest) of a message and compare it with a reference value.
| alg | The hash algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(alg) is true). | |
| [in] | input | Buffer containing the message to hash. |
| input_length | Size of the input buffer in bytes. | |
| [out] | hash | Buffer containing the expected hash value. |
| hash_length | Size of the hash buffer in bytes. |
| PSA_SUCCESS | The expected hash is identical to the actual hash of the input. |
| PSA_ERROR_INVALID_SIGNATURE | The hash of the message was calculated successfully, but it differs from the expected hash. |
| PSA_ERROR_NOT_SUPPORTED | alg is not supported or is not a hash algorithm. |
| PSA_ERROR_INVALID_ARGUMENT | input_length or hash_length do not match the hash size for alg |
| PSA_ERROR_INSUFFICIENT_MEMORY | |
| PSA_ERROR_COMMUNICATION_FAILURE | |
| PSA_ERROR_HARDWARE_FAILURE | |
| PSA_ERROR_CORRUPTION_DETECTED | |
| PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
|
static |
Return an initial value for a hash operation object.
| psa_status_t psa_hash_setup | ( | psa_hash_operation_t * | operation, |
| psa_algorithm_t | alg | ||
| ) |
Set up a multipart hash operation.
The sequence of operations to calculate a hash (message digest) is as follows:
If an error occurs at any step after a call to psa_hash_setup(), the operation will need to be reset by a call to psa_hash_abort(). The application may call psa_hash_abort() at any time after the operation has been initialized.
After a successful call to psa_hash_setup(), the application must eventually terminate the operation. The following events terminate an operation:
| [in,out] | operation | The operation object to set up. It must have been initialized as per the documentation for psa_hash_operation_t and not yet in use. |
| alg | The hash algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(alg) is true). |
| PSA_SUCCESS | Success. |
| PSA_ERROR_NOT_SUPPORTED | alg is not a supported hash algorithm. |
| PSA_ERROR_INVALID_ARGUMENT | alg is not a hash algorithm. |
| PSA_ERROR_INSUFFICIENT_MEMORY | |
| PSA_ERROR_COMMUNICATION_FAILURE | |
| PSA_ERROR_HARDWARE_FAILURE | |
| PSA_ERROR_CORRUPTION_DETECTED | |
| PSA_ERROR_BAD_STATE | The operation state is not valid (it must be inactive), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_hash_update | ( | psa_hash_operation_t * | operation, |
| const uint8_t * | input, | ||
| size_t | input_length | ||
| ) |
Add a message fragment to a multipart hash operation.
The application must call psa_hash_setup() before calling this function.
If this function returns an error status, the operation enters an error state and must be aborted by calling psa_hash_abort().
| [in,out] | operation | Active hash operation. |
| [in] | input | Buffer containing the message fragment to hash. |
| input_length | Size of the input buffer in bytes. |
| PSA_SUCCESS | Success. |
| PSA_ERROR_INSUFFICIENT_MEMORY | |
| PSA_ERROR_COMMUNICATION_FAILURE | |
| PSA_ERROR_HARDWARE_FAILURE | |
| PSA_ERROR_CORRUPTION_DETECTED | |
| PSA_ERROR_BAD_STATE | The operation state is not valid (it must be active), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_hash_finish | ( | psa_hash_operation_t * | operation, |
| uint8_t * | hash, | ||
| size_t | hash_size, | ||
| size_t * | hash_length | ||
| ) |
Finish the calculation of the hash of a message.
The application must call psa_hash_setup() before calling this function. This function calculates the hash of the message formed by concatenating the inputs passed to preceding calls to psa_hash_update().
When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling psa_hash_abort().
memcmp is risky because the time taken by the comparison may leak information about the hashed data which could allow an attacker to guess a valid hash and thereby bypass security controls.| [in,out] | operation | Active hash operation. |
| [out] | hash | Buffer where the hash is to be written. |
| hash_size | Size of the hash buffer in bytes. | |
| [out] | hash_length | On success, the number of bytes that make up the hash value. This is always PSA_HASH_LENGTH(alg) where alg is the hash algorithm that is calculated. |
| PSA_SUCCESS | Success. |
| PSA_ERROR_BUFFER_TOO_SMALL | The size of the hash buffer is too small. You can determine a sufficient buffer size by calling PSA_HASH_LENGTH(alg) where alg is the hash algorithm that is calculated. |
| PSA_ERROR_INSUFFICIENT_MEMORY | |
| PSA_ERROR_COMMUNICATION_FAILURE | |
| PSA_ERROR_HARDWARE_FAILURE | |
| PSA_ERROR_CORRUPTION_DETECTED | |
| PSA_ERROR_BAD_STATE | The operation state is not valid (it must be active), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_hash_verify | ( | psa_hash_operation_t * | operation, |
| const uint8_t * | hash, | ||
| size_t | hash_length | ||
| ) |
Finish the calculation of the hash of a message and compare it with an expected value.
The application must call psa_hash_setup() before calling this function. This function calculates the hash of the message formed by concatenating the inputs passed to preceding calls to psa_hash_update(). It then compares the calculated hash with the expected hash passed as a parameter to this function.
When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling psa_hash_abort().
| [in,out] | operation | Active hash operation. |
| [in] | hash | Buffer containing the expected hash value. |
| hash_length | Size of the hash buffer in bytes. |
| PSA_SUCCESS | The expected hash is identical to the actual hash of the message. |
| PSA_ERROR_INVALID_SIGNATURE | The hash of the message was calculated successfully, but it differs from the expected hash. |
| PSA_ERROR_INSUFFICIENT_MEMORY | |
| PSA_ERROR_COMMUNICATION_FAILURE | |
| PSA_ERROR_HARDWARE_FAILURE | |
| PSA_ERROR_CORRUPTION_DETECTED | |
| PSA_ERROR_BAD_STATE | The operation state is not valid (it must be active), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_hash_abort | ( | psa_hash_operation_t * | operation | ) |
Abort a hash operation.
Aborting an operation frees all associated resources except for the operation structure itself. Once aborted, the operation object can be reused for another operation by calling psa_hash_setup() again.
You may call this function any time after the operation object has been initialized by one of the methods described in psa_hash_operation_t.
In particular, calling psa_hash_abort() after the operation has been terminated by a call to psa_hash_abort(), psa_hash_finish() or psa_hash_verify() is safe and has no effect.
| [in,out] | operation | Initialized hash operation. |
| PSA_SUCCESS | |
| PSA_ERROR_COMMUNICATION_FAILURE | |
| PSA_ERROR_HARDWARE_FAILURE | |
| PSA_ERROR_CORRUPTION_DETECTED | |
| PSA_ERROR_BAD_STATE | The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |
| psa_status_t psa_hash_clone | ( | const psa_hash_operation_t * | source_operation, |
| psa_hash_operation_t * | target_operation | ||
| ) |
Clone a hash operation.
This function copies the state of an ongoing hash operation to a new operation object. In other words, this function is equivalent to calling psa_hash_setup() on target_operation with the same algorithm that source_operation was set up for, then psa_hash_update() on target_operation with the same input that that was passed to source_operation. After this function returns, the two objects are independent, i.e. subsequent calls involving one of the objects do not affect the other object.
| [in] | source_operation | The active hash operation to clone. |
| [in,out] | target_operation | The operation object to set up. It must be initialized but not active. |
| PSA_SUCCESS | |
| PSA_ERROR_COMMUNICATION_FAILURE | |
| PSA_ERROR_HARDWARE_FAILURE | |
| PSA_ERROR_CORRUPTION_DETECTED | |
| PSA_ERROR_INSUFFICIENT_MEMORY | |
| PSA_ERROR_BAD_STATE | The source_operation state is not valid (it must be active), or the target_operation state is not valid (it must be inactive), or the library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code. |