![]() |
![]() |
Macros | |
| #define | PSA_KEY_DERIVATION_INPUT_SECRET ((psa_key_derivation_step_t) 0x0101) |
| #define | PSA_KEY_DERIVATION_INPUT_PASSWORD ((psa_key_derivation_step_t) 0x0102) |
| #define | PSA_KEY_DERIVATION_INPUT_OTHER_SECRET ((psa_key_derivation_step_t) 0x0103) |
| #define | PSA_KEY_DERIVATION_INPUT_LABEL ((psa_key_derivation_step_t) 0x0201) |
| #define | PSA_KEY_DERIVATION_INPUT_SALT ((psa_key_derivation_step_t) 0x0202) |
| #define | PSA_KEY_DERIVATION_INPUT_INFO ((psa_key_derivation_step_t) 0x0203) |
| #define | PSA_KEY_DERIVATION_INPUT_SEED ((psa_key_derivation_step_t) 0x0204) |
| #define | PSA_KEY_DERIVATION_INPUT_COST ((psa_key_derivation_step_t) 0x0205) |
| #define | PSA_KEY_DERIVATION_INPUT_CONTEXT ((psa_key_derivation_step_t)0x0206U) |
Typedefs | |
| typedef uint16_t | psa_key_derivation_step_t |
| Encoding of the step of a key derivation. More... | |
| #define PSA_KEY_DERIVATION_INPUT_SECRET ((psa_key_derivation_step_t) 0x0101) |
A secret input for key derivation.
This should be a key of type PSA_KEY_TYPE_DERIVE (passed to psa_key_derivation_input_key()) or the shared secret resulting from a key agreement (obtained via psa_key_derivation_key_agreement()).
The secret can also be a direct input (passed to key_derivation_input_bytes()). In this case, the derivation operation may not be used to derive keys: the operation will only allow psa_key_derivation_output_bytes(), psa_key_derivation_verify_bytes(), or psa_key_derivation_verify_key(), but not psa_key_derivation_output_key().
| #define PSA_KEY_DERIVATION_INPUT_PASSWORD ((psa_key_derivation_step_t) 0x0102) |
A low-entropy secret input for password hashing / key stretching.
This is usually a key of type PSA_KEY_TYPE_PASSWORD (passed to psa_key_derivation_input_key()) or a direct input (passed to psa_key_derivation_input_bytes()) that is a password or passphrase. It can also be high-entropy secret such as a key of type PSA_KEY_TYPE_DERIVE or the shared secret resulting from a key agreement.
The secret can also be a direct input (passed to key_derivation_input_bytes()). In this case, the derivation operation may not be used to derive keys: the operation will only allow psa_key_derivation_output_bytes(), psa_key_derivation_verify_bytes(), or psa_key_derivation_verify_key(), but not psa_key_derivation_output_key().
| #define PSA_KEY_DERIVATION_INPUT_OTHER_SECRET ((psa_key_derivation_step_t) 0x0103) |
A high-entropy additional secret input for key derivation.
This is typically the shared secret resulting from a key agreement obtained via psa_key_derivation_key_agreement(). It may alternatively be a key of type PSA_KEY_TYPE_DERIVE passed to psa_key_derivation_input_key(), or a direct input passed to psa_key_derivation_input_bytes().
| #define PSA_KEY_DERIVATION_INPUT_LABEL ((psa_key_derivation_step_t) 0x0201) |
A label for key derivation.
This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.
| #define PSA_KEY_DERIVATION_INPUT_SALT ((psa_key_derivation_step_t) 0x0202) |
A salt for key derivation.
This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA or PSA_KEY_TYPE_PEPPER.
| #define PSA_KEY_DERIVATION_INPUT_INFO ((psa_key_derivation_step_t) 0x0203) |
An information string for key derivation.
This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.
| #define PSA_KEY_DERIVATION_INPUT_SEED ((psa_key_derivation_step_t) 0x0204) |
A seed for key derivation.
This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.
| #define PSA_KEY_DERIVATION_INPUT_COST ((psa_key_derivation_step_t) 0x0205) |
A cost parameter for password hashing / key stretching.
This must be a direct input, passed to psa_key_derivation_input_integer().
| #define PSA_KEY_DERIVATION_INPUT_CONTEXT ((psa_key_derivation_step_t)0x0206U) |
A context for key derivation.
This is typically a direct input. It is currently unsupported to use it as a key of type PSA_KEY_TYPE_RAW_DATA.
| typedef uint16_t psa_key_derivation_step_t |
Encoding of the step of a key derivation.
Values of this type are generally constructed by macros called PSA_KEY_DERIVATION_INPUT_xxx.