![]() |
![]() |
Typedefs | |
| typedef uint16_t | psa_key_type_t |
| Encoding of a key type. More... | |
| typedef uint8_t | psa_ecc_family_t |
| typedef uint8_t | psa_dh_family_t |
| typedef uint32_t | psa_algorithm_t |
| Encoding of a cryptographic algorithm. More... | |
| #define PSA_KEY_TYPE_NONE ((psa_key_type_t) 0x0000) |
An invalid key type value.
Zero is not the encoding of any key type.
| #define PSA_KEY_TYPE_VENDOR_FLAG ((psa_key_type_t) 0x8000) |
Vendor-defined key type flag.
Key types defined by this standard will never have the PSA_KEY_TYPE_VENDOR_FLAG bit set. Vendors who define additional key types must use an encoding with the PSA_KEY_TYPE_VENDOR_FLAG bit set and should respect the bitwise structure used by standard encodings whenever practical.
| #define PSA_KEY_TYPE_CATEGORY_MASK ((psa_key_type_t) 0x7000) |
| #define PSA_KEY_TYPE_CATEGORY_RAW ((psa_key_type_t) 0x1000) |
| #define PSA_KEY_TYPE_CATEGORY_SYMMETRIC ((psa_key_type_t) 0x2000) |
| #define PSA_KEY_TYPE_CATEGORY_PUBLIC_KEY ((psa_key_type_t) 0x4000) |
| #define PSA_KEY_TYPE_CATEGORY_KEY_PAIR ((psa_key_type_t) 0x7000) |
| #define PSA_KEY_TYPE_CATEGORY_FLAG_PAIR ((psa_key_type_t) 0x3000) |
| #define PSA_KEY_TYPE_IS_VENDOR_DEFINED | ( | type | ) | (((type) & PSA_KEY_TYPE_VENDOR_FLAG) != 0) |
Whether a key type is vendor-defined.
See also PSA_KEY_TYPE_VENDOR_FLAG.
| #define PSA_KEY_TYPE_IS_UNSTRUCTURED | ( | type | ) |
Whether a key type is an unstructured array of bytes.
This encompasses both symmetric keys and non-key data.
| #define PSA_KEY_TYPE_IS_ASYMMETRIC | ( | type | ) |
Whether a key type is asymmetric: either a key pair or a public key.
| #define PSA_KEY_TYPE_IS_PUBLIC_KEY | ( | type | ) | (((type) & PSA_KEY_TYPE_CATEGORY_MASK) == PSA_KEY_TYPE_CATEGORY_PUBLIC_KEY) |
Whether a key type is the public part of a key pair.
| #define PSA_KEY_TYPE_IS_KEY_PAIR | ( | type | ) | (((type) & PSA_KEY_TYPE_CATEGORY_MASK) == PSA_KEY_TYPE_CATEGORY_KEY_PAIR) |
Whether a key type is a key pair containing a private part and a public part.
| #define PSA_KEY_TYPE_KEY_PAIR_OF_PUBLIC_KEY | ( | type | ) | ((type) | PSA_KEY_TYPE_CATEGORY_FLAG_PAIR) |
The key pair type corresponding to a public key type.
You may also pass a key pair type as type, it will be left unchanged.
| type | A public key type or key pair type. |
type is not a public key or a key pair, the return value is undefined. | #define PSA_KEY_TYPE_PUBLIC_KEY_OF_KEY_PAIR | ( | type | ) | ((type) & ~PSA_KEY_TYPE_CATEGORY_FLAG_PAIR) |
The public key type corresponding to a key pair type.
You may also pass a key pair type as type, it will be left unchanged.
| type | A public key type or key pair type. |
type is not a public key or a key pair, the return value is undefined. | #define PSA_KEY_TYPE_RAW_DATA ((psa_key_type_t) 0x1001) |
Raw data.
A "key" of this type cannot be used for any cryptographic operation. Applications may use this type to store arbitrary data in the keystore.
| #define PSA_KEY_TYPE_HMAC ((psa_key_type_t) 0x1100) |
HMAC key.
The key policy determines which underlying hash algorithm the key can be used for.
HMAC keys should generally have the same size as the underlying hash. This size can be calculated with PSA_HASH_LENGTH(alg) where alg is the HMAC algorithm or the underlying hash algorithm.
| #define PSA_KEY_TYPE_DERIVE ((psa_key_type_t) 0x1200) |
A secret for key derivation.
This key type is for high-entropy secrets only. For low-entropy secrets, PSA_KEY_TYPE_PASSWORD should be used instead.
These keys can be used as the PSA_KEY_DERIVATION_INPUT_SECRET or PSA_KEY_DERIVATION_INPUT_PASSWORD input of key derivation algorithms.
The key policy determines which key derivation algorithm the key can be used for.
| #define PSA_KEY_TYPE_PASSWORD ((psa_key_type_t) 0x1203) |
A low-entropy secret for password hashing or key derivation.
This key type is suitable for passwords and passphrases which are typically intended to be memorizable by humans, and have a low entropy relative to their size. It can be used for randomly generated or derived keys with maximum or near-maximum entropy, but PSA_KEY_TYPE_DERIVE is more suitable for such keys. It is not suitable for passwords with extremely low entropy, such as numerical PINs.
These keys can be used as the PSA_KEY_DERIVATION_INPUT_PASSWORD input of key derivation algorithms. Algorithms that accept such an input were designed to accept low-entropy secret and are known as password hashing or key stretching algorithms.
These keys cannot be used as the PSA_KEY_DERIVATION_INPUT_SECRET input of key derivation algorithms, as the algorithms that take such an input expect it to be high-entropy.
The key policy determines which key derivation algorithm the key can be used for, among the permissible subset defined above.
| #define PSA_KEY_TYPE_PASSWORD_HASH ((psa_key_type_t) 0x1205) |
A secret value that can be used to verify a password hash.
The key policy determines which key derivation algorithm the key can be used for, among the same permissible subset as for PSA_KEY_TYPE_PASSWORD.
| #define PSA_KEY_TYPE_PEPPER ((psa_key_type_t) 0x1206) |
A secret value that can be used in when computing a password hash.
The key policy determines which key derivation algorithm the key can be used for, among the subset of algorithms that can use pepper.
| #define PSA_KEY_TYPE_AES ((psa_key_type_t) 0x2400) |
Key for a cipher, AEAD or MAC algorithm based on the AES block cipher.
The size of the key can be 16 bytes (AES-128), 24 bytes (AES-192) or 32 bytes (AES-256).
| #define PSA_KEY_TYPE_ARIA ((psa_key_type_t) 0x2406) |
Key for a cipher, AEAD or MAC algorithm based on the ARIA block cipher.
| #define PSA_KEY_TYPE_DES ((psa_key_type_t) 0x2301) |
Key for a cipher or MAC algorithm based on DES or 3DES (Triple-DES).
The size of the key can be 64 bits (single DES), 128 bits (2-key 3DES) or 192 bits (3-key 3DES).
Note that single DES and 2-key 3DES are weak and strongly deprecated and should only be used to decrypt legacy data. 3-key 3DES is weak and deprecated and should only be used in legacy protocols.
| #define PSA_KEY_TYPE_CAMELLIA ((psa_key_type_t) 0x2403) |
Key for a cipher, AEAD or MAC algorithm based on the Camellia block cipher.
| #define PSA_KEY_TYPE_CHACHA20 ((psa_key_type_t) 0x2004) |
Key for the ChaCha20 stream cipher or the Chacha20-Poly1305 AEAD algorithm.
ChaCha20 and the ChaCha20_Poly1305 construction are defined in RFC 7539.
| #define PSA_KEY_TYPE_RSA_PUBLIC_KEY ((psa_key_type_t) 0x4001) |
RSA public key.
The size of an RSA key is the bit size of the modulus.
| #define PSA_KEY_TYPE_RSA_KEY_PAIR ((psa_key_type_t) 0x7001) |
RSA key pair (private and public key).
The size of an RSA key is the bit size of the modulus.
| #define PSA_KEY_TYPE_IS_RSA | ( | type | ) | (PSA_KEY_TYPE_PUBLIC_KEY_OF_KEY_PAIR(type) == PSA_KEY_TYPE_RSA_PUBLIC_KEY) |
Whether a key type is an RSA key (pair or public-only).
| #define PSA_KEY_TYPE_ECC_PUBLIC_KEY_BASE ((psa_key_type_t) 0x4100) |
| #define PSA_KEY_TYPE_ECC_KEY_PAIR_BASE ((psa_key_type_t) 0x7100) |
| #define PSA_KEY_TYPE_ECC_CURVE_MASK ((psa_key_type_t) 0x00ff) |
| #define PSA_KEY_TYPE_ECC_KEY_PAIR | ( | curve | ) | (PSA_KEY_TYPE_ECC_KEY_PAIR_BASE | (curve)) |
Elliptic curve key pair.
The size of an elliptic curve key is the bit size associated with the curve, i.e. the bit size of q for a curve over a field Fq. See the documentation of PSA_ECC_FAMILY_xxx curve families for details.
| curve | A value of type psa_ecc_family_t that identifies the ECC curve to be used. |
| #define PSA_KEY_TYPE_ECC_PUBLIC_KEY | ( | curve | ) | (PSA_KEY_TYPE_ECC_PUBLIC_KEY_BASE | (curve)) |
Elliptic curve public key.
The size of an elliptic curve public key is the same as the corresponding private key (see PSA_KEY_TYPE_ECC_KEY_PAIR and the documentation of PSA_ECC_FAMILY_xxx curve families).
| curve | A value of type psa_ecc_family_t that identifies the ECC curve to be used. |
| #define PSA_KEY_TYPE_IS_ECC | ( | type | ) |
Whether a key type is an elliptic curve key (pair or public-only).
| #define PSA_KEY_TYPE_IS_ECC_KEY_PAIR | ( | type | ) |
Whether a key type is an elliptic curve key pair.
| #define PSA_KEY_TYPE_IS_ECC_PUBLIC_KEY | ( | type | ) |
Whether a key type is an elliptic curve public key.
| #define PSA_KEY_TYPE_ECC_GET_FAMILY | ( | type | ) |
Extract the curve from an elliptic curve key type.
| #define PSA_ECC_FAMILY_IS_WEIERSTRASS | ( | family | ) | ((family & 0xc0) == 0) |
Check if the curve of given family is Weierstrass elliptic curve.
| #define PSA_ECC_FAMILY_SECP_K1 ((psa_ecc_family_t) 0x17) |
SEC Koblitz curves over prime fields.
This family comprises the following curves: secp192k1, secp224k1, secp256k1. They are defined in Standards for Efficient Cryptography, SEC 2: Recommended Elliptic Curve Domain Parameters. https://www.secg.org/sec2-v2.pdf
| #define PSA_ECC_FAMILY_SECP_R1 ((psa_ecc_family_t) 0x12) |
SEC random curves over prime fields.
This family comprises the following curves: secp192k1, secp224r1, secp256r1, secp384r1, secp521r1. They are defined in Standards for Efficient Cryptography, SEC 2: Recommended Elliptic Curve Domain Parameters. https://www.secg.org/sec2-v2.pdf
| #define PSA_ECC_FAMILY_SECP_R2 ((psa_ecc_family_t) 0x1b) |
| #define PSA_ECC_FAMILY_SECT_K1 ((psa_ecc_family_t) 0x27) |
SEC Koblitz curves over binary fields.
This family comprises the following curves: sect163k1, sect233k1, sect239k1, sect283k1, sect409k1, sect571k1. They are defined in Standards for Efficient Cryptography, SEC 2: Recommended Elliptic Curve Domain Parameters. https://www.secg.org/sec2-v2.pdf
| #define PSA_ECC_FAMILY_SECT_R1 ((psa_ecc_family_t) 0x22) |
SEC random curves over binary fields.
This family comprises the following curves: sect163r1, sect233r1, sect283r1, sect409r1, sect571r1. They are defined in Standards for Efficient Cryptography, SEC 2: Recommended Elliptic Curve Domain Parameters. https://www.secg.org/sec2-v2.pdf
| #define PSA_ECC_FAMILY_SECT_R2 ((psa_ecc_family_t) 0x2b) |
SEC additional random curves over binary fields.
This family comprises the following curve: sect163r2. It is defined in Standards for Efficient Cryptography, SEC 2: Recommended Elliptic Curve Domain Parameters. https://www.secg.org/sec2-v2.pdf
| #define PSA_ECC_FAMILY_BRAINPOOL_P_R1 ((psa_ecc_family_t) 0x30) |
Brainpool P random curves.
This family comprises the following curves: brainpoolP160r1, brainpoolP192r1, brainpoolP224r1, brainpoolP256r1, brainpoolP320r1, brainpoolP384r1, brainpoolP512r1. It is defined in RFC 5639.
| #define PSA_ECC_FAMILY_MONTGOMERY ((psa_ecc_family_t) 0x41) |
Curve25519 and Curve448.
This family comprises the following Montgomery curves:
| #define PSA_ECC_FAMILY_TWISTED_EDWARDS ((psa_ecc_family_t) 0x42) |
The twisted Edwards curves Ed25519 and Ed448.
These curves are suitable for EdDSA (PSA_ALG_PURE_EDDSA for both curves, PSA_ALG_ED25519PH for the 255-bit curve, PSA_ALG_ED448PH for the 448-bit curve).
This family comprises the following twisted Edwards curves:
| #define PSA_KEY_TYPE_DH_PUBLIC_KEY_BASE ((psa_key_type_t) 0x4200) |
| #define PSA_KEY_TYPE_DH_KEY_PAIR_BASE ((psa_key_type_t) 0x7200) |
| #define PSA_KEY_TYPE_DH_GROUP_MASK ((psa_key_type_t) 0x00ff) |
| #define PSA_KEY_TYPE_DH_KEY_PAIR | ( | group | ) | (PSA_KEY_TYPE_DH_KEY_PAIR_BASE | (group)) |
Diffie-Hellman key pair.
| group | A value of type psa_dh_family_t that identifies the Diffie-Hellman group to be used. |
| #define PSA_KEY_TYPE_DH_PUBLIC_KEY | ( | group | ) | (PSA_KEY_TYPE_DH_PUBLIC_KEY_BASE | (group)) |
Diffie-Hellman public key.
| group | A value of type psa_dh_family_t that identifies the Diffie-Hellman group to be used. |
| #define PSA_KEY_TYPE_IS_DH | ( | type | ) |
Whether a key type is a Diffie-Hellman key (pair or public-only).
| #define PSA_KEY_TYPE_IS_DH_KEY_PAIR | ( | type | ) |
Whether a key type is a Diffie-Hellman key pair.
| #define PSA_KEY_TYPE_IS_DH_PUBLIC_KEY | ( | type | ) |
Whether a key type is a Diffie-Hellman public key.
| #define PSA_KEY_TYPE_DH_GET_FAMILY | ( | type | ) |
Extract the group from a Diffie-Hellman key type.
| #define PSA_DH_FAMILY_RFC7919 ((psa_dh_family_t) 0x03) |
Diffie-Hellman groups defined in RFC 7919 Appendix A.
This family includes groups with the following key sizes (in bits): 2048, 3072, 4096, 6144, 8192. A given implementation may support all of these sizes or only a subset.
| #define PSA_GET_KEY_TYPE_BLOCK_SIZE_EXPONENT | ( | type | ) | (((type) >> 8) & 7) |
| #define PSA_BLOCK_CIPHER_BLOCK_LENGTH | ( | type | ) |
The block size of a block cipher.
| type | A cipher key type (value of type psa_key_type_t). |
type is not a supported cipher key type.| #define PSA_ALG_VENDOR_FLAG ((psa_algorithm_t) 0x80000000) |
Vendor-defined algorithm flag.
Algorithms defined by this standard will never have the PSA_ALG_VENDOR_FLAG bit set. Vendors who define additional algorithms must use an encoding with the PSA_ALG_VENDOR_FLAG bit set and should respect the bitwise structure used by standard encodings whenever practical.
| #define PSA_ALG_CATEGORY_MASK ((psa_algorithm_t) 0x7f000000) |
| #define PSA_ALG_CATEGORY_HASH ((psa_algorithm_t) 0x02000000) |
| #define PSA_ALG_CATEGORY_MAC ((psa_algorithm_t) 0x03000000) |
| #define PSA_ALG_CATEGORY_CIPHER ((psa_algorithm_t) 0x04000000) |
| #define PSA_ALG_CATEGORY_AEAD ((psa_algorithm_t) 0x05000000) |
| #define PSA_ALG_CATEGORY_SIGN ((psa_algorithm_t) 0x06000000) |
| #define PSA_ALG_CATEGORY_ASYMMETRIC_ENCRYPTION ((psa_algorithm_t) 0x07000000) |
| #define PSA_ALG_CATEGORY_KEY_DERIVATION ((psa_algorithm_t) 0x08000000) |
| #define PSA_ALG_CATEGORY_KEY_AGREEMENT ((psa_algorithm_t) 0x09000000) |
| #define PSA_ALG_IS_VENDOR_DEFINED | ( | alg | ) | (((alg) & PSA_ALG_VENDOR_FLAG) != 0) |
Whether an algorithm is vendor-defined.
See also PSA_ALG_VENDOR_FLAG.
| #define PSA_ALG_IS_HASH | ( | alg | ) | (((alg) & PSA_ALG_CATEGORY_MASK) == PSA_ALG_CATEGORY_HASH) |
Whether the specified algorithm is a hash algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a hash algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_MAC | ( | alg | ) | (((alg) & PSA_ALG_CATEGORY_MASK) == PSA_ALG_CATEGORY_MAC) |
Whether the specified algorithm is a MAC algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a MAC algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_CIPHER | ( | alg | ) | (((alg) & PSA_ALG_CATEGORY_MASK) == PSA_ALG_CATEGORY_CIPHER) |
Whether the specified algorithm is a symmetric cipher algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a symmetric cipher algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_AEAD | ( | alg | ) | (((alg) & PSA_ALG_CATEGORY_MASK) == PSA_ALG_CATEGORY_AEAD) |
Whether the specified algorithm is an authenticated encryption with associated data (AEAD) algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an AEAD algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_SIGN | ( | alg | ) | (((alg) & PSA_ALG_CATEGORY_MASK) == PSA_ALG_CATEGORY_SIGN) |
Whether the specified algorithm is an asymmetric signature algorithm, also known as public-key signature algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an asymmetric signature algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_ASYMMETRIC_ENCRYPTION | ( | alg | ) | (((alg) & PSA_ALG_CATEGORY_MASK) == PSA_ALG_CATEGORY_ASYMMETRIC_ENCRYPTION) |
Whether the specified algorithm is an asymmetric encryption algorithm, also known as public-key encryption algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an asymmetric encryption algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_KEY_AGREEMENT | ( | alg | ) | (((alg) & PSA_ALG_CATEGORY_MASK) == PSA_ALG_CATEGORY_KEY_AGREEMENT) |
Whether the specified algorithm is a key agreement algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a key agreement algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_KEY_DERIVATION | ( | alg | ) | (((alg) & PSA_ALG_CATEGORY_MASK) == PSA_ALG_CATEGORY_KEY_DERIVATION) |
Whether the specified algorithm is a key derivation algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a key derivation algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_KEY_DERIVATION_STRETCHING | ( | alg | ) |
Whether the specified algorithm is a key stretching / password hashing algorithm.
A key stretching / password hashing algorithm is a key derivation algorithm that is suitable for use with a low-entropy secret such as a password. Equivalently, it's a key derivation algorithm that uses a PSA_KEY_DERIVATION_INPUT_PASSWORD input step.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a key stretching / password hashing algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_NONE ((psa_algorithm_t)0) |
An invalid algorithm identifier value.
| #define PSA_ALG_HASH_MASK ((psa_algorithm_t) 0x000000ff) |
| #define PSA_ALG_MD5 ((psa_algorithm_t) 0x02000003) |
MD5
| #define PSA_ALG_RIPEMD160 ((psa_algorithm_t) 0x02000004) |
PSA_ALG_RIPEMD160
| #define PSA_ALG_SHA_1 ((psa_algorithm_t) 0x02000005) |
SHA1
| #define PSA_ALG_SHA_224 ((psa_algorithm_t) 0x02000008) |
SHA2-224
| #define PSA_ALG_SHA_256 ((psa_algorithm_t) 0x02000009) |
SHA2-256
| #define PSA_ALG_SHA_384 ((psa_algorithm_t) 0x0200000a) |
SHA2-384
| #define PSA_ALG_SHA_512 ((psa_algorithm_t) 0x0200000b) |
SHA2-512
| #define PSA_ALG_SHA_512_224 ((psa_algorithm_t) 0x0200000c) |
SHA2-512/224
| #define PSA_ALG_SHA_512_256 ((psa_algorithm_t) 0x0200000d) |
SHA2-512/256
| #define PSA_ALG_SHA3_224 ((psa_algorithm_t) 0x02000010) |
SHA3-224
| #define PSA_ALG_SHA3_256 ((psa_algorithm_t) 0x02000011) |
SHA3-256
| #define PSA_ALG_SHA3_384 ((psa_algorithm_t) 0x02000012) |
SHA3-384
| #define PSA_ALG_SHA3_512 ((psa_algorithm_t) 0x02000013) |
SHA3-512
| #define PSA_ALG_SHAKE256_512 ((psa_algorithm_t) 0x02000015) |
The first 512 bits (64 bytes) of the SHAKE256 output.
This is the prehashing for Ed448ph (see PSA_ALG_ED448PH). For other scenarios where a hash function based on SHA3/SHAKE is desired, SHA3-512 has the same output size and a (theoretically) higher security strength.
| #define PSA_ALG_ANY_HASH ((psa_algorithm_t) 0x020000ff) |
In a hash-and-sign algorithm policy, allow any hash algorithm.
This value may be used to form the algorithm usage field of a policy for a signature algorithm that is parametrized by a hash. The key may then be used to perform operations using the same signature algorithm parametrized with any supported hash.
That is, suppose that PSA_xxx_SIGNATURE is one of the following macros:
PSA_xxx_SIGNATURE and a specific hash. Each call to sign or verify a message may use a different hash. This value may not be used to build other algorithms that are parametrized over a hash. For any valid use of this macro to build an algorithm alg, PSA_ALG_IS_HASH_AND_SIGN(alg) is true.
This value may not be used to build an algorithm specification to perform an operation. It is only valid to build policies.
| #define PSA_ALG_MAC_SUBCATEGORY_MASK ((psa_algorithm_t) 0x00c00000) |
| #define PSA_ALG_HMAC_BASE ((psa_algorithm_t) 0x03800000) |
| #define PSA_ALG_HMAC | ( | hash_alg | ) | (PSA_ALG_HMAC_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Macro to build an HMAC algorithm.
For example, PSA_ALG_HMAC(PSA_ALG_SHA_256) is HMAC-SHA-256.
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_HMAC_GET_HASH | ( | hmac_alg | ) | (PSA_ALG_CATEGORY_HASH | ((hmac_alg) & PSA_ALG_HASH_MASK)) |
| #define PSA_ALG_IS_HMAC | ( | alg | ) |
Whether the specified algorithm is an HMAC algorithm.
HMAC is a family of MAC algorithms that are based on a hash function.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an HMAC algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_MAC_TRUNCATION_MASK ((psa_algorithm_t) 0x003f0000) |
| #define PSA_MAC_TRUNCATION_OFFSET 16 |
| #define PSA_ALG_MAC_AT_LEAST_THIS_LENGTH_FLAG ((psa_algorithm_t) 0x00008000) |
| #define PSA_ALG_TRUNCATED_MAC | ( | mac_alg, | |
| mac_length | |||
| ) |
Macro to build a truncated MAC algorithm.
A truncated MAC algorithm is identical to the corresponding MAC algorithm except that the MAC value for the truncated algorithm consists of only the first mac_length bytes of the MAC value for the untruncated algorithm.
| mac_alg | A MAC algorithm identifier (value of type psa_algorithm_t such that PSA_ALG_IS_MAC(mac_alg) is true). This may be a truncated or untruncated MAC algorithm. |
| mac_length | Desired length of the truncated MAC in bytes. This must be at most the full length of the MAC and must be at least an implementation-specified minimum. The implementation-specified minimum shall not be zero. |
mac_alg is not a supported MAC algorithm or if mac_length is too small or too large for the specified MAC algorithm. | #define PSA_ALG_FULL_LENGTH_MAC | ( | mac_alg | ) |
Macro to build the base MAC algorithm corresponding to a truncated MAC algorithm.
| mac_alg | A MAC algorithm identifier (value of type psa_algorithm_t such that PSA_ALG_IS_MAC(mac_alg) is true). This may be a truncated or untruncated MAC algorithm. |
mac_alg is not a supported MAC algorithm. | #define PSA_MAC_TRUNCATED_LENGTH | ( | mac_alg | ) | (((mac_alg) & PSA_ALG_MAC_TRUNCATION_MASK) >> PSA_MAC_TRUNCATION_OFFSET) |
Length to which a MAC algorithm is truncated.
| mac_alg | A MAC algorithm identifier (value of type psa_algorithm_t such that PSA_ALG_IS_MAC(mac_alg) is true). |
mac_alg is a non-truncated MAC algorithm. mac_alg is not a supported MAC algorithm. | #define PSA_ALG_AT_LEAST_THIS_LENGTH_MAC | ( | mac_alg, | |
| min_mac_length | |||
| ) |
Macro to build a MAC minimum-MAC-length wildcard algorithm.
A minimum-MAC-length MAC wildcard algorithm permits all MAC algorithms sharing the same base algorithm, and where the (potentially truncated) MAC length of the specific algorithm is equal to or larger then the wildcard algorithm's minimum MAC length.
| mac_alg | A MAC algorithm identifier (value of type psa_algorithm_t such that PSA_ALG_IS_MAC(mac_alg) is true). |
| min_mac_length | Desired minimum length of the message authentication code in bytes. This must be at most the untruncated length of the MAC and must be at least 1. |
mac_alg is not a supported MAC algorithm or if min_mac_length is less than 1 or too large for the specified MAC algorithm. | #define PSA_ALG_CIPHER_MAC_BASE ((psa_algorithm_t) 0x03c00000) |
| #define PSA_ALG_CBC_MAC ((psa_algorithm_t) 0x03c00100) |
The CBC-MAC construction over a block cipher
| #define PSA_ALG_CMAC ((psa_algorithm_t) 0x03c00200) |
The CMAC construction over a block cipher
| #define PSA_ALG_IS_BLOCK_CIPHER_MAC | ( | alg | ) |
Whether the specified algorithm is a MAC algorithm based on a block cipher.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a MAC algorithm based on a block cipher, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_CIPHER_STREAM_FLAG ((psa_algorithm_t) 0x00800000) |
| #define PSA_ALG_CIPHER_FROM_BLOCK_FLAG ((psa_algorithm_t) 0x00400000) |
| #define PSA_ALG_IS_STREAM_CIPHER | ( | alg | ) |
Whether the specified algorithm is a stream cipher.
A stream cipher is a symmetric cipher that encrypts or decrypts messages by applying a bitwise-xor with a stream of bytes that is generated from a key.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a stream cipher algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier or if it is not a symmetric cipher algorithm. | #define PSA_ALG_STREAM_CIPHER ((psa_algorithm_t) 0x04800100) |
The stream cipher mode of a stream cipher algorithm.
The underlying stream cipher is determined by the key type.
| #define PSA_ALG_CTR ((psa_algorithm_t) 0x04c01000) |
The CTR stream cipher mode.
CTR is a stream cipher which is built from a block cipher. The underlying block cipher is determined by the key type. For example, to use AES-128-CTR, use this algorithm with a key of type PSA_KEY_TYPE_AES and a length of 128 bits (16 bytes).
| #define PSA_ALG_CFB ((psa_algorithm_t) 0x04c01100) |
The CFB stream cipher mode.
The underlying block cipher is determined by the key type.
| #define PSA_ALG_OFB ((psa_algorithm_t) 0x04c01200) |
The OFB stream cipher mode.
The underlying block cipher is determined by the key type.
| #define PSA_ALG_XTS ((psa_algorithm_t) 0x0440ff00) |
The XTS cipher mode.
XTS is a cipher mode which is built from a block cipher. It requires at least one full block of input, but beyond this minimum the input does not need to be a whole number of blocks.
| #define PSA_ALG_ECB_NO_PADDING ((psa_algorithm_t) 0x04404400) |
The Electronic Code Book (ECB) mode of a block cipher, with no padding.
The underlying block cipher is determined by the key type.
This symmetric cipher mode can only be used with messages whose lengths are a multiple of the block size of the chosen block cipher.
ECB mode does not accept an initialization vector (IV). When using a multi-part cipher operation with this algorithm, psa_cipher_generate_iv() and psa_cipher_set_iv() must not be called.
| #define PSA_ALG_CBC_NO_PADDING ((psa_algorithm_t) 0x04404000) |
The CBC block cipher chaining mode, with no padding.
The underlying block cipher is determined by the key type.
This symmetric cipher mode can only be used with messages whose lengths are whole number of blocks for the chosen block cipher.
| #define PSA_ALG_CBC_PKCS7 ((psa_algorithm_t) 0x04404100) |
The CBC block cipher chaining mode with PKCS#7 padding.
The underlying block cipher is determined by the key type.
This is the padding method defined by PKCS#7 (RFC 2315) §10.3.
| #define PSA_ALG_AEAD_FROM_BLOCK_FLAG ((psa_algorithm_t) 0x00400000) |
| #define PSA_ALG_IS_AEAD_ON_BLOCK_CIPHER | ( | alg | ) |
Whether the specified algorithm is an AEAD mode on a block cipher.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an AEAD algorithm which is an AEAD mode based on a block cipher, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_CCM ((psa_algorithm_t) 0x05500100) |
The CCM authenticated encryption algorithm.
The underlying block cipher is determined by the key type.
| #define PSA_ALG_CCM_STAR_NO_TAG ((psa_algorithm_t) 0x04c01300) |
The CCM* cipher mode without authentication.
This is CCM* as specified in IEEE 802.15.4 s7, with a tag length of 0. For CCM* with a nonzero tag length, use the AEAD algorithm PSA_ALG_CCM.
The underlying block cipher is determined by the key type.
Currently only 13-byte long IV's are supported.
| #define PSA_ALG_GCM ((psa_algorithm_t) 0x05500200) |
The GCM authenticated encryption algorithm.
The underlying block cipher is determined by the key type.
| #define PSA_ALG_CHACHA20_POLY1305 ((psa_algorithm_t) 0x05100500) |
The Chacha20-Poly1305 AEAD algorithm.
The ChaCha20_Poly1305 construction is defined in RFC 7539.
Implementations must support 12-byte nonces, may support 8-byte nonces, and should reject other sizes.
Implementations must support 16-byte tags and should reject other sizes.
| #define PSA_ALG_AEAD_TAG_LENGTH_MASK ((psa_algorithm_t) 0x003f0000) |
| #define PSA_AEAD_TAG_LENGTH_OFFSET 16 |
| #define PSA_ALG_AEAD_AT_LEAST_THIS_LENGTH_FLAG ((psa_algorithm_t) 0x00008000) |
| #define PSA_ALG_AEAD_WITH_SHORTENED_TAG | ( | aead_alg, | |
| tag_length | |||
| ) |
Macro to build a shortened AEAD algorithm.
A shortened AEAD algorithm is similar to the corresponding AEAD algorithm, but has an authentication tag that consists of fewer bytes. Depending on the algorithm, the tag length may affect the calculation of the ciphertext.
| aead_alg | An AEAD algorithm identifier (value of type psa_algorithm_t such that PSA_ALG_IS_AEAD(aead_alg) is true). |
| tag_length | Desired length of the authentication tag in bytes. |
aead_alg is not a supported AEAD algorithm or if tag_length is not valid for the specified AEAD algorithm. | #define PSA_ALG_AEAD_GET_TAG_LENGTH | ( | aead_alg | ) |
Retrieve the tag length of a specified AEAD algorithm
| aead_alg | An AEAD algorithm identifier (value of type psa_algorithm_t such that PSA_ALG_IS_AEAD(aead_alg) is true). |
aead_alg is not a supported AEAD algorithm. | #define PSA_ALG_AEAD_WITH_DEFAULT_LENGTH_TAG | ( | aead_alg | ) |
Calculate the corresponding AEAD algorithm with the default tag length.
| aead_alg | An AEAD algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(aead_alg) is true). |
| #define PSA_ALG_AEAD_WITH_DEFAULT_LENGTH_TAG_CASE | ( | aead_alg, | |
| ref | |||
| ) |
| #define PSA_ALG_AEAD_WITH_AT_LEAST_THIS_LENGTH_TAG | ( | aead_alg, | |
| min_tag_length | |||
| ) |
Macro to build an AEAD minimum-tag-length wildcard algorithm.
A minimum-tag-length AEAD wildcard algorithm permits all AEAD algorithms sharing the same base algorithm, and where the tag length of the specific algorithm is equal to or larger then the minimum tag length specified by the wildcard algorithm.
| aead_alg | An AEAD algorithm identifier (value of type psa_algorithm_t such that PSA_ALG_IS_AEAD(aead_alg) is true). |
| min_tag_length | Desired minimum length of the authentication tag in bytes. This must be at least 1 and at most the largest allowed tag length of the algorithm. |
aead_alg is not a supported AEAD algorithm or if min_tag_length is less than 1 or too large for the specified AEAD algorithm. | #define PSA_ALG_RSA_PKCS1V15_SIGN_BASE ((psa_algorithm_t) 0x06000200) |
| #define PSA_ALG_RSA_PKCS1V15_SIGN | ( | hash_alg | ) | (PSA_ALG_RSA_PKCS1V15_SIGN_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
RSA PKCS#1 v1.5 signature with hashing.
This is the signature scheme defined by RFC 8017 (PKCS#1: RSA Cryptography Specifications) under the name RSASSA-PKCS1-v1_5.
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). This includes PSA_ALG_ANY_HASH when specifying the algorithm in a usage policy. |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_RSA_PKCS1V15_SIGN_RAW PSA_ALG_RSA_PKCS1V15_SIGN_BASE |
Raw PKCS#1 v1.5 signature.
The input to this algorithm is the DigestInfo structure used by RFC 8017 (PKCS#1: RSA Cryptography Specifications), §9.2 steps 3–6.
| #define PSA_ALG_IS_RSA_PKCS1V15_SIGN | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_RSA_PKCS1V15_SIGN_BASE) |
| #define PSA_ALG_RSA_PSS_BASE ((psa_algorithm_t) 0x06000300) |
| #define PSA_ALG_RSA_PSS_ANY_SALT_BASE ((psa_algorithm_t) 0x06001300) |
| #define PSA_ALG_RSA_PSS | ( | hash_alg | ) | (PSA_ALG_RSA_PSS_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
RSA PSS signature with hashing.
This is the signature scheme defined by RFC 8017 (PKCS#1: RSA Cryptography Specifications) under the name RSASSA-PSS, with the message generation function MGF1, and with a salt length equal to the length of the hash, or the largest possible salt length for the algorithm and key size if that is smaller than the hash length. The specified hash algorithm is used to hash the input message, to create the salted hash, and for the mask generation.
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). This includes PSA_ALG_ANY_HASH when specifying the algorithm in a usage policy. |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_RSA_PSS_ANY_SALT | ( | hash_alg | ) | (PSA_ALG_RSA_PSS_ANY_SALT_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
RSA PSS signature with hashing with relaxed verification.
This algorithm has the same behavior as PSA_ALG_RSA_PSS when signing, but allows an arbitrary salt length (including 0) when verifying a signature.
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). This includes PSA_ALG_ANY_HASH when specifying the algorithm in a usage policy. |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_IS_RSA_PSS_STANDARD_SALT | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_RSA_PSS_BASE) |
Whether the specified algorithm is RSA PSS with standard salt.
| alg | An algorithm value or an algorithm policy wildcard. |
alg is of the form PSA_ALG_RSA_PSS(hash_alg), where hash_alg is a hash algorithm or PSA_ALG_ANY_HASH. 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier or policy. | #define PSA_ALG_IS_RSA_PSS_ANY_SALT | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_RSA_PSS_ANY_SALT_BASE) |
Whether the specified algorithm is RSA PSS with any salt.
| alg | An algorithm value or an algorithm policy wildcard. |
alg is of the form PSA_ALG_RSA_PSS_ANY_SALT_BASE(hash_alg), where hash_alg is a hash algorithm or PSA_ALG_ANY_HASH. 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier or policy. | #define PSA_ALG_IS_RSA_PSS | ( | alg | ) |
Whether the specified algorithm is RSA PSS.
This includes any of the RSA PSS algorithm variants, regardless of the constraints on salt length.
| alg | An algorithm value or an algorithm policy wildcard. |
alg is of the form PSA_ALG_RSA_PSS(hash_alg) or PSA_ALG_RSA_PSS_ANY_SALT_BASE(hash_alg), where hash_alg is a hash algorithm or PSA_ALG_ANY_HASH. 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier or policy. | #define PSA_ALG_ECDSA_BASE ((psa_algorithm_t) 0x06000600) |
| #define PSA_ALG_ECDSA | ( | hash_alg | ) | (PSA_ALG_ECDSA_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
ECDSA signature with hashing.
This is the ECDSA signature scheme defined by ANSI X9.62, with a random per-message secret number (k).
The representation of the signature as a byte string consists of the concatenation of the signature values r and s. Each of r and s is encoded as an N-octet string, where N is the length of the base point of the curve in octets. Each value is represented in big-endian order (most significant octet first).
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). This includes PSA_ALG_ANY_HASH when specifying the algorithm in a usage policy. |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_ECDSA_ANY PSA_ALG_ECDSA_BASE |
ECDSA signature without hashing.
This is the same signature scheme as PSA_ALG_ECDSA(), but without specifying a hash algorithm. This algorithm may only be used to sign or verify a sequence of bytes that should be an already-calculated hash. Note that the input is padded with zeros on the left or truncated on the left as required to fit the curve size.
| #define PSA_ALG_DETERMINISTIC_ECDSA_BASE ((psa_algorithm_t) 0x06000700) |
| #define PSA_ALG_DETERMINISTIC_ECDSA | ( | hash_alg | ) | (PSA_ALG_DETERMINISTIC_ECDSA_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Deterministic ECDSA signature with hashing.
This is the deterministic ECDSA signature scheme defined by RFC 6979.
The representation of a signature is the same as with PSA_ALG_ECDSA().
Note that when this algorithm is used for verification, signatures made with randomized ECDSA (PSA_ALG_ECDSA(hash_alg)) with the same private key are accepted. In other words, PSA_ALG_DETERMINISTIC_ECDSA(hash_alg) differs from PSA_ALG_ECDSA(hash_alg) only for signature, not for verification.
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). This includes PSA_ALG_ANY_HASH when specifying the algorithm in a usage policy. |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_ECDSA_DETERMINISTIC_FLAG ((psa_algorithm_t) 0x00000100) |
| #define PSA_ALG_IS_ECDSA | ( | alg | ) |
| #define PSA_ALG_ECDSA_IS_DETERMINISTIC | ( | alg | ) | (((alg) & PSA_ALG_ECDSA_DETERMINISTIC_FLAG) != 0) |
| #define PSA_ALG_IS_DETERMINISTIC_ECDSA | ( | alg | ) | (PSA_ALG_IS_ECDSA(alg) && PSA_ALG_ECDSA_IS_DETERMINISTIC(alg)) |
| #define PSA_ALG_IS_RANDOMIZED_ECDSA | ( | alg | ) | (PSA_ALG_IS_ECDSA(alg) && !PSA_ALG_ECDSA_IS_DETERMINISTIC(alg)) |
| #define PSA_ALG_PURE_EDDSA ((psa_algorithm_t) 0x06000800) |
Edwards-curve digital signature algorithm without prehashing (PureEdDSA), using standard parameters.
Contexts are not supported in the current version of this specification because there is no suitable signature interface that can take the context as a parameter. A future version of this specification may add suitable functions and extend this algorithm to support contexts.
PureEdDSA requires an elliptic curve key on a twisted Edwards curve. In this specification, the following curves are supported:
This algorithm can be used with psa_sign_message() and psa_verify_message(). Since there is no prehashing, it cannot be used with psa_sign_hash() or psa_verify_hash().
The signature format is the concatenation of R and S as defined by RFC 8032 s5.1.6 and s5.2.6 (a 64-byte string for Ed25519, a 114-byte string for Ed448).
| #define PSA_ALG_HASH_EDDSA_BASE ((psa_algorithm_t) 0x06000900) |
| #define PSA_ALG_IS_HASH_EDDSA | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_HASH_EDDSA_BASE) |
| #define PSA_ALG_ED25519PH (PSA_ALG_HASH_EDDSA_BASE | (PSA_ALG_SHA_512 & PSA_ALG_HASH_MASK)) |
Edwards-curve digital signature algorithm with prehashing (HashEdDSA), using SHA-512 and the Edwards25519 curve.
See PSA_ALG_PURE_EDDSA regarding context support and the signature format.
This algorithm is Ed25519 as specified in RFC 8032. The curve is Edwards25519. The prehash is SHA-512. The hash function used internally is SHA-512.
This is a hash-and-sign algorithm: to calculate a signature, you can either:
| #define PSA_ALG_ED448PH (PSA_ALG_HASH_EDDSA_BASE | (PSA_ALG_SHAKE256_512 & PSA_ALG_HASH_MASK)) |
Edwards-curve digital signature algorithm with prehashing (HashEdDSA), using SHAKE256 and the Edwards448 curve.
See PSA_ALG_PURE_EDDSA regarding context support and the signature format.
This algorithm is Ed448 as specified in RFC 8032. The curve is Edwards448. The prehash is the first 64 bytes of the SHAKE256 output. The hash function used internally is the first 114 bytes of the SHAKE256 output.
This is a hash-and-sign algorithm: to calculate a signature, you can either:
| #define PSA_ALG_IS_VENDOR_HASH_AND_SIGN | ( | alg | ) | 0 |
| #define PSA_ALG_IS_SIGN_HASH | ( | alg | ) |
Whether the specified algorithm is a signature algorithm that can be used with psa_sign_hash() and psa_verify_hash().
This encompasses all strict hash-and-sign algorithms categorized by PSA_ALG_IS_HASH_AND_SIGN(), as well as algorithms that follow the paradigm more loosely:
| alg | An algorithm identifier (value of type psa_algorithm_t). |
| #define PSA_ALG_IS_SIGN_MESSAGE | ( | alg | ) | (PSA_ALG_IS_SIGN_HASH(alg) || (alg) == PSA_ALG_PURE_EDDSA) |
Whether the specified algorithm is a signature algorithm that can be used with psa_sign_message() and psa_verify_message().
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a signature algorithm that can only be used to sign an already-calculated hash. 0 if alg is not a signature algorithm. This macro can return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_HASH_AND_SIGN | ( | alg | ) |
Whether the specified algorithm is a hash-and-sign algorithm.
Hash-and-sign algorithms are asymmetric (public-key) signature algorithms structured in two parts: first the calculation of a hash in a way that does not depend on the key, then the calculation of a signature from the hash value and the key. Hash-and-sign algorithms encode the hash used for the hashing step, and you can call PSA_ALG_SIGN_GET_HASH to extract this algorithm.
Thus, for a hash-and-sign algorithm, psa_sign_message(key, alg, input, ...) is equivalent to
Most usefully, separating the hash from the signature allows the hash to be calculated in multiple steps with psa_hash_setup(), psa_hash_update() and psa_hash_finish(). Likewise psa_verify_message() is equivalent to calculating the hash and then calling psa_verify_hash().
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a hash-and-sign algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_SIGN_GET_HASH | ( | alg | ) |
Get the hash used by a hash-and-sign signature algorithm.
A hash-and-sign algorithm is a signature algorithm which is composed of two phases: first a hashing phase which does not use the key and produces a hash of the input message, then a signing phase which only uses the hash and the key and not the message itself.
| alg | A signature algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_SIGN(alg) is true). |
alg is a hash-and-sign algorithm. alg is a signature algorithm that does not follow the hash-and-sign structure. alg is not a signature algorithm or if it is not supported by the implementation. | #define PSA_ALG_RSA_PKCS1V15_CRYPT ((psa_algorithm_t) 0x07000200) |
RSA PKCS#1 v1.5 encryption.
| #define PSA_ALG_RSA_OAEP_BASE ((psa_algorithm_t) 0x07000300) |
| #define PSA_ALG_RSA_OAEP | ( | hash_alg | ) | (PSA_ALG_RSA_OAEP_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
RSA OAEP encryption.
This is the encryption scheme defined by RFC 8017 (PKCS#1: RSA Cryptography Specifications) under the name RSAES-OAEP, with the message generation function MGF1.
| hash_alg | The hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true) to use for MGF1. |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_IS_RSA_OAEP | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_RSA_OAEP_BASE) |
| #define PSA_ALG_RSA_OAEP_GET_HASH | ( | alg | ) |
| #define PSA_ALG_HKDF_BASE ((psa_algorithm_t) 0x08000100) |
| #define PSA_ALG_HKDF | ( | hash_alg | ) | (PSA_ALG_HKDF_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Macro to build an HKDF algorithm.
For example, PSA_ALG_HKDF(PSA_ALG_SHA_256) is HKDF using HMAC-SHA-256.
This key derivation algorithm uses the following inputs:
PSA_KEY_DERIVATION_INPUT_INFO is the info string used in the "expand" step. You must pass PSA_KEY_DERIVATION_INPUT_SALT before PSA_KEY_DERIVATION_INPUT_SECRET. You may pass PSA_KEY_DERIVATION_INPUT_INFO at any time after steup and before starting to generate output.
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_IS_HKDF | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_HKDF_BASE) |
Whether the specified algorithm is an HKDF algorithm.
HKDF is a family of key derivation algorithms that are based on a hash function and the HMAC construction.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an HKDF algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key derivation algorithm identifier. | #define PSA_ALG_HKDF_GET_HASH | ( | hkdf_alg | ) | (PSA_ALG_CATEGORY_HASH | ((hkdf_alg) & PSA_ALG_HASH_MASK)) |
| #define PSA_ALG_HKDF_EXTRACT_BASE ((psa_algorithm_t) 0x08000400) |
| #define PSA_ALG_HKDF_EXTRACT | ( | hash_alg | ) | (PSA_ALG_HKDF_EXTRACT_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Macro to build an HKDF-Extract algorithm.
For example, PSA_ALG_HKDF_EXTRACT(PSA_ALG_SHA_256) is HKDF-Extract using HMAC-SHA-256.
This key derivation algorithm uses the following inputs:
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_IS_HKDF_EXTRACT | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_HKDF_EXTRACT_BASE) |
Whether the specified algorithm is an HKDF-Extract algorithm.
HKDF-Extract is a family of key derivation algorithms that are based on a hash function and the HMAC construction.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an HKDF-Extract algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key derivation algorithm identifier. | #define PSA_ALG_HKDF_EXPAND_BASE ((psa_algorithm_t) 0x08000500) |
| #define PSA_ALG_HKDF_EXPAND | ( | hash_alg | ) | (PSA_ALG_HKDF_EXPAND_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Macro to build an HKDF-Expand algorithm.
For example, PSA_ALG_HKDF_EXPAND(PSA_ALG_SHA_256) is HKDF-Expand using HMAC-SHA-256.
This key derivation algorithm uses the following inputs:
The inputs are mandatory and must be passed in the order above. Each input may only be passed once.
PSA_ALG_HKDF should be used instead if possible. PSA_ALG_HKDF_EXPAND is provided as a separate algorithm for the sake of protocols that use it as a building block. It may also be a slight performance optimization in applications that use HKDF with the same salt and key but many different info strings.| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_IS_HKDF_EXPAND | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_HKDF_EXPAND_BASE) |
Whether the specified algorithm is an HKDF-Expand algorithm.
HKDF-Expand is a family of key derivation algorithms that are based on a hash function and the HMAC construction.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an HKDF-Expand algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key derivation algorithm identifier. | #define PSA_ALG_IS_ANY_HKDF | ( | alg | ) |
Whether the specified algorithm is an HKDF or HKDF-Extract or HKDF-Expand algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is any HKDF type algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key derivation algorithm identifier. | #define PSA_ALG_SP800_108_COUNTER_MAC_BASE ((psa_algorithm_t)0x08000400U) |
| #define PSA_ALG_SP800_108_COUNTER_CMAC (PSA_ALG_SP800_108_COUNTER_MAC_BASE | (0x01)) |
Macro to build a NIST SP 800-108 conformant, counter-mode KDF algorithm based on CMAC.
This is a CMAC-based, counter mode key derivation function, using the construction recommended by Section 4.1 of NIST Special Publication 800-108r1: Recommendation for Key Derivation Using Pseudorandom Functions.
This key derivation algorithm uses the following inputs, which must be passed in the order given here:
| #define PSA_ALG_SP800_108_COUNTER_HMAC | ( | hash_alg | ) | (PSA_ALG_SP800_108_COUNTER_MAC_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Macro to build a NIST SP 800-108 conformant, counter-mode KDF algorithm based on HMAC.
This is an HMAC-based, counter mode key derivation function, using the construction recommended by Section 4.1 of NIST Special Publication 800-108r1: Recommendation for Key Derivation Using Pseudorandom Functions.
This key derivation algorithm uses the following inputs, which must be passed in the order given here:
| #define PSA_ALG_IS_SP800_108_COUNTER_MAC | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_SP800_108_COUNTER_MAC_BASE) |
Whether the specified algorithm is a NIST SP 800-108 conformant, counter-mode KDF algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is the specified algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key derivation algorithm identifier. | #define PSA_ALG_TLS12_PRF_BASE ((psa_algorithm_t) 0x08000200) |
| #define PSA_ALG_TLS12_PRF | ( | hash_alg | ) | (PSA_ALG_TLS12_PRF_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Macro to build a TLS-1.2 PRF algorithm.
TLS 1.2 uses a custom pseudorandom function (PRF) for key schedule, specified in Section 5 of RFC 5246. It is based on HMAC and can be used with either SHA-256 or SHA-384.
This key derivation algorithm uses the following inputs, which must be passed in the order given here:
For the application to TLS-1.2 key expansion, the seed is the concatenation of ServerHello.Random + ClientHello.Random, and the label is "key expansion".
For example, PSA_ALG_TLS12_PRF(PSA_ALG_SHA_256) represents the TLS 1.2 PRF using HMAC-SHA-256.
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_IS_TLS12_PRF | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_TLS12_PRF_BASE) |
Whether the specified algorithm is a TLS-1.2 PRF algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a TLS-1.2 PRF algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key derivation algorithm identifier. | #define PSA_ALG_TLS12_PRF_GET_HASH | ( | hkdf_alg | ) | (PSA_ALG_CATEGORY_HASH | ((hkdf_alg) & PSA_ALG_HASH_MASK)) |
| #define PSA_ALG_TLS12_PSK_TO_MS_BASE ((psa_algorithm_t) 0x08000300) |
| #define PSA_ALG_TLS12_PSK_TO_MS | ( | hash_alg | ) | (PSA_ALG_TLS12_PSK_TO_MS_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Macro to build a TLS-1.2 PSK-to-MasterSecret algorithm.
In a pure-PSK handshake in TLS 1.2, the master secret is derived from the PreSharedKey (PSK) through the application of padding (RFC 4279, Section 2) and the TLS-1.2 PRF (RFC 5246, Section 5). The latter is based on HMAC and can be used with either SHA-256 or SHA-384.
This key derivation algorithm uses the following inputs, which must be passed in the order given here:
For the application to TLS-1.2, the seed (which is forwarded to the TLS-1.2 PRF) is the concatenation of the ClientHello.Random + ServerHello.Random, the label is "master secret" or "extended master secret" and the other secret depends on the key exchange specified in the cipher suite:
psa_raw_key_agreement() passed with psa_key_derivation_input_bytes(), or an equivalent input passed with psa_key_derivation_input_bytes() or psa_key_derivation_input_key().psa_key_derivation_input_bytes().For example, PSA_ALG_TLS12_PSK_TO_MS(PSA_ALG_SHA_256) represents the TLS-1.2 PSK to MasterSecret derivation PRF using HMAC-SHA-256.
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_IS_TLS12_PSK_TO_MS | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_TLS12_PSK_TO_MS_BASE) |
Whether the specified algorithm is a TLS-1.2 PSK to MS algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a TLS-1.2 PSK to MS algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key derivation algorithm identifier. | #define PSA_ALG_TLS12_PSK_TO_MS_GET_HASH | ( | hkdf_alg | ) | (PSA_ALG_CATEGORY_HASH | ((hkdf_alg) & PSA_ALG_HASH_MASK)) |
| #define PSA_ALG_TLS12_ECJPAKE_TO_PMS ((psa_algorithm_t) 0x08000609) |
| #define PSA_ALG_KEY_DERIVATION_STRETCHING_FLAG ((psa_algorithm_t) 0x00800000) |
| #define PSA_ALG_PBKDF2_HMAC_BASE ((psa_algorithm_t) 0x08800100) |
| #define PSA_ALG_PBKDF2_HMAC | ( | hash_alg | ) | (PSA_ALG_PBKDF2_HMAC_BASE | ((hash_alg) & PSA_ALG_HASH_MASK)) |
Macro to build a PBKDF2-HMAC password hashing / key stretching algorithm.
PBKDF2 is defined by PKCS#5, republished as RFC 8018 (section 5.2). This macro specifies the PBKDF2 algorithm constructed using a PRF based on HMAC with the specified hash. For example, PSA_ALG_PBKDF2_HMAC(PSA_ALG_SHA_256) specifies PBKDF2 using the PRF HMAC-SHA-256.
This key derivation algorithm uses the following inputs, which must be provided in the following order:
| hash_alg | A hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(hash_alg) is true). |
hash_alg is not a supported hash algorithm. | #define PSA_ALG_IS_PBKDF2_HMAC | ( | alg | ) | (((alg) & ~PSA_ALG_HASH_MASK) == PSA_ALG_PBKDF2_HMAC_BASE) |
Whether the specified algorithm is a PBKDF2-HMAC algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a PBKDF2-HMAC algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key derivation algorithm identifier. | #define PSA_ALG_PBKDF2_HMAC_GET_HASH | ( | pbkdf2_alg | ) | (PSA_ALG_CATEGORY_HASH | ((pbkdf2_alg) & PSA_ALG_HASH_MASK)) |
| #define PSA_ALG_PBKDF2_AES_CMAC_PRF_128 ((psa_algorithm_t) 0x08800200) |
The PBKDF2-AES-CMAC-PRF-128 password hashing / key stretching algorithm.
PBKDF2 is defined by PKCS#5, republished as RFC 8018 (section 5.2). This macro specifies the PBKDF2 algorithm constructed using the AES-CMAC-PRF-128 PRF specified by RFC 4615.
This key derivation algorithm uses the same inputs as PSA_ALG_PBKDF2_HMAC() with the same constraints.
| #define PSA_ALG_IS_PBKDF2 | ( | kdf_alg | ) |
| #define PSA_ALG_KEY_DERIVATION_MASK ((psa_algorithm_t) 0xfe00ffff) |
| #define PSA_ALG_KEY_AGREEMENT_MASK ((psa_algorithm_t) 0xffff0000) |
| #define PSA_ALG_KEY_AGREEMENT | ( | ka_alg, | |
| kdf_alg | |||
| ) | ((ka_alg) | (kdf_alg)) |
Macro to build a combined algorithm that chains a key agreement with a key derivation.
| ka_alg | A key agreement algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_KEY_AGREEMENT(ka_alg) is true). |
| kdf_alg | A key derivation algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_KEY_DERIVATION(kdf_alg) is true). |
ka_alg is not a supported key agreement algorithm or kdf_alg is not a supported key derivation algorithm. | #define PSA_ALG_KEY_AGREEMENT_GET_KDF | ( | alg | ) | (((alg) & PSA_ALG_KEY_DERIVATION_MASK) | PSA_ALG_CATEGORY_KEY_DERIVATION) |
| #define PSA_ALG_KEY_AGREEMENT_GET_BASE | ( | alg | ) | (((alg) & PSA_ALG_KEY_AGREEMENT_MASK) | PSA_ALG_CATEGORY_KEY_AGREEMENT) |
| #define PSA_ALG_IS_RAW_KEY_AGREEMENT | ( | alg | ) |
Whether the specified algorithm is a raw key agreement algorithm.
A raw key agreement algorithm is one that does not specify a key derivation function. Usually, raw key agreement algorithms are constructed directly with a PSA_ALG_xxx macro while non-raw key agreement algorithms are constructed with PSA_ALG_KEY_AGREEMENT().
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a raw key agreement algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported algorithm identifier. | #define PSA_ALG_IS_KEY_DERIVATION_OR_AGREEMENT | ( | alg | ) | ((PSA_ALG_IS_KEY_DERIVATION(alg) || PSA_ALG_IS_KEY_AGREEMENT(alg))) |
| #define PSA_ALG_FFDH ((psa_algorithm_t) 0x09010000) |
The finite-field Diffie-Hellman (DH) key agreement algorithm.
The shared secret produced by key agreement is g^{ab} in big-endian format. It is ceiling(m / 8) bytes long where m is the size of the prime p in bits.
| #define PSA_ALG_IS_FFDH | ( | alg | ) | (PSA_ALG_KEY_AGREEMENT_GET_BASE(alg) == PSA_ALG_FFDH) |
Whether the specified algorithm is a finite field Diffie-Hellman algorithm.
This includes the raw finite field Diffie-Hellman algorithm as well as finite-field Diffie-Hellman followed by any supporter key derivation algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a finite field Diffie-Hellman algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key agreement algorithm identifier. | #define PSA_ALG_ECDH ((psa_algorithm_t) 0x09020000) |
The elliptic curve Diffie-Hellman (ECDH) key agreement algorithm.
The shared secret produced by key agreement is the x-coordinate of the shared secret point. It is always ceiling(m / 8) bytes long where m is the bit size associated with the curve, i.e. the bit size of the order of the curve's coordinate field. When m is not a multiple of 8, the byte containing the most significant bit of the shared secret is padded with zero bits. The byte order is either little-endian or big-endian depending on the curve type.
PSA_ECC_FAMILY_CURVEXXX), the shared secret is the x-coordinate of d_A Q_B = d_B Q_A in little-endian byte order. The bit size is 448 for Curve448 and 255 for Curve25519.PSA_ECC_FAMILY_SECPXXX and PSA_ECC_FAMILY_BRAINPOOL_PXXX), the shared secret is the x-coordinate of d_A Q_B = d_B Q_A in big-endian byte order. The bit size is m = ceiling(log_2(p)) for the field F_p.PSA_ECC_FAMILY_SECTXXX), the shared secret is the x-coordinate of d_A Q_B = d_B Q_A in big-endian byte order. The bit size is m for the field F_{2^m}. | #define PSA_ALG_IS_ECDH | ( | alg | ) | (PSA_ALG_KEY_AGREEMENT_GET_BASE(alg) == PSA_ALG_ECDH) |
Whether the specified algorithm is an elliptic curve Diffie-Hellman algorithm.
This includes the raw elliptic curve Diffie-Hellman algorithm as well as elliptic curve Diffie-Hellman followed by any supporter key derivation algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is an elliptic curve Diffie-Hellman algorithm, 0 otherwise. This macro may return either 0 or 1 if alg is not a supported key agreement algorithm identifier. | #define PSA_ALG_IS_WILDCARD | ( | alg | ) |
Whether the specified algorithm encoding is a wildcard.
Wildcard values may only be used to set the usage algorithm field in a policy, not to perform an operation.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
alg is a wildcard algorithm encoding. alg is a non-wildcard algorithm encoding (suitable for an operation). alg is not a supported algorithm identifier. | #define PSA_ALG_GET_HASH | ( | alg | ) | (((alg) & 0x000000ff) == 0 ? ((psa_algorithm_t) 0) : 0x02000000 | ((alg) & 0x000000ff)) |
Get the hash used by a composite algorithm.
| alg | An algorithm identifier (value of type psa_algorithm_t). |
0 if alg is not a composite algorithm that uses a hash. | typedef uint16_t psa_key_type_t |
Encoding of a key type.
Values of this type are generally constructed by macros called PSA_KEY_TYPE_xxx.
| typedef uint8_t psa_ecc_family_t |
The type of PSA elliptic curve family identifiers.
Values of this type are generally constructed by macros called PSA_ECC_FAMILY_xxx.
The curve identifier is required to create an ECC key using the PSA_KEY_TYPE_ECC_KEY_PAIR() or PSA_KEY_TYPE_ECC_PUBLIC_KEY() macros.
Values defined by this standard will never be in the range 0x80-0xff. Vendors who define additional families must use an encoding in this range.
| typedef uint8_t psa_dh_family_t |
The type of PSA Diffie-Hellman group family identifiers.
Values of this type are generally constructed by macros called PSA_DH_FAMILY_xxx.
The group identifier is required to create a Diffie-Hellman key using the PSA_KEY_TYPE_DH_KEY_PAIR() or PSA_KEY_TYPE_DH_PUBLIC_KEY() macros.
Values defined by this standard will never be in the range 0x80-0xff. Vendors who define additional families must use an encoding in this range.
| typedef uint32_t psa_algorithm_t |
Encoding of a cryptographic algorithm.
Values of this type are generally constructed by macros called PSA_ALG_xxx.
For algorithms that can be applied to multiple key types, this type does not encode the key type. For example, for symmetric ciphers based on a block cipher, psa_algorithm_t encodes the block cipher mode and the padding mode while the block cipher itself is encoded via psa_key_type_t.