Data Structures | Macros | Typedefs | Functions
crypto_types.h File Reference

Detailed Description

PSA cryptography module: type aliases.

Note
This file may not be included directly. Applications must include psa/crypto.h. Drivers must include the appropriate driver header file.

This file contains portable definitions of integral types for properties of cryptographic keys, designations of cryptographic algorithms, and error codes returned by the library.

This header file does not declare any function.

#include <stdint.h>
Include dependency graph for crypto_types.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  mbedtls_svc_key_id_t
 

Macros

#define MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER
 

Typedefs

typedef int32_t psa_status_t
 Function return status. More...
 
typedef uint16_t psa_key_type_t
 Encoding of a key type. More...
 
typedef uint8_t psa_ecc_family_t
 
typedef uint8_t psa_dh_family_t
 
typedef uint32_t psa_algorithm_t
 Encoding of a cryptographic algorithm. More...
 
typedef uint32_t psa_key_lifetime_t
 
typedef uint8_t psa_key_persistence_t
 
typedef uint32_t psa_key_location_t
 
typedef uint32_t psa_key_id_t
 
typedef int32_t mbedtls_key_owner_id_t
 
typedef uint32_t psa_key_usage_t
 Encoding of permitted usage on a key. More...
 
typedef struct psa_key_attributes_s psa_key_attributes_t
 
typedef uint16_t psa_key_derivation_step_t
 Encoding of the step of a key derivation. More...
 

Functions

static int mbedtls_key_owner_id_equal (mbedtls_key_owner_id_t id1, mbedtls_key_owner_id_t id2)
 

Macro Definition Documentation

§ MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER

#define MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale