Macros
crypto_sizes.h File Reference

Detailed Description

PSA cryptography module: Mbed TLS buffer size macros.

Note
This file may not be included directly. Applications must include psa/crypto.h.

This file contains the definitions of macros that are useful to compute buffer sizes. The signatures and semantics of these macros are standardized, but the definitions are not, because they depend on the available algorithms and, in some cases, on permitted tolerances on buffer sizes.

In implementations with isolation between the application and the cryptography module, implementers should take care to ensure that the definitions that are exposed to applications match what the module implements.

Macros that compute sizes whose values do not depend on the implementation are in crypto.h.

This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Macros

#define PSA_BITS_TO_BYTES(bits)   (((bits) + 7u) / 8u)
 
#define PSA_BYTES_TO_BITS(bytes)   ((bytes) * 8u)
 
#define PSA_MAX_OF_THREE(a, b, c)
 
#define PSA_ROUND_UP_TO_MULTIPLE(block_size, length)   (((length) + (block_size) - 1) / (block_size) * (block_size))
 
#define PSA_HASH_LENGTH(alg)
 
#define PSA_HASH_BLOCK_LENGTH(alg)
 
#define PSA_HMAC_MAX_HASH_BLOCK_SIZE   64u
 
#define PSA_HASH_MAX_SIZE   20u
 
#define PSA_HASH_SUSPEND_INPUT_LENGTH_FIELD_LENGTH(alg)
 
#define PSA_HASH_SUSPEND_HASH_STATE_FIELD_LENGTH(alg)
 
#define PSA_HASH_SUSPEND_OUTPUT_SIZE(alg)
 
#define PSA_HASH_SUSPEND_OUTPUT_MAX_SIZE   PSA_HASH_SUSPEND_OUTPUT_SIZE(PSA_ALG_SHA_512)
 
#define PSA_MAC_MAX_SIZE   PSA_HASH_MAX_SIZE
 
#define PSA_AEAD_TAG_LENGTH(key_type, key_bits, alg)
 
#define PSA_AEAD_TAG_MAX_SIZE   16u
 
#define PSA_VENDOR_RSA_MAX_KEY_BITS   4096u
 
#define PSA_VENDOR_RSA_GENERATE_MIN_KEY_BITS   1024
 
#define PSA_VENDOR_FFDH_MAX_KEY_BITS   8192u
 
#define PSA_VENDOR_ECC_MAX_CURVE_BITS   0u
 
#define PSA_TLS12_PSK_TO_MS_PSK_MAX_SIZE   128u
 
#define PSA_TLS12_ECJPAKE_TO_PMS_INPUT_SIZE   65u
 
#define PSA_TLS12_ECJPAKE_TO_PMS_DATA_SIZE   32u
 
#define PSA_VENDOR_PBKDF2_MAX_ITERATIONS   0xffffffffU
 
#define PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE   16u
 
#define PSA_MAC_LENGTH(key_type, key_bits, alg)
 
#define PSA_AEAD_ENCRYPT_OUTPUT_SIZE(key_type, alg, plaintext_length)
 
#define PSA_AEAD_ENCRYPT_OUTPUT_MAX_SIZE(plaintext_length)   ((plaintext_length) + PSA_AEAD_TAG_MAX_SIZE)
 
#define PSA_AEAD_DECRYPT_OUTPUT_SIZE(key_type, alg, ciphertext_length)
 
#define PSA_AEAD_DECRYPT_OUTPUT_MAX_SIZE(ciphertext_length)   (ciphertext_length)
 
#define PSA_AEAD_NONCE_LENGTH(key_type, alg)
 
#define PSA_AEAD_NONCE_MAX_SIZE   13u
 
#define PSA_AEAD_UPDATE_OUTPUT_SIZE(key_type, alg, input_length)
 
#define PSA_AEAD_UPDATE_OUTPUT_MAX_SIZE(input_length)   (PSA_ROUND_UP_TO_MULTIPLE(PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE, (input_length)))
 
#define PSA_AEAD_FINISH_OUTPUT_SIZE(key_type, alg)
 
#define PSA_AEAD_FINISH_OUTPUT_MAX_SIZE   (PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE)
 
#define PSA_AEAD_VERIFY_OUTPUT_SIZE(key_type, alg)
 
#define PSA_AEAD_VERIFY_OUTPUT_MAX_SIZE   (PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE)
 
#define PSA_RSA_MINIMUM_PADDING_SIZE(alg)
 
#define PSA_ECDSA_SIGNATURE_SIZE(curve_bits)   (PSA_BITS_TO_BYTES(curve_bits) * 2u)
 ECDSA signature size for a given curve bit size. More...
 
#define PSA_SIGN_OUTPUT_SIZE(key_type, key_bits, alg)
 
#define PSA_VENDOR_ECDSA_SIGNATURE_MAX_SIZE   PSA_ECDSA_SIGNATURE_SIZE(PSA_VENDOR_ECC_MAX_CURVE_BITS)
 
#define PSA_SIGNATURE_MAX_SIZE   1
 
#define PSA_ASYMMETRIC_ENCRYPT_OUTPUT_SIZE(key_type, key_bits, alg)
 
#define PSA_ASYMMETRIC_ENCRYPT_OUTPUT_MAX_SIZE   (PSA_BITS_TO_BYTES(PSA_VENDOR_RSA_MAX_KEY_BITS))
 
#define PSA_ASYMMETRIC_DECRYPT_OUTPUT_SIZE(key_type, key_bits, alg)
 
#define PSA_ASYMMETRIC_DECRYPT_OUTPUT_MAX_SIZE   (PSA_BITS_TO_BYTES(PSA_VENDOR_RSA_MAX_KEY_BITS))
 
#define PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE(bits)   ((bits) / 8u + 5u)
 
#define PSA_KEY_EXPORT_RSA_PUBLIC_KEY_MAX_SIZE(key_bits)   (PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE(key_bits) + 11u)
 
#define PSA_KEY_EXPORT_RSA_KEY_PAIR_MAX_SIZE(key_bits)   (9u * PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE((key_bits) / 2u + 1u) + 14u)
 
#define PSA_KEY_EXPORT_DSA_PUBLIC_KEY_MAX_SIZE(key_bits)   (PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE(key_bits) * 3u + 59u)
 
#define PSA_KEY_EXPORT_DSA_KEY_PAIR_MAX_SIZE(key_bits)   (PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE(key_bits) * 3u + 75u)
 
#define PSA_KEY_EXPORT_ECC_PUBLIC_KEY_MAX_SIZE(key_bits)   (2u * PSA_BITS_TO_BYTES(key_bits) + 1u)
 
#define PSA_KEY_EXPORT_ECC_KEY_PAIR_MAX_SIZE(key_bits)   (PSA_BITS_TO_BYTES(key_bits))
 
#define PSA_KEY_EXPORT_FFDH_KEY_PAIR_MAX_SIZE(key_bits)   (PSA_BITS_TO_BYTES(key_bits))
 
#define PSA_KEY_EXPORT_FFDH_PUBLIC_KEY_MAX_SIZE(key_bits)   (PSA_BITS_TO_BYTES(key_bits))
 
#define PSA_EXPORT_KEY_OUTPUT_SIZE(key_type, key_bits)
 
#define PSA_EXPORT_PUBLIC_KEY_OUTPUT_SIZE(key_type, key_bits)
 
#define PSA_EXPORT_KEY_PAIR_MAX_SIZE   1
 
#define PSA_EXPORT_PUBLIC_KEY_MAX_SIZE   1
 
#define PSA_RAW_KEY_AGREEMENT_OUTPUT_SIZE(key_type, key_bits)
 
#define PSA_RAW_KEY_AGREEMENT_OUTPUT_MAX_SIZE   1
 
#define PSA_CIPHER_IV_LENGTH(key_type, alg)
 
#define PSA_CIPHER_IV_MAX_SIZE   16u
 
#define PSA_CIPHER_ENCRYPT_OUTPUT_SIZE(key_type, alg, input_length)
 
#define PSA_CIPHER_ENCRYPT_OUTPUT_MAX_SIZE(input_length)
 
#define PSA_CIPHER_DECRYPT_OUTPUT_SIZE(key_type, alg, input_length)
 
#define PSA_CIPHER_DECRYPT_OUTPUT_MAX_SIZE(input_length)   (input_length)
 
#define PSA_CIPHER_UPDATE_OUTPUT_SIZE(key_type, alg, input_length)
 
#define PSA_CIPHER_UPDATE_OUTPUT_MAX_SIZE(input_length)   (PSA_ROUND_UP_TO_MULTIPLE(PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE, input_length))
 
#define PSA_CIPHER_FINISH_OUTPUT_SIZE(key_type, alg)
 
#define PSA_CIPHER_FINISH_OUTPUT_MAX_SIZE   (PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE)
 

Macro Definition Documentation

§ PSA_BITS_TO_BYTES

#define PSA_BITS_TO_BYTES (   bits)    (((bits) + 7u) / 8u)

§ PSA_BYTES_TO_BITS

#define PSA_BYTES_TO_BITS (   bytes)    ((bytes) * 8u)

§ PSA_MAX_OF_THREE

#define PSA_MAX_OF_THREE (   a,
  b,
 
)
Value:
((a) <= (b) ? (b) <= (c) ? \
(c) : (b) : (a) <= (c) ? (c) : (a))

§ PSA_ROUND_UP_TO_MULTIPLE

#define PSA_ROUND_UP_TO_MULTIPLE (   block_size,
  length 
)    (((length) + (block_size) - 1) / (block_size) * (block_size))

§ PSA_HASH_LENGTH

#define PSA_HASH_LENGTH (   alg)
Value:
( \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_MD5 ? 16u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_RIPEMD160 ? 20u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_1 ? 20u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_224 ? 28u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_256 ? 32u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_384 ? 48u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_512 ? 64u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_512_224 ? 28u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_512_256 ? 32u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA3_224 ? 28u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA3_256 ? 32u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA3_384 ? 48u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA3_512 ? 64u : \
0u)
#define PSA_ALG_SHA3_256
Definition: crypto_values.h:981
#define PSA_ALG_SHA3_224
Definition: crypto_values.h:979
#define PSA_ALG_SHA3_512
Definition: crypto_values.h:985
#define PSA_ALG_SHA_256
Definition: crypto_values.h:969
#define PSA_ALG_SHA_512
Definition: crypto_values.h:973
#define PSA_ALG_SHA_224
Definition: crypto_values.h:967
#define PSA_ALG_RIPEMD160
Definition: crypto_values.h:963
#define PSA_ALG_SHA_384
Definition: crypto_values.h:971
#define PSA_ALG_SHA_512_224
Definition: crypto_values.h:975
#define PSA_ALG_SHA_512_256
Definition: crypto_values.h:977
#define PSA_ALG_SHA_1
Definition: crypto_values.h:965
#define PSA_ALG_MD5
Definition: crypto_values.h:961
#define PSA_ALG_SHA3_384
Definition: crypto_values.h:983

The size of the output of psa_hash_finish(), in bytes.

This is also the hash size that psa_hash_verify() expects.

Parameters
algA hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(alg) is true), or an HMAC algorithm (PSA_ALG_HMAC(hash_alg) where hash_alg is a hash algorithm).
Returns
The hash size for the specified hash algorithm. If the hash algorithm is not recognized, return 0.

§ PSA_HASH_BLOCK_LENGTH

#define PSA_HASH_BLOCK_LENGTH (   alg)
Value:
( \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_MD5 ? 64u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_RIPEMD160 ? 64u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_1 ? 64u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_224 ? 64u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_256 ? 64u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_384 ? 128u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_512 ? 128u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_512_224 ? 128u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA_512_256 ? 128u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA3_224 ? 144u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA3_256 ? 136u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA3_384 ? 104u : \
PSA_ALG_HMAC_GET_HASH(alg) == PSA_ALG_SHA3_512 ? 72u : \
0u)
#define PSA_ALG_SHA3_256
Definition: crypto_values.h:981
#define PSA_ALG_SHA3_224
Definition: crypto_values.h:979
#define PSA_ALG_SHA3_512
Definition: crypto_values.h:985
#define PSA_ALG_SHA_256
Definition: crypto_values.h:969
#define PSA_ALG_SHA_512
Definition: crypto_values.h:973
#define PSA_ALG_SHA_224
Definition: crypto_values.h:967
#define PSA_ALG_RIPEMD160
Definition: crypto_values.h:963
#define PSA_ALG_SHA_384
Definition: crypto_values.h:971
#define PSA_ALG_SHA_512_224
Definition: crypto_values.h:975
#define PSA_ALG_SHA_512_256
Definition: crypto_values.h:977
#define PSA_ALG_SHA_1
Definition: crypto_values.h:965
#define PSA_ALG_MD5
Definition: crypto_values.h:961
#define PSA_ALG_SHA3_384
Definition: crypto_values.h:983

The input block size of a hash algorithm, in bytes.

Hash algorithms process their input data in blocks. Hash operations will retain any partial blocks until they have enough input to fill the block or until the operation is finished. This affects the output from psa_hash_suspend().

Parameters
algA hash algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_HASH(alg) is true).
Returns
The block size in bytes for the specified hash algorithm. If the hash algorithm is not recognized, return 0. An implementation can return either 0 or the correct size for a hash algorithm that it recognizes, but does not support.

§ PSA_HMAC_MAX_HASH_BLOCK_SIZE

#define PSA_HMAC_MAX_HASH_BLOCK_SIZE   64u

§ PSA_HASH_MAX_SIZE

#define PSA_HASH_MAX_SIZE   20u

Maximum size of a hash.

This macro expands to a compile-time constant integer. This value is the maximum size of a hash in bytes.

Referenced by psa_aead_operation_init().

§ PSA_HASH_SUSPEND_INPUT_LENGTH_FIELD_LENGTH

#define PSA_HASH_SUSPEND_INPUT_LENGTH_FIELD_LENGTH (   alg)
Value:
(((alg == PSA_ALG_SHA_224) || (alg == PSA_ALG_SHA_256)) ? 8u : \
((alg == PSA_ALG_SHA_384) || (alg == PSA_ALG_SHA_512)) ? 16u : \
0u)
#define PSA_ALG_SHA_256
Definition: crypto_values.h:969
#define PSA_ALG_SHA_512
Definition: crypto_values.h:973
#define PSA_ALG_SHA_224
Definition: crypto_values.h:967
#define PSA_ALG_SHA_384
Definition: crypto_values.h:971

Returns the number of bytes of the input length field for a SHA2 alg. Returns zero if the alg is not SHA2.

§ PSA_HASH_SUSPEND_HASH_STATE_FIELD_LENGTH

#define PSA_HASH_SUSPEND_HASH_STATE_FIELD_LENGTH (   alg)
Value:
(((alg == PSA_ALG_SHA_224) || (alg == PSA_ALG_SHA_256)) ? 32u : \
((alg == PSA_ALG_SHA_384) || (alg == PSA_ALG_SHA_512)) ? 64u : \
0u)
#define PSA_ALG_SHA_256
Definition: crypto_values.h:969
#define PSA_ALG_SHA_512
Definition: crypto_values.h:973
#define PSA_ALG_SHA_224
Definition: crypto_values.h:967
#define PSA_ALG_SHA_384
Definition: crypto_values.h:971

Returns the number of bytes of the hash suspend state field for a SHA2 alg. Returns zero if the alg is not SHA2.

§ PSA_HASH_SUSPEND_OUTPUT_SIZE

#define PSA_HASH_SUSPEND_OUTPUT_SIZE (   alg)
Value:
(4u /* 32-bit algorithm */ + \
PSA_HASH_SUSPEND_INPUT_LENGTH_FIELD_LENGTH(alg) + \
PSA_HASH_SUSPEND_HASH_STATE_FIELD_LENGTH(alg) + \
(PSA_HASH_BLOCK_LENGTH(alg) - 1u) /* max unprocessed input */)
#define PSA_HASH_BLOCK_LENGTH(alg)
Definition: crypto_sizes.h:106

Returns a sufficient hash suspend state buffer size for psa_hash_suspend(), in bytes.

§ PSA_HASH_SUSPEND_OUTPUT_MAX_SIZE

#define PSA_HASH_SUSPEND_OUTPUT_MAX_SIZE   PSA_HASH_SUSPEND_OUTPUT_SIZE(PSA_ALG_SHA_512)

Returns a sufficient hash suspend state buffer size for psa_hash_suspend(), for any supported hash algorithms. SHA-512 is largest supported hash.

§ PSA_MAC_MAX_SIZE

#define PSA_MAC_MAX_SIZE   PSA_HASH_MAX_SIZE

Maximum size of a MAC.

This macro expands to a compile-time constant integer. This value is the maximum size of a MAC in bytes.

§ PSA_AEAD_TAG_LENGTH

#define PSA_AEAD_TAG_LENGTH (   key_type,
  key_bits,
  alg 
)
Value:
(PSA_AEAD_NONCE_LENGTH(key_type, alg) != 0 ? \
PSA_ALG_AEAD_GET_TAG_LENGTH(alg) : \
((void) (key_bits), 0u))
#define PSA_AEAD_NONCE_LENGTH(key_type, alg)
Definition: crypto_sizes.h:504

The length of a tag for an AEAD algorithm, in bytes.

This macro can be used to allocate a buffer of sufficient size to store the tag output from psa_aead_finish().

See also PSA_AEAD_TAG_MAX_SIZE.

Parameters
key_typeThe type of the AEAD key.
key_bitsThe size of the AEAD key in bits.
algAn AEAD algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).
Returns
The tag length for the specified algorithm and key. If the AEAD algorithm does not have an identified tag that can be distinguished from the rest of the ciphertext, return 0. If the key type or AEAD algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_AEAD_TAG_MAX_SIZE

#define PSA_AEAD_TAG_MAX_SIZE   16u

The maximum tag size for all supported AEAD algorithms, in bytes.

See also PSA_AEAD_TAG_LENGTH(key_type, key_bits, alg).

§ PSA_VENDOR_RSA_MAX_KEY_BITS

#define PSA_VENDOR_RSA_MAX_KEY_BITS   4096u

§ PSA_VENDOR_RSA_GENERATE_MIN_KEY_BITS

#define PSA_VENDOR_RSA_GENERATE_MIN_KEY_BITS   1024

§ PSA_VENDOR_FFDH_MAX_KEY_BITS

#define PSA_VENDOR_FFDH_MAX_KEY_BITS   8192u

§ PSA_VENDOR_ECC_MAX_CURVE_BITS

#define PSA_VENDOR_ECC_MAX_CURVE_BITS   0u

§ PSA_TLS12_PSK_TO_MS_PSK_MAX_SIZE

#define PSA_TLS12_PSK_TO_MS_PSK_MAX_SIZE   128u

This macro returns the maximum supported length of the PSK for the TLS-1.2 PSK-to-MS key derivation (PSA_ALG_TLS12_PSK_TO_MS(hash_alg)).

The maximum supported length does not depend on the chosen hash algorithm.

Quoting RFC 4279, Sect 5.3: TLS implementations supporting these ciphersuites MUST support arbitrary PSK identities up to 128 octets in length, and arbitrary PSKs up to 64 octets in length. Supporting longer identities and keys is RECOMMENDED.

Therefore, no implementation should define a value smaller than 64 for PSA_TLS12_PSK_TO_MS_PSK_MAX_SIZE.

§ PSA_TLS12_ECJPAKE_TO_PMS_INPUT_SIZE

#define PSA_TLS12_ECJPAKE_TO_PMS_INPUT_SIZE   65u

§ PSA_TLS12_ECJPAKE_TO_PMS_DATA_SIZE

#define PSA_TLS12_ECJPAKE_TO_PMS_DATA_SIZE   32u

§ PSA_VENDOR_PBKDF2_MAX_ITERATIONS

#define PSA_VENDOR_PBKDF2_MAX_ITERATIONS   0xffffffffU

§ PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE

#define PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE   16u

The maximum size of a block cipher.

§ PSA_MAC_LENGTH

#define PSA_MAC_LENGTH (   key_type,
  key_bits,
  alg 
)
Value:
PSA_ALG_IS_HMAC(alg) ? PSA_HASH_LENGTH(PSA_ALG_HMAC_GET_HASH(alg)) : \
((void) (key_type), (void) (key_bits), 0u))
#define PSA_BLOCK_CIPHER_BLOCK_LENGTH(type)
Definition: crypto_values.h:809
#define PSA_ALG_IS_BLOCK_CIPHER_MAC(alg)
Definition: crypto_values.h:1194
#define PSA_ALG_MAC_TRUNCATION_MASK
Definition: crypto_values.h:1069
#define PSA_ALG_HMAC_GET_HASH(hmac_alg)
Definition: crypto_values.h:1045
#define PSA_MAC_TRUNCATED_LENGTH(mac_alg)
Definition: crypto_values.h:1145
#define PSA_HASH_LENGTH(alg)
Definition: crypto_sizes.h:74

The size of the output of psa_mac_sign_finish(), in bytes.

This is also the MAC size that psa_mac_verify_finish() expects.

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeThe type of the MAC key.
key_bitsThe size of the MAC key in bits.
algA MAC algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_MAC(alg) is true).
Returns
The MAC size for the specified algorithm with the specified key parameters.
0 if the MAC algorithm is not recognized.
Either 0 or the correct size for a MAC algorithm that the implementation recognizes, but does not support.
Unspecified if the key parameters are not consistent with the algorithm.

§ PSA_AEAD_ENCRYPT_OUTPUT_SIZE

#define PSA_AEAD_ENCRYPT_OUTPUT_SIZE (   key_type,
  alg,
  plaintext_length 
)
Value:
(PSA_AEAD_NONCE_LENGTH(key_type, alg) != 0 ? \
(plaintext_length) + PSA_ALG_AEAD_GET_TAG_LENGTH(alg) : \
0u)
#define PSA_AEAD_NONCE_LENGTH(key_type, alg)
Definition: crypto_sizes.h:504
#define PSA_ALG_AEAD_GET_TAG_LENGTH(aead_alg)
Definition: crypto_values.h:1388

The maximum size of the output of psa_aead_encrypt(), in bytes.

If the size of the ciphertext buffer is at least this large, it is guaranteed that psa_aead_encrypt() will not fail due to an insufficient buffer size. Depending on the algorithm, the actual size of the ciphertext may be smaller.

See also PSA_AEAD_ENCRYPT_OUTPUT_MAX_SIZE(plaintext_length).

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algAn AEAD algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).
plaintext_lengthSize of the plaintext in bytes.
Returns
The AEAD ciphertext size for the specified algorithm. If the key type or AEAD algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_AEAD_ENCRYPT_OUTPUT_MAX_SIZE

#define PSA_AEAD_ENCRYPT_OUTPUT_MAX_SIZE (   plaintext_length)    ((plaintext_length) + PSA_AEAD_TAG_MAX_SIZE)

A sufficient output buffer size for psa_aead_encrypt(), for any of the supported key types and AEAD algorithms.

If the size of the ciphertext buffer is at least this large, it is guaranteed that psa_aead_encrypt() will not fail due to an insufficient buffer size.

Note
This macro returns a compile-time constant if its arguments are compile-time constants.

See also PSA_AEAD_ENCRYPT_OUTPUT_SIZE(key_type, alg, plaintext_length).

Parameters
plaintext_lengthSize of the plaintext in bytes.
Returns
A sufficient output buffer size for any of the supported key types and AEAD algorithms.

§ PSA_AEAD_DECRYPT_OUTPUT_SIZE

#define PSA_AEAD_DECRYPT_OUTPUT_SIZE (   key_type,
  alg,
  ciphertext_length 
)
Value:
(PSA_AEAD_NONCE_LENGTH(key_type, alg) != 0 && \
(ciphertext_length) > PSA_ALG_AEAD_GET_TAG_LENGTH(alg) ? \
(ciphertext_length) - PSA_ALG_AEAD_GET_TAG_LENGTH(alg) : \
0u)
#define PSA_AEAD_NONCE_LENGTH(key_type, alg)
Definition: crypto_sizes.h:504
#define PSA_ALG_AEAD_GET_TAG_LENGTH(aead_alg)
Definition: crypto_values.h:1388

The maximum size of the output of psa_aead_decrypt(), in bytes.

If the size of the plaintext buffer is at least this large, it is guaranteed that psa_aead_decrypt() will not fail due to an insufficient buffer size. Depending on the algorithm, the actual size of the plaintext may be smaller.

See also PSA_AEAD_DECRYPT_OUTPUT_MAX_SIZE(ciphertext_length).

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algAn AEAD algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).
ciphertext_lengthSize of the plaintext in bytes.
Returns
The AEAD ciphertext size for the specified algorithm. If the key type or AEAD algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_AEAD_DECRYPT_OUTPUT_MAX_SIZE

#define PSA_AEAD_DECRYPT_OUTPUT_MAX_SIZE (   ciphertext_length)    (ciphertext_length)

A sufficient output buffer size for psa_aead_decrypt(), for any of the supported key types and AEAD algorithms.

If the size of the plaintext buffer is at least this large, it is guaranteed that psa_aead_decrypt() will not fail due to an insufficient buffer size.

Note
This macro returns a compile-time constant if its arguments are compile-time constants.

See also PSA_AEAD_DECRYPT_OUTPUT_SIZE(key_type, alg, ciphertext_length).

Parameters
ciphertext_lengthSize of the ciphertext in bytes.
Returns
A sufficient output buffer size for any of the supported key types and AEAD algorithms.

§ PSA_AEAD_NONCE_LENGTH

#define PSA_AEAD_NONCE_LENGTH (   key_type,
  alg 
)
Value:
(PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type) == 16 ? \
MBEDTLS_PSA_ALG_AEAD_EQUAL(alg, PSA_ALG_CCM) ? 13u : \
MBEDTLS_PSA_ALG_AEAD_EQUAL(alg, PSA_ALG_GCM) ? 12u : \
0u : \
(key_type) == PSA_KEY_TYPE_CHACHA20 && \
0u)
#define PSA_BLOCK_CIPHER_BLOCK_LENGTH(type)
Definition: crypto_values.h:809
#define PSA_KEY_TYPE_CHACHA20
Definition: crypto_values.h:591
#define PSA_ALG_GCM
Definition: crypto_values.h:1326
#define MBEDTLS_PSA_ALG_AEAD_EQUAL(aead_alg_1, aead_alg_2)
Definition: crypto_values.h:2892
#define PSA_ALG_CCM
Definition: crypto_values.h:1309
#define PSA_ALG_CHACHA20_POLY1305
Definition: crypto_values.h:1337

The default nonce size for an AEAD algorithm, in bytes.

This macro can be used to allocate a buffer of sufficient size to store the nonce output from psa_aead_generate_nonce().

See also PSA_AEAD_NONCE_MAX_SIZE.

Note
This is not the maximum size of nonce supported as input to psa_aead_set_nonce(), psa_aead_encrypt() or psa_aead_decrypt(), just the default size that is generated by psa_aead_generate_nonce().
Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algAn AEAD algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).
Returns
The default nonce size for the specified key type and algorithm. If the key type or AEAD algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_AEAD_NONCE_MAX_SIZE

#define PSA_AEAD_NONCE_MAX_SIZE   13u

The maximum default nonce size among all supported pairs of key types and AEAD algorithms, in bytes.

This is equal to or greater than any value that PSA_AEAD_NONCE_LENGTH() may return.

Note
This is not the maximum size of nonce supported as input to psa_aead_set_nonce(), psa_aead_encrypt() or psa_aead_decrypt(), just the largest size that may be generated by psa_aead_generate_nonce().

§ PSA_AEAD_UPDATE_OUTPUT_SIZE

#define PSA_AEAD_UPDATE_OUTPUT_SIZE (   key_type,
  alg,
  input_length 
)
Value:
(PSA_AEAD_NONCE_LENGTH(key_type, alg) != 0 ? \
PSA_ALG_IS_AEAD_ON_BLOCK_CIPHER(alg) ? \
PSA_ROUND_UP_TO_MULTIPLE(PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type), (input_length)) : \
(input_length) : \
0u)
#define PSA_BLOCK_CIPHER_BLOCK_LENGTH(type)
Definition: crypto_values.h:809
#define PSA_AEAD_NONCE_LENGTH(key_type, alg)
Definition: crypto_sizes.h:504

A sufficient output buffer size for psa_aead_update().

If the size of the output buffer is at least this large, it is guaranteed that psa_aead_update() will not fail due to an insufficient buffer size. The actual size of the output may be smaller in any given call.

See also PSA_AEAD_UPDATE_OUTPUT_MAX_SIZE(input_length).

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algAn AEAD algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).
input_lengthSize of the input in bytes.
Returns
A sufficient output buffer size for the specified algorithm. If the key type or AEAD algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_AEAD_UPDATE_OUTPUT_MAX_SIZE

#define PSA_AEAD_UPDATE_OUTPUT_MAX_SIZE (   input_length)    (PSA_ROUND_UP_TO_MULTIPLE(PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE, (input_length)))

A sufficient output buffer size for psa_aead_update(), for any of the supported key types and AEAD algorithms.

If the size of the output buffer is at least this large, it is guaranteed that psa_aead_update() will not fail due to an insufficient buffer size.

See also PSA_AEAD_UPDATE_OUTPUT_SIZE(key_type, alg, input_length).

Parameters
input_lengthSize of the input in bytes.

§ PSA_AEAD_FINISH_OUTPUT_SIZE

#define PSA_AEAD_FINISH_OUTPUT_SIZE (   key_type,
  alg 
)
Value:
(PSA_AEAD_NONCE_LENGTH(key_type, alg) != 0 && \
PSA_ALG_IS_AEAD_ON_BLOCK_CIPHER(alg) ? \
PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type) : \
0u)
#define PSA_AEAD_NONCE_LENGTH(key_type, alg)
Definition: crypto_sizes.h:504

A sufficient ciphertext buffer size for psa_aead_finish().

If the size of the ciphertext buffer is at least this large, it is guaranteed that psa_aead_finish() will not fail due to an insufficient ciphertext buffer size. The actual size of the output may be smaller in any given call.

See also PSA_AEAD_FINISH_OUTPUT_MAX_SIZE.

Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algAn AEAD algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).
Returns
A sufficient ciphertext buffer size for the specified algorithm. If the key type or AEAD algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_AEAD_FINISH_OUTPUT_MAX_SIZE

#define PSA_AEAD_FINISH_OUTPUT_MAX_SIZE   (PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE)

A sufficient ciphertext buffer size for psa_aead_finish(), for any of the supported key types and AEAD algorithms.

See also PSA_AEAD_FINISH_OUTPUT_SIZE(key_type, alg).

§ PSA_AEAD_VERIFY_OUTPUT_SIZE

#define PSA_AEAD_VERIFY_OUTPUT_SIZE (   key_type,
  alg 
)
Value:
(PSA_AEAD_NONCE_LENGTH(key_type, alg) != 0 && \
PSA_ALG_IS_AEAD_ON_BLOCK_CIPHER(alg) ? \
PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type) : \
0u)
#define PSA_AEAD_NONCE_LENGTH(key_type, alg)
Definition: crypto_sizes.h:504

A sufficient plaintext buffer size for psa_aead_verify().

If the size of the plaintext buffer is at least this large, it is guaranteed that psa_aead_verify() will not fail due to an insufficient plaintext buffer size. The actual size of the output may be smaller in any given call.

See also PSA_AEAD_VERIFY_OUTPUT_MAX_SIZE.

Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algAn AEAD algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).
Returns
A sufficient plaintext buffer size for the specified algorithm. If the key type or AEAD algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_AEAD_VERIFY_OUTPUT_MAX_SIZE

#define PSA_AEAD_VERIFY_OUTPUT_MAX_SIZE   (PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE)

A sufficient plaintext buffer size for psa_aead_verify(), for any of the supported key types and AEAD algorithms.

See also PSA_AEAD_VERIFY_OUTPUT_SIZE(key_type, alg).

§ PSA_RSA_MINIMUM_PADDING_SIZE

#define PSA_RSA_MINIMUM_PADDING_SIZE (   alg)
Value:
11u /*PKCS#1v1.5*/)
#define PSA_ALG_RSA_OAEP_GET_HASH(alg)
Definition: crypto_values.h:1826
#define PSA_ALG_IS_RSA_OAEP(alg)
Definition: crypto_values.h:1824
#define PSA_HASH_LENGTH(alg)
Definition: crypto_sizes.h:74

§ PSA_ECDSA_SIGNATURE_SIZE

#define PSA_ECDSA_SIGNATURE_SIZE (   curve_bits)    (PSA_BITS_TO_BYTES(curve_bits) * 2u)

ECDSA signature size for a given curve bit size.

Parameters
curve_bitsCurve size in bits.
Returns
Signature size in bytes.
Note
This macro returns a compile-time constant if its argument is one.

§ PSA_SIGN_OUTPUT_SIZE

#define PSA_SIGN_OUTPUT_SIZE (   key_type,
  key_bits,
  alg 
)
Value:
(PSA_KEY_TYPE_IS_RSA(key_type) ? ((void) alg, PSA_BITS_TO_BYTES(key_bits)) : \
((void) alg, 0u))
#define PSA_KEY_TYPE_IS_RSA(type)
Definition: crypto_values.h:604
#define PSA_ECDSA_SIGNATURE_SIZE(curve_bits)
ECDSA signature size for a given curve bit size.
Definition: crypto_sizes.h:657
#define PSA_KEY_TYPE_IS_ECC(type)
Definition: crypto_values.h:634
#define PSA_BITS_TO_BYTES(bits)
Definition: crypto_sizes.h:54

Sufficient signature buffer size for psa_sign_hash().

This macro returns a sufficient buffer size for a signature using a key of the specified type and size, with the specified algorithm. Note that the actual size of the signature may be smaller (some algorithms produce a variable-size signature).

Warning
This function may call its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeAn asymmetric key type (this may indifferently be a key pair type or a public key type).
key_bitsThe size of the key in bits.
algThe signature algorithm.
Returns
If the parameters are valid and supported, return a buffer size in bytes that guarantees that psa_sign_hash() will not fail with PSA_ERROR_BUFFER_TOO_SMALL. If the parameters are a valid combination that is not supported, return either a sensible size or 0. If the parameters are not valid, the return value is unspecified.

§ PSA_VENDOR_ECDSA_SIGNATURE_MAX_SIZE

#define PSA_VENDOR_ECDSA_SIGNATURE_MAX_SIZE   PSA_ECDSA_SIGNATURE_SIZE(PSA_VENDOR_ECC_MAX_CURVE_BITS)

§ PSA_SIGNATURE_MAX_SIZE

#define PSA_SIGNATURE_MAX_SIZE   1

Maximum size of an asymmetric signature.

This macro expands to a compile-time constant integer. This value is the maximum size of a signature in bytes.

§ PSA_ASYMMETRIC_ENCRYPT_OUTPUT_SIZE

#define PSA_ASYMMETRIC_ENCRYPT_OUTPUT_SIZE (   key_type,
  key_bits,
  alg 
)
Value:
(PSA_KEY_TYPE_IS_RSA(key_type) ? \
((void) alg, PSA_BITS_TO_BYTES(key_bits)) : \
0u)
#define PSA_KEY_TYPE_IS_RSA(type)
Definition: crypto_values.h:604
#define PSA_BITS_TO_BYTES(bits)
Definition: crypto_sizes.h:54

Sufficient output buffer size for psa_asymmetric_encrypt().

This macro returns a sufficient buffer size for a ciphertext produced using a key of the specified type and size, with the specified algorithm. Note that the actual size of the ciphertext may be smaller, depending on the algorithm.

Warning
This function may call its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeAn asymmetric key type (this may indifferently be a key pair type or a public key type).
key_bitsThe size of the key in bits.
algThe asymmetric encryption algorithm.
Returns
If the parameters are valid and supported, return a buffer size in bytes that guarantees that psa_asymmetric_encrypt() will not fail with PSA_ERROR_BUFFER_TOO_SMALL. If the parameters are a valid combination that is not supported, return either a sensible size or 0. If the parameters are not valid, the return value is unspecified.

§ PSA_ASYMMETRIC_ENCRYPT_OUTPUT_MAX_SIZE

#define PSA_ASYMMETRIC_ENCRYPT_OUTPUT_MAX_SIZE   (PSA_BITS_TO_BYTES(PSA_VENDOR_RSA_MAX_KEY_BITS))

A sufficient output buffer size for psa_asymmetric_encrypt(), for any supported asymmetric encryption.

See also PSA_ASYMMETRIC_ENCRYPT_OUTPUT_SIZE(key_type, key_bits, alg).

§ PSA_ASYMMETRIC_DECRYPT_OUTPUT_SIZE

#define PSA_ASYMMETRIC_DECRYPT_OUTPUT_SIZE (   key_type,
  key_bits,
  alg 
)
Value:
(PSA_KEY_TYPE_IS_RSA(key_type) ? \
PSA_BITS_TO_BYTES(key_bits) - PSA_RSA_MINIMUM_PADDING_SIZE(alg) : \
0u)
#define PSA_RSA_MINIMUM_PADDING_SIZE(alg)
Definition: crypto_sizes.h:644
#define PSA_KEY_TYPE_IS_RSA(type)
Definition: crypto_values.h:604

Sufficient output buffer size for psa_asymmetric_decrypt().

This macro returns a sufficient buffer size for a plaintext produced using a key of the specified type and size, with the specified algorithm. Note that the actual size of the plaintext may be smaller, depending on the algorithm.

Warning
This function may call its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeAn asymmetric key type (this may indifferently be a key pair type or a public key type).
key_bitsThe size of the key in bits.
algThe asymmetric encryption algorithm.
Returns
If the parameters are valid and supported, return a buffer size in bytes that guarantees that psa_asymmetric_decrypt() will not fail with PSA_ERROR_BUFFER_TOO_SMALL. If the parameters are a valid combination that is not supported, return either a sensible size or 0. If the parameters are not valid, the return value is unspecified.

§ PSA_ASYMMETRIC_DECRYPT_OUTPUT_MAX_SIZE

#define PSA_ASYMMETRIC_DECRYPT_OUTPUT_MAX_SIZE   (PSA_BITS_TO_BYTES(PSA_VENDOR_RSA_MAX_KEY_BITS))

A sufficient output buffer size for psa_asymmetric_decrypt(), for any supported asymmetric decryption.

This macro assumes that RSA is the only supported asymmetric encryption.

See also PSA_ASYMMETRIC_DECRYPT_OUTPUT_SIZE(key_type, key_bits, alg).

§ PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE

#define PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE (   bits)    ((bits) / 8u + 5u)

§ PSA_KEY_EXPORT_RSA_PUBLIC_KEY_MAX_SIZE

#define PSA_KEY_EXPORT_RSA_PUBLIC_KEY_MAX_SIZE (   key_bits)    (PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE(key_bits) + 11u)

§ PSA_KEY_EXPORT_RSA_KEY_PAIR_MAX_SIZE

#define PSA_KEY_EXPORT_RSA_KEY_PAIR_MAX_SIZE (   key_bits)    (9u * PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE((key_bits) / 2u + 1u) + 14u)

§ PSA_KEY_EXPORT_DSA_PUBLIC_KEY_MAX_SIZE

#define PSA_KEY_EXPORT_DSA_PUBLIC_KEY_MAX_SIZE (   key_bits)    (PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE(key_bits) * 3u + 59u)

§ PSA_KEY_EXPORT_DSA_KEY_PAIR_MAX_SIZE

#define PSA_KEY_EXPORT_DSA_KEY_PAIR_MAX_SIZE (   key_bits)    (PSA_KEY_EXPORT_ASN1_INTEGER_MAX_SIZE(key_bits) * 3u + 75u)

§ PSA_KEY_EXPORT_ECC_PUBLIC_KEY_MAX_SIZE

#define PSA_KEY_EXPORT_ECC_PUBLIC_KEY_MAX_SIZE (   key_bits)    (2u * PSA_BITS_TO_BYTES(key_bits) + 1u)

§ PSA_KEY_EXPORT_ECC_KEY_PAIR_MAX_SIZE

#define PSA_KEY_EXPORT_ECC_KEY_PAIR_MAX_SIZE (   key_bits)    (PSA_BITS_TO_BYTES(key_bits))

§ PSA_KEY_EXPORT_FFDH_KEY_PAIR_MAX_SIZE

#define PSA_KEY_EXPORT_FFDH_KEY_PAIR_MAX_SIZE (   key_bits)    (PSA_BITS_TO_BYTES(key_bits))

§ PSA_KEY_EXPORT_FFDH_PUBLIC_KEY_MAX_SIZE

#define PSA_KEY_EXPORT_FFDH_PUBLIC_KEY_MAX_SIZE (   key_bits)    (PSA_BITS_TO_BYTES(key_bits))

§ PSA_EXPORT_KEY_OUTPUT_SIZE

#define PSA_EXPORT_KEY_OUTPUT_SIZE (   key_type,
  key_bits 
)
Value:
PSA_KEY_TYPE_IS_DH(key_type) ? PSA_BITS_TO_BYTES(key_bits) : \
0u)
#define PSA_KEY_EXPORT_ECC_KEY_PAIR_MAX_SIZE(key_bits)
Definition: crypto_sizes.h:899
#define PSA_KEY_TYPE_RSA_KEY_PAIR
Definition: crypto_values.h:602
#define PSA_KEY_TYPE_IS_DH(type)
Definition: crypto_values.h:763
#define PSA_KEY_TYPE_IS_UNSTRUCTURED(type)
Definition: crypto_values.h:446
#define PSA_KEY_TYPE_DSA_KEY_PAIR
Definition: crypto_extra.h:67
#define PSA_KEY_TYPE_IS_ECC_KEY_PAIR(type)
Definition: crypto_values.h:638
#define PSA_KEY_EXPORT_RSA_KEY_PAIR_MAX_SIZE(key_bits)
Definition: crypto_sizes.h:841
#define PSA_KEY_TYPE_RSA_PUBLIC_KEY
Definition: crypto_values.h:597
#define PSA_KEY_EXPORT_ECC_PUBLIC_KEY_MAX_SIZE(key_bits)
Definition: crypto_sizes.h:892
#define PSA_KEY_EXPORT_DSA_KEY_PAIR_MAX_SIZE(key_bits)
Definition: crypto_sizes.h:879
#define PSA_KEY_TYPE_IS_ECC_PUBLIC_KEY(type)
Definition: crypto_values.h:642
#define PSA_KEY_EXPORT_DSA_PUBLIC_KEY_MAX_SIZE(key_bits)
Definition: crypto_sizes.h:860
#define PSA_KEY_EXPORT_RSA_PUBLIC_KEY_MAX_SIZE(key_bits)
Definition: crypto_sizes.h:816
#define PSA_BITS_TO_BYTES(bits)
Definition: crypto_sizes.h:54
#define PSA_KEY_TYPE_DSA_PUBLIC_KEY
Definition: crypto_extra.h:49

Sufficient output buffer size for psa_export_key() or psa_export_public_key().

This macro returns a compile-time constant if its arguments are compile-time constants.

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.

The following code illustrates how to allocate enough memory to export a key by querying the key type and size at runtime.

psa_status_t status;
status = psa_get_key_attributes(key, &attributes);
if (status != PSA_SUCCESS) handle_error(...);
psa_key_type_t key_type = psa_get_key_type(&attributes);
size_t key_bits = psa_get_key_bits(&attributes);
size_t buffer_size = PSA_EXPORT_KEY_OUTPUT_SIZE(key_type, key_bits);
uint8_t *buffer = malloc(buffer_size);
if (buffer == NULL) handle_error(...);
size_t buffer_length;
status = psa_export_key(key, buffer, buffer_size, &buffer_length);
if (status != PSA_SUCCESS) handle_error(...);
Parameters
key_typeA supported key type.
key_bitsThe size of the key in bits.
Returns
If the parameters are valid and supported, return a buffer size in bytes that guarantees that psa_export_key() or psa_export_public_key() will not fail with PSA_ERROR_BUFFER_TOO_SMALL. If the parameters are a valid combination that is not supported, return either a sensible size or 0. If the parameters are not valid, the return value is unspecified.

§ PSA_EXPORT_PUBLIC_KEY_OUTPUT_SIZE

#define PSA_EXPORT_PUBLIC_KEY_OUTPUT_SIZE (   key_type,
  key_bits 
)
Value:
PSA_KEY_TYPE_IS_DH(key_type) ? PSA_BITS_TO_BYTES(key_bits) : \
0u)
#define PSA_KEY_TYPE_IS_DH(type)
Definition: crypto_values.h:763
#define PSA_KEY_TYPE_IS_RSA(type)
Definition: crypto_values.h:604
#define PSA_KEY_EXPORT_ECC_PUBLIC_KEY_MAX_SIZE(key_bits)
Definition: crypto_sizes.h:892
#define PSA_KEY_TYPE_IS_ECC(type)
Definition: crypto_values.h:634
#define PSA_KEY_EXPORT_RSA_PUBLIC_KEY_MAX_SIZE(key_bits)
Definition: crypto_sizes.h:816
#define PSA_BITS_TO_BYTES(bits)
Definition: crypto_sizes.h:54

Sufficient output buffer size for psa_export_public_key().

This macro returns a compile-time constant if its arguments are compile-time constants.

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.

The following code illustrates how to allocate enough memory to export a public key by querying the key type and size at runtime.

psa_status_t status;
status = psa_get_key_attributes(key, &attributes);
if (status != PSA_SUCCESS) handle_error(...);
psa_key_type_t key_type = psa_get_key_type(&attributes);
size_t key_bits = psa_get_key_bits(&attributes);
size_t buffer_size = PSA_EXPORT_PUBLIC_KEY_OUTPUT_SIZE(key_type, key_bits);
uint8_t *buffer = malloc(buffer_size);
if (buffer == NULL) handle_error(...);
size_t buffer_length;
status = psa_export_public_key(key, buffer, buffer_size, &buffer_length);
if (status != PSA_SUCCESS) handle_error(...);
Parameters
key_typeA public key or key pair key type.
key_bitsThe size of the key in bits.
Returns
If the parameters are valid and supported, return a buffer size in bytes that guarantees that psa_export_public_key() will not fail with PSA_ERROR_BUFFER_TOO_SMALL. If the parameters are a valid combination that is not supported, return either a sensible size or 0. If the parameters are not valid, the return value is unspecified.

If the parameters are valid and supported, return the same result as PSA_EXPORT_KEY_OUTPUT_SIZE( PSA_KEY_TYPE_PUBLIC_KEY_OF_KEY_PAIR(key_type), key_bits).

§ PSA_EXPORT_KEY_PAIR_MAX_SIZE

#define PSA_EXPORT_KEY_PAIR_MAX_SIZE   1

Sufficient buffer size for exporting any asymmetric key pair.

This macro expands to a compile-time constant integer. This value is a sufficient buffer size when calling psa_export_key() to export any asymmetric key pair, regardless of the exact key type and key size.

See also PSA_EXPORT_KEY_OUTPUT_SIZE(key_type, key_bits).

§ PSA_EXPORT_PUBLIC_KEY_MAX_SIZE

#define PSA_EXPORT_PUBLIC_KEY_MAX_SIZE   1

Sufficient buffer size for exporting any asymmetric public key.

This macro expands to a compile-time constant integer. This value is a sufficient buffer size when calling psa_export_key() or psa_export_public_key() to export any asymmetric public key, regardless of the exact key type and key size.

See also PSA_EXPORT_PUBLIC_KEY_OUTPUT_SIZE(key_type, key_bits).

§ PSA_RAW_KEY_AGREEMENT_OUTPUT_SIZE

#define PSA_RAW_KEY_AGREEMENT_OUTPUT_SIZE (   key_type,
  key_bits 
)
Value:
PSA_KEY_TYPE_IS_DH_KEY_PAIR(key_type)) ? PSA_BITS_TO_BYTES(key_bits) : 0u)
#define PSA_KEY_TYPE_IS_ECC_KEY_PAIR(type)
Definition: crypto_values.h:638
#define PSA_BITS_TO_BYTES(bits)
Definition: crypto_sizes.h:54

Sufficient output buffer size for psa_raw_key_agreement().

This macro returns a compile-time constant if its arguments are compile-time constants.

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.

See also PSA_RAW_KEY_AGREEMENT_OUTPUT_MAX_SIZE.

Parameters
key_typeA supported key type.
key_bitsThe size of the key in bits.
Returns
If the parameters are valid and supported, return a buffer size in bytes that guarantees that psa_raw_key_agreement() will not fail with PSA_ERROR_BUFFER_TOO_SMALL. If the parameters are a valid combination that is not supported, return either a sensible size or 0. If the parameters are not valid, the return value is unspecified.

§ PSA_RAW_KEY_AGREEMENT_OUTPUT_MAX_SIZE

#define PSA_RAW_KEY_AGREEMENT_OUTPUT_MAX_SIZE   1

Maximum size of the output from psa_raw_key_agreement().

This macro expands to a compile-time constant integer. This value is the maximum size of the output any raw key agreement algorithm, in bytes.

See also PSA_RAW_KEY_AGREEMENT_OUTPUT_SIZE(key_type, key_bits).

§ PSA_CIPHER_IV_LENGTH

#define PSA_CIPHER_IV_LENGTH (   key_type,
  alg 
)
Value:
(PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type) > 1 && \
((alg) == PSA_ALG_CTR || \
(alg) == PSA_ALG_CFB || \
(alg) == PSA_ALG_OFB || \
(alg) == PSA_ALG_XTS || \
(alg) == PSA_ALG_CBC_NO_PADDING || \
(key_type) == PSA_KEY_TYPE_CHACHA20 && \
(alg) == PSA_ALG_STREAM_CIPHER ? 12u : \
(alg) == PSA_ALG_CCM_STAR_NO_TAG ? 13u : \
0u)
#define PSA_BLOCK_CIPHER_BLOCK_LENGTH(type)
Definition: crypto_values.h:809
#define PSA_ALG_CBC_PKCS7
Definition: crypto_values.h:1288
#define PSA_KEY_TYPE_CHACHA20
Definition: crypto_values.h:591
#define PSA_ALG_STREAM_CIPHER
Definition: crypto_values.h:1222
#define PSA_ALG_CBC_NO_PADDING
Definition: crypto_values.h:1280
#define PSA_ALG_CFB
Definition: crypto_values.h:1237
#define PSA_ALG_OFB
Definition: crypto_values.h:1243
#define PSA_ALG_CTR
Definition: crypto_values.h:1231
#define PSA_ALG_XTS
Definition: crypto_values.h:1251
#define PSA_ALG_CCM_STAR_NO_TAG
Definition: crypto_values.h:1320

The default IV size for a cipher algorithm, in bytes.

The IV that is generated as part of a call to psa_cipher_encrypt() is always the default IV length for the algorithm.

This macro can be used to allocate a buffer of sufficient size to store the IV output from psa_cipher_generate_iv() when using a multi-part cipher operation.

See also PSA_CIPHER_IV_MAX_SIZE.

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algA cipher algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_CIPHER(alg) is true).
Returns
The default IV size for the specified key type and algorithm. If the algorithm does not use an IV, return 0. If the key type or cipher algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_CIPHER_IV_MAX_SIZE

#define PSA_CIPHER_IV_MAX_SIZE   16u

The maximum IV size for all supported cipher algorithms, in bytes.

See also PSA_CIPHER_IV_LENGTH().

§ PSA_CIPHER_ENCRYPT_OUTPUT_SIZE

#define PSA_CIPHER_ENCRYPT_OUTPUT_SIZE (   key_type,
  alg,
  input_length 
)
Value:
(alg == PSA_ALG_CBC_PKCS7 ? \
(PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type) != 0 ? \
PSA_ROUND_UP_TO_MULTIPLE(PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type), \
(input_length) + 1u) + \
PSA_CIPHER_IV_LENGTH((key_type), (alg)) : 0u) : \
(input_length) + PSA_CIPHER_IV_LENGTH((key_type), (alg)) : \
0u))
#define PSA_BLOCK_CIPHER_BLOCK_LENGTH(type)
Definition: crypto_values.h:809
#define PSA_ALG_CBC_PKCS7
Definition: crypto_values.h:1288
#define PSA_CIPHER_IV_LENGTH(key_type, alg)
Definition: crypto_sizes.h:1151
#define PSA_ALG_IS_CIPHER(alg)
Definition: crypto_values.h:875

The maximum size of the output of psa_cipher_encrypt(), in bytes.

If the size of the output buffer is at least this large, it is guaranteed that psa_cipher_encrypt() will not fail due to an insufficient buffer size. Depending on the algorithm, the actual size of the output might be smaller.

See also PSA_CIPHER_ENCRYPT_OUTPUT_MAX_SIZE(input_length).

Warning
This macro may evaluate its arguments multiple times or zero times, so you should not pass arguments that contain side effects.
Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algA cipher algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_CIPHER(alg) is true).
input_lengthSize of the input in bytes.
Returns
A sufficient output size for the specified key type and algorithm. If the key type or cipher algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_CIPHER_ENCRYPT_OUTPUT_MAX_SIZE

#define PSA_CIPHER_ENCRYPT_OUTPUT_MAX_SIZE (   input_length)
Value:
(input_length) + 1u) + \
PSA_CIPHER_IV_MAX_SIZE)
#define PSA_ROUND_UP_TO_MULTIPLE(block_size, length)
Definition: crypto_sizes.h:59
#define PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE
Definition: crypto_sizes.h:344

A sufficient output buffer size for psa_cipher_encrypt(), for any of the supported key types and cipher algorithms.

If the size of the output buffer is at least this large, it is guaranteed that psa_cipher_encrypt() will not fail due to an insufficient buffer size.

See also PSA_CIPHER_ENCRYPT_OUTPUT_SIZE(key_type, alg, input_length).

Parameters
input_lengthSize of the input in bytes.

§ PSA_CIPHER_DECRYPT_OUTPUT_SIZE

#define PSA_CIPHER_DECRYPT_OUTPUT_SIZE (   key_type,
  alg,
  input_length 
)
Value:
(input_length) : \
0u)
#define PSA_KEY_TYPE_CATEGORY_SYMMETRIC
Definition: crypto_values.h:429
#define PSA_ALG_IS_CIPHER(alg)
Definition: crypto_values.h:875
#define PSA_KEY_TYPE_CATEGORY_MASK
Definition: crypto_values.h:427

The maximum size of the output of psa_cipher_decrypt(), in bytes.

If the size of the output buffer is at least this large, it is guaranteed that psa_cipher_decrypt() will not fail due to an insufficient buffer size. Depending on the algorithm, the actual size of the output might be smaller.

See also PSA_CIPHER_DECRYPT_OUTPUT_MAX_SIZE(input_length).

Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algA cipher algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_CIPHER(alg) is true).
input_lengthSize of the input in bytes.
Returns
A sufficient output size for the specified key type and algorithm. If the key type or cipher algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_CIPHER_DECRYPT_OUTPUT_MAX_SIZE

#define PSA_CIPHER_DECRYPT_OUTPUT_MAX_SIZE (   input_length)    (input_length)

A sufficient output buffer size for psa_cipher_decrypt(), for any of the supported key types and cipher algorithms.

If the size of the output buffer is at least this large, it is guaranteed that psa_cipher_decrypt() will not fail due to an insufficient buffer size.

See also PSA_CIPHER_DECRYPT_OUTPUT_SIZE(key_type, alg, input_length).

Parameters
input_lengthSize of the input in bytes.

§ PSA_CIPHER_UPDATE_OUTPUT_SIZE

#define PSA_CIPHER_UPDATE_OUTPUT_SIZE (   key_type,
  alg,
  input_length 
)
Value:
(PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type) != 0 ? \
(((alg) == PSA_ALG_CBC_PKCS7 || \
(alg) == PSA_ALG_CBC_NO_PADDING || \
(alg) == PSA_ALG_ECB_NO_PADDING) ? \
PSA_ROUND_UP_TO_MULTIPLE(PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type), \
input_length) : \
(input_length)) : 0u) : \
0u)
#define PSA_BLOCK_CIPHER_BLOCK_LENGTH(type)
Definition: crypto_values.h:809
#define PSA_ALG_CBC_PKCS7
Definition: crypto_values.h:1288
#define PSA_ALG_ECB_NO_PADDING
Definition: crypto_values.h:1271
#define PSA_ALG_CBC_NO_PADDING
Definition: crypto_values.h:1280
#define PSA_ALG_IS_CIPHER(alg)
Definition: crypto_values.h:875

A sufficient output buffer size for psa_cipher_update().

If the size of the output buffer is at least this large, it is guaranteed that psa_cipher_update() will not fail due to an insufficient buffer size. The actual size of the output might be smaller in any given call.

See also PSA_CIPHER_UPDATE_OUTPUT_MAX_SIZE(input_length).

Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algA cipher algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_CIPHER(alg) is true).
input_lengthSize of the input in bytes.
Returns
A sufficient output size for the specified key type and algorithm. If the key type or cipher algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_CIPHER_UPDATE_OUTPUT_MAX_SIZE

#define PSA_CIPHER_UPDATE_OUTPUT_MAX_SIZE (   input_length)    (PSA_ROUND_UP_TO_MULTIPLE(PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE, input_length))

A sufficient output buffer size for psa_cipher_update(), for any of the supported key types and cipher algorithms.

If the size of the output buffer is at least this large, it is guaranteed that psa_cipher_update() will not fail due to an insufficient buffer size.

See also PSA_CIPHER_UPDATE_OUTPUT_SIZE(key_type, alg, input_length).

Parameters
input_lengthSize of the input in bytes.

§ PSA_CIPHER_FINISH_OUTPUT_SIZE

#define PSA_CIPHER_FINISH_OUTPUT_SIZE (   key_type,
  alg 
)
Value:
(alg == PSA_ALG_CBC_PKCS7 ? \
PSA_BLOCK_CIPHER_BLOCK_LENGTH(key_type) : \
0u) : \
0u)
#define PSA_ALG_CBC_PKCS7
Definition: crypto_values.h:1288
#define PSA_ALG_IS_CIPHER(alg)
Definition: crypto_values.h:875

A sufficient ciphertext buffer size for psa_cipher_finish().

If the size of the ciphertext buffer is at least this large, it is guaranteed that psa_cipher_finish() will not fail due to an insufficient ciphertext buffer size. The actual size of the output might be smaller in any given call.

See also PSA_CIPHER_FINISH_OUTPUT_MAX_SIZE().

Parameters
key_typeA symmetric key type that is compatible with algorithm alg.
algA cipher algorithm (PSA_ALG_XXX value such that PSA_ALG_IS_CIPHER(alg) is true).
Returns
A sufficient output size for the specified key type and algorithm. If the key type or cipher algorithm is not recognized, or the parameters are incompatible, return 0.

§ PSA_CIPHER_FINISH_OUTPUT_MAX_SIZE

#define PSA_CIPHER_FINISH_OUTPUT_MAX_SIZE   (PSA_BLOCK_CIPHER_BLOCK_MAX_SIZE)

A sufficient ciphertext buffer size for psa_cipher_finish(), for any of the supported key types and cipher algorithms.

See also PSA_CIPHER_FINISH_OUTPUT_SIZE(key_type, alg).

© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale