![]() |
![]() |
|
SimpleLinkGraphicsLibrary
5.00.00.05
|
Functions | |
| void | Graphics_drawImageButton (const Graphics_Context *context, const Graphics_ImageButton *imageButton) |
| bool | Graphics_isImageButtonSelected (const Graphics_ImageButton *imageButton, uint16_t x, uint16_t y) |
| void | Graphics_drawSelectedImageButton (const Graphics_Context *context, const Graphics_ImageButton *imageButton) |
| void | Graphics_drawReleasedImageButton (const Graphics_Context *context, const Graphics_ImageButton *imageButton) |
| void Graphics_drawImageButton | ( | const Graphics_Context * | context, |
| const Graphics_ImageButton * | imageButton | ||
| ) |
Draws a ImageButton .
| context | is a pointer to the drawing context to use. |
| imageButton | is a pointer to the structure containing the extents of the ImageButton . |
This function draws a ImageButton . The ImageButton will contain the image passed in the ImageButton struct.
References Graphics_ImageButton::borderWidth, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_drawImage(), Graphics_fillRectangle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_ImageButton::imageHeight, Graphics_ImageButton::imageWidth, Graphics_ImageButton::xPosition, and Graphics_ImageButton::yPosition.
| bool Graphics_isImageButtonSelected | ( | const Graphics_ImageButton * | imageButton, |
| uint16_t | x, | ||
| uint16_t | y | ||
| ) |
Determines if x and y coordinates are contained in ImageButton .
| imageButton | is a pointer to the structure containing the extents of the ImageButton . |
| x | x-coordinate to be determined if is inside ImageButton |
| y | y-coordinate to be determined if is inside ImageButton |
This function determines if x and y coordinates are contains inside ImageButton
References Graphics_ImageButton::borderWidth, Graphics_ImageButton::imageHeight, Graphics_ImageButton::imageWidth, Graphics_ImageButton::xPosition, and Graphics_ImageButton::yPosition.
| void Graphics_drawSelectedImageButton | ( | const Graphics_Context * | context, |
| const Graphics_ImageButton * | imageButton | ||
| ) |
Draws a selected ImageButton .
| context | is a pointer to the drawing context to use. |
| imageButton | is a pointer to the structure containing the extents of the ImageButton . |
This function draws a ImageButton using the selected parameters.
References Graphics_ImageButton::borderWidth, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_drawImage(), Graphics_fillRectangle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_ImageButton::imageHeight, Graphics_ImageButton::imageWidth, Graphics_ImageButton::xPosition, and Graphics_ImageButton::yPosition.
| void Graphics_drawReleasedImageButton | ( | const Graphics_Context * | context, |
| const Graphics_ImageButton * | imageButton | ||
| ) |
Draws a released ImageButton .
| context | is a pointer to the drawing context to use. |
| imageButton | is a pointer to the structure containing the extents of the ImageButton . |
This function draws a ImageButton using the released parameters.
References Graphics_ImageButton::borderWidth, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_drawImage(), Graphics_fillRectangle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_ImageButton::imageHeight, Graphics_ImageButton::imageWidth, Graphics_ImageButton::xPosition, and Graphics_ImageButton::yPosition.