Data Fields
SemaphoreP_Struct Union Reference

SemaphoreP structure. More...

#include <SemaphoreP.h>

Data Fields

uint32_t dummy
 
uint8_t data [(80)]
 

Detailed Description

SemaphoreP structure.

Opaque structure that should be large enough to hold any of the RTOS specific SemaphoreP objects.

Field Documentation

§ dummy

uint32_t SemaphoreP_Struct::dummy

Align object

§ data

uint8_t SemaphoreP_Struct::data[(80)]

The documentation for this union was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale